CC13xx Driver Library
rfc_CMD_FS_s Struct Reference

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0803. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips if the rule involves skipping. More...
 
condition
 
uint16_t frequency
 The frequency in MHz to tune to. More...
 
uint16_t fractFreq
 Fractional part of the frequency to tune to. More...
 
struct {
   uint8_t   bTxMode:1
 0: Start synth in Rx mode
1: Start synth in Tx mode More...
 
   uint8_t   refFreq:6
 0: Use default reference frequency
Others: Use reference frequency 24 MHz/refFreq More...
 
synthConf
 
uint8_t __dummy0
 
uint8_t midPrecal
 Mid pre-calibration value to use when bOverrideCalib and bSkipCoarseCalib are both 1. More...
 
uint8_t ktPrecal
 KT pre-calibration value to use when bOverrideCalib and bSkipCoarseCalib are both 1. More...
 
uint16_t tdcPrecal
 TDC pre-calibration value to use when bOverrideCalib and bSkipCoarseCalib are both 1. More...
 

Detailed Description

Definition at line 223 of file rf_common_cmd.h.

Field Documentation

uint8_t rfc_CMD_FS_s::__dummy0

Definition at line 250 of file rf_common_cmd.h.

uint8_t rfc_CMD_FS_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

Definition at line 232 of file rf_common_cmd.h.

uint8_t rfc_CMD_FS_s::bTxMode

0: Start synth in Rx mode
1: Start synth in Tx mode

Definition at line 245 of file rf_common_cmd.h.

uint16_t rfc_CMD_FS_s::commandNo

The command ID number 0x0803.

Definition at line 224 of file rf_common_cmd.h.

struct { ... } rfc_CMD_FS_s::condition
uint16_t rfc_CMD_FS_s::fractFreq

Fractional part of the frequency to tune to.

Definition at line 243 of file rf_common_cmd.h.

uint16_t rfc_CMD_FS_s::frequency

The frequency in MHz to tune to.

Definition at line 242 of file rf_common_cmd.h.

uint8_t rfc_CMD_FS_s::ktPrecal

KT pre-calibration value to use when bOverrideCalib and bSkipCoarseCalib are both 1.

Definition at line 252 of file rf_common_cmd.h.

uint8_t rfc_CMD_FS_s::midPrecal

Mid pre-calibration value to use when bOverrideCalib and bSkipCoarseCalib are both 1.

Definition at line 251 of file rf_common_cmd.h.

uint8_t rfc_CMD_FS_s::nSkip

Number of skips if the rule involves skipping.

Definition at line 240 of file rf_common_cmd.h.

uint8_t rfc_CMD_FS_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

Definition at line 235 of file rf_common_cmd.h.

rfc_radioOp_t* rfc_CMD_FS_s::pNextOp

Pointer to the next operation to run after this operation is done.

Definition at line 228 of file rf_common_cmd.h.

uint8_t rfc_CMD_FS_s::refFreq

0: Use default reference frequency
Others: Use reference frequency 24 MHz/refFreq

Definition at line 247 of file rf_common_cmd.h.

uint8_t rfc_CMD_FS_s::rule

Condition for running next command: Rule for how to proceed.

Definition at line 239 of file rf_common_cmd.h.

ratmr_t rfc_CMD_FS_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

Definition at line 229 of file rf_common_cmd.h.

struct { ... } rfc_CMD_FS_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_FS_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

Definition at line 225 of file rf_common_cmd.h.

struct { ... } rfc_CMD_FS_s::synthConf
uint16_t rfc_CMD_FS_s::tdcPrecal

TDC pre-calibration value to use when bOverrideCalib and bSkipCoarseCalib are both 1.

Definition at line 253 of file rf_common_cmd.h.

uint8_t rfc_CMD_FS_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

Definition at line 234 of file rf_common_cmd.h.

uint8_t rfc_CMD_FS_s::triggerType

The type of trigger.

Definition at line 231 of file rf_common_cmd.h.