Go to the source code of this file.
Typedefs | |
typedef void(* | aes_ecb_encrypt_t) (uint8_t *, uint16_t, uint8_t *) |
typedef void(* | aes_ecb_decrypt_t) (uint8_t *, uint16_t, uint8_t *) |
typedef int8_t(* | aes_ccm_encrypt_t) (uint8_t, uint8_t, uint8_t *, uint8_t *, uint16_t, uint8_t *, uint16_t, uint8_t *, uint8_t *, uint8_t) |
typedef int8_t(* | aes_ccm_decrypt_t) (uint8_t, uint8_t, uint8_t *, uint8_t *, uint16_t, uint8_t *, uint16_t, uint8_t *, uint8_t *, uint8_t) |
typedef uint8_t(* | aes_ctr_encrypt_t) (uint8_t *, uint16_t, uint8_t *, uint8_t *, uint8_t *) |
typedef uint8_t(* | aes_ctr_decrypt_t) (uint8_t *, uint16_t, uint8_t *, uint8_t *, uint8_t *) |
typedef uint8_t(* | ecc_keygen_t) (uint32_t *, uint32_t *, uint32_t *, uint32_t *) |
typedef uint8_t(* | ecdsa_sign_t) (uint32_t *, uint32_t *, uint32_t *, uint32_t *, uint32_t *) |
typedef uint8_t(* | ecdsa_verify_t) (uint32_t *, uint32_t *, uint32_t *, uint32_t *, uint32_t *) |
typedef uint8_t(* | ecdh_computeSharedSecret_t) (uint32_t *, uint32_t *, uint32_t *, uint32_t *, uint32_t *) |
typedef uint8_t(* | sha256_full_t) (SHA256_memory_t *, uint8_t *, uint8_t *, uint32_t) |
typedef uint8_t(* | sha256_init_t) (SHA256_memory_t *) |
typedef uint8_t(* | sha256_process_t) (SHA256_memory_t *, uint8_t *, uint32_t) |
typedef uint8_t(* | sha256_final_t) (SHA256_memory_t *, uint8_t *) |
Functions | |
void | AES_ECB_EncryptData (uint8_t *text, uint16_t textLen, uint8_t *aesKey) |
Use a random 128 bit key to encrypt data with the AES. More... | |
void | AES_ECB_DecryptData (uint8_t *text, uint16_t textLen, uint8_t *aesKey) |
Use a random 128 bit key to decrypt data with the AES. More... | |
int8_t | AES_CCM_EncryptData (uint8_t encryptFlag, uint8_t MACLen, uint8_t *nonce, uint8_t *plainText, uint16_t textLen, uint8_t *addDataBuf, uint16_t addBufLen, uint8_t *aesKey, uint8_t *MAC, uint8_t ccmLVal) |
Authenticate and optionally encrypt message plainText. More... | |
int8_t | AES_CCM_DecryptData (uint8_t decryptFlag, uint8_t MACLen, uint8_t *nonce, uint8_t *cipherText, uint16_t textLen, uint8_t *addDataBuf, uint16_t addBufLen, uint8_t *aesKey, uint8_t *MAC, uint8_t ccmLVal) |
Authenticate and optionally decrypt message cipherText. More... | |
uint8_t | AES_CTR_EncryptData (uint8_t *plainText, uint16_t textLen, uint8_t *aesKey, uint8_t *nonce, uint8_t *initVector) |
Encrypt plaintext using the AES key, nonce and initialization vector. More... | |
uint8_t | AES_CTR_DecryptData (uint8_t *cipherText, uint16_t textLen, uint8_t *aesKey, uint8_t *nonce, uint8_t *initVector) |
Decrypt ciphertext using the AES key, nonce and initialization vector. More... | |
void | ECC_initialize (uint32_t *pWorkzone) |
Pass pointer to ECC memory allocation to ECC engine. More... | |
uint8_t | ECC_generateKey (uint32_t *randString, uint32_t *privateKey, uint32_t *publicKey_x, uint32_t *publicKey_y) |
Generate a key. More... | |
uint8_t | ECC_ECDSA_sign (uint32_t *secretKey, uint32_t *text, uint32_t *randString, uint32_t *sign1, uint32_t *sign2) |
Sign data. More... | |
uint8_t | ECC_ECDSA_verify (uint32_t *publicKey_x, uint32_t *publicKey_y, uint32_t *text, uint32_t *sign1, uint32_t *sign2) |
Verify signature. More... | |
uint8_t | ECC_ECDH_computeSharedSecret (uint32_t *privateKey, uint32_t *publicKey_x, uint32_t *publicKey_y, uint32_t *sharedSecret_x, uint32_t *sharedSecret_y) |
Compute the shared secret. More... | |
uint8_t | SHA256_runFullAlgorithm (SHA256_memory_t *memory, uint8_t *pBufIn, uint32_t bufLen, uint8_t *pBufOut) |
Perform SHA256 on the the input data. More... | |
uint8_t | SHA256_initialize (SHA256_memory_t *memory) |
Intializes the SHA256 engine. More... | |
uint8_t | SHA256_execute (SHA256_memory_t *memory, uint8_t *pBufIn, uint32_t bufLen) |
Perform SHA256. More... | |
uint8_t | SHA256_output (SHA256_memory_t *memory, uint8_t *pBufOut) |
Complete the process by passing the modified data back. More... | |
Variables | |
aes_ecb_encrypt_t | aes_ecb_encrypt = (aes_ecb_encrypt_t)(0x10018a99) |
aes_ecb_decrypt_t | aes_ecb_decrypt = (aes_ecb_decrypt_t)(0x10018ac5) |
aes_ccm_encrypt_t | aes_ccm_encrypt = (aes_ccm_encrypt_t)(0x10018a19) |
aes_ccm_decrypt_t | aes_ccm_decrypt = (aes_ccm_decrypt_t)(0x10018a35) |
aes_ctr_encrypt_t | aes_ctr_encrypt = (aes_ctr_encrypt_t)(0x100175ed) |
aes_ctr_decrypt_t | aes_ctr_decrypt = (aes_ctr_decrypt_t)(0x10017771) |
ecc_keygen_t | ecc_generatekey = (ecc_keygen_t)(0x10017dbd) |
ecdsa_sign_t | ecc_ecdsa_sign = (ecdsa_sign_t)(0x10017969) |
ecdsa_verify_t | ecc_ecdsa_verify = (ecdsa_verify_t)(0x10017b01) |
ecdh_computeSharedSecret_t | ecdh_computeSharedSecret = (ecdh_computeSharedSecret_t)(0x10017ded) |
sha256_full_t | sha256_runfullalg = (sha256_full_t)(0x10018129) |
sha256_init_t | sha256_initialize = (sha256_init_t)(0x10017ffd) |
sha256_process_t | sha256_execute = (sha256_process_t)(0x10018019) |
sha256_final_t | sha256_output = (sha256_final_t)(0x10018089) |
typedef int8_t(* aes_ccm_decrypt_t) (uint8_t, uint8_t, uint8_t *, uint8_t *, uint16_t, uint8_t *, uint16_t, uint8_t *, uint8_t *, uint8_t) |
Definition at line 74 of file rom_crypto.c.
typedef int8_t(* aes_ccm_encrypt_t) (uint8_t, uint8_t, uint8_t *, uint8_t *, uint16_t, uint8_t *, uint16_t, uint8_t *, uint8_t *, uint8_t) |
Definition at line 69 of file rom_crypto.c.
typedef uint8_t(* aes_ctr_decrypt_t) (uint8_t *, uint16_t, uint8_t *, uint8_t *, uint8_t *) |
Definition at line 109 of file rom_crypto.c.
typedef uint8_t(* aes_ctr_encrypt_t) (uint8_t *, uint16_t, uint8_t *, uint8_t *, uint8_t *) |
Definition at line 105 of file rom_crypto.c.
typedef void(* aes_ecb_decrypt_t) (uint8_t *, uint16_t, uint8_t *) |
Definition at line 49 of file rom_crypto.c.
typedef void(* aes_ecb_encrypt_t) (uint8_t *, uint16_t, uint8_t *) |
Definition at line 46 of file rom_crypto.c.
typedef uint8_t(* ecc_keygen_t) (uint32_t *, uint32_t *, uint32_t *, uint32_t *) |
Definition at line 190 of file rom_crypto.c.
typedef uint8_t(* ecdh_computeSharedSecret_t) (uint32_t *, uint32_t *, uint32_t *, uint32_t *, uint32_t *) |
Definition at line 199 of file rom_crypto.c.
typedef uint8_t(* ecdsa_sign_t) (uint32_t *, uint32_t *, uint32_t *, uint32_t *, uint32_t *) |
Definition at line 193 of file rom_crypto.c.
typedef uint8_t(* ecdsa_verify_t) (uint32_t *, uint32_t *, uint32_t *, uint32_t *, uint32_t *) |
Definition at line 196 of file rom_crypto.c.
typedef uint8_t(* sha256_final_t) (SHA256_memory_t *, uint8_t *) |
Definition at line 257 of file rom_crypto.c.
typedef uint8_t(* sha256_full_t) (SHA256_memory_t *, uint8_t *, uint8_t *, uint32_t) |
Definition at line 248 of file rom_crypto.c.
typedef uint8_t(* sha256_init_t) (SHA256_memory_t *) |
Definition at line 251 of file rom_crypto.c.
typedef uint8_t(* sha256_process_t) (SHA256_memory_t *, uint8_t *, uint32_t) |
Definition at line 254 of file rom_crypto.c.
aes_ccm_decrypt_t aes_ccm_decrypt = (aes_ccm_decrypt_t)(0x10018a35) |
Definition at line 77 of file rom_crypto.c.
Referenced by AES_CCM_DecryptData().
aes_ccm_encrypt_t aes_ccm_encrypt = (aes_ccm_encrypt_t)(0x10018a19) |
Definition at line 72 of file rom_crypto.c.
Referenced by AES_CCM_EncryptData().
aes_ctr_decrypt_t aes_ctr_decrypt = (aes_ctr_decrypt_t)(0x10017771) |
Definition at line 111 of file rom_crypto.c.
Referenced by AES_CTR_DecryptData().
aes_ctr_encrypt_t aes_ctr_encrypt = (aes_ctr_encrypt_t)(0x100175ed) |
Definition at line 107 of file rom_crypto.c.
Referenced by AES_CTR_EncryptData().
aes_ecb_decrypt_t aes_ecb_decrypt = (aes_ecb_decrypt_t)(0x10018ac5) |
Definition at line 50 of file rom_crypto.c.
Referenced by AES_ECB_DecryptData().
aes_ecb_encrypt_t aes_ecb_encrypt = (aes_ecb_encrypt_t)(0x10018a99) |
Definition at line 47 of file rom_crypto.c.
Referenced by AES_ECB_EncryptData().
ecdsa_sign_t ecc_ecdsa_sign = (ecdsa_sign_t)(0x10017969) |
Definition at line 194 of file rom_crypto.c.
Referenced by ECC_ECDSA_sign().
ecdsa_verify_t ecc_ecdsa_verify = (ecdsa_verify_t)(0x10017b01) |
Definition at line 197 of file rom_crypto.c.
Referenced by ECC_ECDSA_verify().
ecc_keygen_t ecc_generatekey = (ecc_keygen_t)(0x10017dbd) |
Definition at line 191 of file rom_crypto.c.
Referenced by ECC_generateKey().
ecdh_computeSharedSecret_t ecdh_computeSharedSecret = (ecdh_computeSharedSecret_t)(0x10017ded) |
Definition at line 200 of file rom_crypto.c.
Referenced by ECC_ECDH_computeSharedSecret().
sha256_process_t sha256_execute = (sha256_process_t)(0x10018019) |
Definition at line 255 of file rom_crypto.c.
Referenced by SHA256_execute().
sha256_init_t sha256_initialize = (sha256_init_t)(0x10017ffd) |
Definition at line 252 of file rom_crypto.c.
Referenced by SHA256_initialize().
sha256_final_t sha256_output = (sha256_final_t)(0x10018089) |
Definition at line 258 of file rom_crypto.c.
Referenced by SHA256_output().
sha256_full_t sha256_runfullalg = (sha256_full_t)(0x10018129) |
Definition at line 249 of file rom_crypto.c.
Referenced by SHA256_runFullAlgorithm().