TI-RTOS for SimpleLink Wireless MCUs  2.14.01.20
PWMTimerTiva.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
83 #ifndef ti_driver_pwm_PWMTimerTiva__include
84 #define ti_driver_pwm_PWMTimerTiva__include
85 
86 #ifdef __cplusplus
87 extern "C" {
88 #endif
89 
90 #include <ti/drivers/PWM.h>
91 
92 /* PWM_control() commands */
93 #define PWMTimerTiva_CHANGE_PERIOD PWM_CMD_RESERVED + 0
94 
95 /* PWM function table pointer */
97 
120 typedef struct PWMTimerTiva_HWAttrs {
121  uint32_t baseAddr;
122  uint16_t timer;
124 
130 typedef struct PWMTimerTiva_Object {
131  uint32_t period;
132  uint32_t duty;
133  uint8_t dutyMode; /* Units in which duty is specified */
136 
137 #ifdef __cplusplus
138 }
139 #endif
140 
141 #endif /* ti_driver_pwm_PWMTimerTiva__include */
PWMTimerTiva Object.
Definition: PWMTimerTiva.h:130
uint32_t period
Definition: PWMTimerTiva.h:131
PWM driver interface.
struct PWMTimerTiva_HWAttrs PWMTimerTiva_HWAttrs
PWMTimerCC3200 Hardware attributes.
PWMTimerCC3200 Hardware attributes.
Definition: PWMTimerTiva.h:120
The definition of a PWM function table that contains the required set of functions to control a speci...
Definition: PWM.h:327
uint8_t cyclesPerMicroSec
Definition: PWMTimerTiva.h:134
uint32_t duty
Definition: PWMTimerTiva.h:132
uint16_t timer
Definition: PWMTimerTiva.h:122
struct PWMTimerTiva_Object PWMTimerTiva_Object
PWMTimerTiva Object.
const PWM_FxnTable PWMTimerTiva_fxnTable
uint8_t dutyMode
Definition: PWMTimerTiva.h:133
uint32_t baseAddr
Definition: PWMTimerTiva.h:121
Copyright 2015, Texas Instruments Incorporated