#include <MmRpc.h>
Field Documentation
uint32_t MmRpc_Xlt::index |
parameter index to base pointer
ptrdiff_t MmRpc_Xlt::offset |
offset to embedded pointer
If param type is MmRpc_ParamType_Ptr, offset
to embedded pointer from addr. If param type
is MmRpc_ParamType_OffPtr, offset to embedded
pointer from base+offset.
addr or file descriptor [+ data offset]
If param type is MmRpc_ParamType_Ptr, the
value of the embedded pointer. If param type
is MmRpc_ParamType_OffPtr, the file descriptor
of the block referenced by the embedded pointer
plus an optional data offset.
The documentation for this struct was generated from the following file: