SysLink API Reference
2.21.03.11
|
Frame_FrameBufInfo_tag | Structure to frame buffer informantion in frame header |
Frame_FrameHeader_Tag | Structure of the base frame header. FrameQ maintains list of frames to be retrieved by FrameQ reader client. Application is expected to use Helper API to extract fileds and exteneded header pointer |
FrameQ_CommonOpenParams_Tag | Common parameters required to open a FrameQ instance of any implementation |
FrameQ_Config_Tag | Structure defining config parameters for the FrameQ module |
FrameQ_CreateParams_Tag | Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure |
FrameQ_NotifyParams_Tag | Notification parameter structure |
FrameQ_Params | Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure |
FrameQ_ShMem_OpenParams_tag | Structure defining open parameters for the FrameQ instance on ShMem (shared memory interface) |
FrameQ_ShMem_Params_tag | Structure defining instance create parameters for the FrameQ on shared memory(inter core and intra core) |
FrameQBufMgr_CommonOpenParams_Tag | Common parameters required to open a FrameQBufMgr instance of any implementation |
FrameQBufMgr_Config_Tag | Structure defining module config parameters for the FrameQBufMgr module |
FrameQBufMgr_CreateParams_Tag | Common parameters required to create FrameQBufMgr instance of any implementation |
FrameQBufMgr_FrameBufParams_Tag | Frame buffer param structure |
FrameQBufMgr_NotifyParams_Tag | Structure defining notification parameter structure |
FrameQBufMgr_Params | Common parameters required to create FrameQBufMgr instance of any implementation |
FrameQBufMgr_ShMem_OpenParams_tag | Structure defining open parameters for the FrameQ instance on ShMem (shared memory interface) |
FrameQBufMgr_ShMem_Params_tag | Structure defining parameters for the FrameQ module |
GateMP_Params | Structure defining parameters for the GateMP module |
GateProcess_Params | Create parameter structure |
GateProcess_ShMem | Shared memory structure used by instance |
HeapBufMP_ExtendedStats | Stats structure for the HeapBufMP_getExtendedStats API |
HeapBufMP_Params | Structure defining parameters for the HeapBufMP module |
HeapMemMP_ExtendedStats | Stats structure for the HeapMemMP_getExtendedStats API |
HeapMemMP_Params | Structure defining parameters for the HeapMemMP module |
IGateProvider_Object | |
IHeap_Object_tag | Structure for the Handle for the Heap |
Ipc_Terminate | Argument for the Ipc_CONTROLCMD_SETTERMINATEPOLICY command |
IpcMemMgr_Config_t | Structure defining config parameters for overall System |
List_Elem_tag | Structure defining object for the list element |
List_Object_tag | Structure defining object for the list |
List_Params_tag | Structure defining params for the list |
ListMP_Elem | Structure defining a ListMP element |
ListMP_Params | Structure defining parameter structure for ListMP_create() |
Memory_Stats_tag | Structure defining memory related statistics |
MessageQ_MsgHeader | Required first field in every message |
MessageQ_Params | Structure defining parameters for the MessageQ module |
NameServer_Params | NameServer_Handle type |
ProcMgr_AddrInfo_tag | This structure defines information about memory regions mapped by the ProcMgr module |
ProcMgr_AttachParams_tag | Configuration parameters specific to the slave ProcMgr instance |
ProcMgr_MappedMemEntry | Structure containing information of mapped memory regions |
ProcMgr_ProcInfo_tag | Characteristics of the slave processor |
ProcMgr_SectionInfo_tag | Characteristics of sections in executable |
ProcMgr_StartParams_tag | Configuration parameters to be provided while starting the slave processor |
ResTrack_Params | Structure defining params for creating an instance |
RingIO_openParams_Tag | Structure defining config parameters for opening the RingIO instances |
RingIO_Params_Tag | Common parameters required to create RingIO instance of any implementation. It should be the first element of the actual implementaton params structure |
RingIO_sharedMemReqDetails_tag | Structure defining config parameters for opening the RingIO instances |
RingIOShm_Params_Tag | Structure defining parameters for creating the RingIOShm instances |
SharedRegion_Entry | Structure defining a region |
SyslinkMemMgr_AllocBlock_tag | |
SyslinkMemMgr_AllocParams_tag | Alloc params |
SyslinkMemMgr_CreateParams_tag | Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params |