![]() |
![]() |
SysLink API Reference
2.21.02.10
|
Frame buffer param structure. More...
#include <FrameQBufMgr.h>
Data Fields | |
UInt32 | size |
UInt32 | pixelFormat |
UInt32 | height |
UInt32 | width |
UInt32 | align |
Frame buffer param structure.
UInt32 FrameQBufMgr_FrameBufParams_Tag::size |
size of the Frame buffer. valid if it is not a Tiler buffer
UInt32 FrameQBufMgr_FrameBufParams_Tag::pixelFormat |
Pixel format.Valid for Tiler buffers
UInt32 FrameQBufMgr_FrameBufParams_Tag::height |
Height of buffer.Valid for Tiler buffers
UInt32 FrameQBufMgr_FrameBufParams_Tag::width |
Width of the buffer.Valid for Tiler buffers
UInt32 FrameQBufMgr_FrameBufParams_Tag::align |
Alignment of the buffer.Currently not used.