![]() |
![]() |
SysLink API Reference
2.21.02.10
|
Structure defining config parameters for the FrameQ module. More...
#include <FrameQ.h>
Data Fields | |
UInt32 | eventNo |
UInt8 | maxInstances |
UInt32 | usedefaultgate |
Structure defining config parameters for the FrameQ module.
UInt32 FrameQ_Config_Tag::eventNo |
Notify event number used for client notifications
UInt8 FrameQ_Config_Tag::maxInstances |
Maximum instances
UInt32 FrameQ_Config_Tag::usedefaultgate |
If set to TRUE, FrameQ instances will use dafault gate set in FrameQ. If default gate is not set in FrameQ, it uses GateMP's default gate. Set it to zero if FrameQ needs to create gate for a instance (remoteProtect and localProtect flags should be valid in params in this case).