SysLink API Reference  2.21.02.10
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Pages
Functions | Variables
Gate.h File Reference

Detailed Description

Critical section support.

Gates are used by clients to protect concurrent access to critical data structures. Critical data structures are those that must be updated by at most one thread at a time. All code that needs access to a critical data structure "enters" a gate (that's associated with the data structure) prior to accessing the data, modifies the data structure, then "leaves" the gate.

A gate is responsible for ensuring that at most one thread at a time can enter and execute "inside" the gate. There are several implementations of gates, with different system executation times and latency tradoffs. In addition, some gates must not be entered by certain thread types; e.g., a gate that is implemented via a "blocking" semaphore must not be called by an interrupt service routine (ISR).

#include <ti/syslink/utils/IGateProvider.h>
Include dependency graph for Gate.h:

Go to the source code of this file.

Functions

IArg Gate_enterSystem (void)
Void Gate_leaveSystem (IArg key)

Variables

IGateProvider_Handle Gate_systemHandle

Function Documentation

IArg Gate_enterSystem ( void  )
Void Gate_leaveSystem ( IArg  key)

Variable Documentation

IGateProvider_Handle Gate_systemHandle
Copyright 2013, Texas Instruments Incorporated