![]() |
![]() |
SysLink API Reference
2.21.02.10
|
Header file for FrameQBufMgr ShMem. (Deprecated)
Go to the source code of this file.
Data Structures | |
struct | FrameQBufMgr_ShMem_Params_tag |
Structure defining parameters for the FrameQ module. More... | |
struct | FrameQBufMgr_ShMem_OpenParams_tag |
Structure defining open parameters for the FrameQ instance on ShMem (shared memory interface). More... |
Typedefs | |
typedef FrameQBufMgr_Config | FrameQBufMgr_ShMem_Config |
typedef struct FrameQBufMgr_ShMem_Params_tag | FrameQBufMgr_ShMem_Params |
Structure defining parameters for the FrameQ module. | |
typedef struct FrameQBufMgr_ShMem_OpenParams_tag | FrameQBufMgr_ShMem_OpenParams |
Structure defining open parameters for the FrameQ instance on ShMem (shared memory interface). |
Functions | |
Int32 | FrameQBufMgr_ShMem_setup (FrameQBufMgr_ShMem_Config *cfg) |
Int32 | FrameQBufMgr_ShMem_destroy (Void) |
void | FrameQBufMgr_ShMem_Params_init (FrameQBufMgr_ShMem_Params *params) |
Function to initiallze the params with the default params. | |
UInt32 | FrameQBufMgr_ShMem_sharedMemReq (const FrameQBufMgr_ShMem_Params *params, UInt32 *hdrBufChunkSize, UInt32 *frmBufChunkSize) |
Function to find out the shared memory requirements. | |
Int32 | FrameQBufMgr_ShMem_getConfig (FrameQBufMgr_ShMem_Config *cfg) |
#define FrameQBufMgr_ShMem_BUFINTERFACE_SHAREDMEM FrameQBufMgr_BUFINTERFACE_SHAREDMEM |
#define FrameQBufMgr_ShMem_BUFINTERFACE_TILERMEM FrameQBufMgr_BUFINTERFACE_TILERMEM |
#define FrameQBufMgr_ShMem_HDRINTERFACE_SHAREDMEM FrameQBufMgr_HDRINTERFACE_SHAREDMEM |
#define FrameQBufMgr_ShMem_FrameBufParams FrameQBufMgr_FrameBufParams |
typedef struct FrameQBufMgr_ShMem_Params_tag FrameQBufMgr_ShMem_Params |
Structure defining parameters for the FrameQ module.
typedef struct FrameQBufMgr_ShMem_OpenParams_tag FrameQBufMgr_ShMem_OpenParams |
Structure defining open parameters for the FrameQ instance on ShMem (shared memory interface).
Int32 FrameQBufMgr_ShMem_setup | ( | FrameQBufMgr_ShMem_Config * | cfg | ) |
void FrameQBufMgr_ShMem_Params_init | ( | FrameQBufMgr_ShMem_Params * | params | ) |
Function to initiallze the params with the default params.
params | pointer to FrameQBufMgr_ShMem_Params. |
UInt32 FrameQBufMgr_ShMem_sharedMemReq | ( | const FrameQBufMgr_ShMem_Params * | params, |
UInt32 * | hdrBufChunkSize, | ||
UInt32 * | frmBufChunkSize | ||
) |
Function to find out the shared memory requirements.
This function returns size of the shared memory required for the instance based on the params provided.
params | pointer to FrameQ_ShMem_Params. | |
[out] | hdrBufChunkSize | Memory required for frame headers |
[out] | frmBufChunkSize | Memory required for frame buffers |
size | shared memory required for the instance |
Int32 FrameQBufMgr_ShMem_getConfig | ( | FrameQBufMgr_ShMem_Config * | cfg | ) |