![]() |
![]() |
SysLink API Reference
2.21.00.03
|
Common parameters required to create RingIO instance of any implementation. It should be the first element of the actual implementaton params structure . More...
#include <RingIO.h>
Data Fields | |
String | name |
RingIO_Type | interfaceType |
Common parameters required to create RingIO instance of any implementation. It should be the first element of the actual implementaton params structure .
String RingIO_Params_Tag::name |
Name of the instance
RingIO_Type RingIO_Params_Tag::interfaceType |
interface type for ringio transport