![]() |
![]() |
SysLink API Reference
2.21.00.03
|
Structure defining notification parameter structure. More...
#include <FrameQBufMgr.h>
Data Fields | |
SysLink_NotifyType | notifyType |
UInt32 | watermark |
FrameQBufMgr_NotifyFunc | cbFxnPtr |
Ptr | cbContext |
Ptr | cbClientHandle |
Structure defining notification parameter structure.
SysLink_NotifyType FrameQBufMgr_NotifyParams_Tag::notifyType |
Notification type.See SysLink_NotifyType
UInt32 FrameQBufMgr_NotifyParams_Tag::watermark |
Minumum number of free frames required to generate notification Same water mark for all the individual freeFramePools in the set.
FrameQBufMgr_NotifyFunc FrameQBufMgr_NotifyParams_Tag::cbFxnPtr |
Callback function
Ptr FrameQBufMgr_NotifyParams_Tag::cbContext |
Context pointer that needs to be passed to call back function.
Ptr FrameQBufMgr_NotifyParams_Tag::cbClientHandle |
Handle that needs to be passed as first arg to call back. Ideally this should be callers client handle.