![]() |
![]() |
SysLink API Reference
2.21.00.03
|
Structure to frame buffer informantion in frame header. More...
#include <FrameQDefs.h>
Data Fields | |
UInt32 | bufPtr |
UInt32 | bufSize |
UInt32 | startOffset |
UInt32 | validSize |
UInt32 | pixelFormat |
UInt32 | height |
UInt32 | width |
UInt32 | stride |
Structure to frame buffer informantion in frame header.
UInt32 Frame_FrameBufInfo_tag::bufPtr |
Pointer to the frame buffer.
UInt32 Frame_FrameBufInfo_tag::bufSize |
Size of the buffer.
UInt32 Frame_FrameBufInfo_tag::startOffset |
Start offset in the buffer from where valid data starts.
UInt32 Frame_FrameBufInfo_tag::validSize |
Valid size in the buffer from the zeroth offset in the frame buffer
UInt32 Frame_FrameBufInfo_tag::pixelFormat |
UInt32 Frame_FrameBufInfo_tag::height |
UInt32 Frame_FrameBufInfo_tag::width |
UInt32 Frame_FrameBufInfo_tag::stride |