![]() |
![]() |
Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params. More...
#include <SyslinkMemMgr.h>
Data Fields | |
UInt32 | size |
SyslinkMemMgr_Type | memMgrType |
UInt8 | name [32u] |
Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params.
Size of the param structure
type of implementation.
Name of the instance