Structure defining parameters for creating the RingIOShm instances. More...
#include <RingIOShm.h>
Structure defining parameters for creating the RingIOShm instances.
Common create parameters .Same for all the implementations of RingIO
Shared region ID for RingIOShm control structures
The index corresponding to the shared region from which shared memory will be allocated if ctrlSharedAddr is NULL. If a valid ctrlSharedAddr is provided, this field is ignored.
Shared region ID for RingIOShm data buffer
The index corresponding to the shared region from which shared memory will be allocated if dataSharedAddr is NULL. If a valid dataSharedAddr is provided, this field is ignored.
Shared region ID for RingIOShm attr buffer
The index corresponding to the shared region from which shared memory will be allocated if attrSharedAddr is NULL. If a valid attrSharedAddr is provided, this field is ignored.
Shared region address for control structure. If this field is NULL, memory equal to that required to allocate the RingIOShm instance control structure is allocated from heap associated with ctrlRegionId
Shared Region Address for data buffer If this field is NULL, memory equal to (dataSharedAddrSize + footBufSize) is allocated from heap associated with dataRegionId
Data Buffer size.
Foot Buffer size.
Shared Region Address for attr buffer If this field is NULL, memory equal to attrSharedAddrSize is allocated from heap associated with attrRegionId
Attr Buffer size.
Gate for protection. If gateHandle is NULL, the default GateMP instance provided by the GateMP module is used.
Local protection level for the module instance.(not used currently)
Remote protection level for the module instance.(not used currently)
Remote processor id with which the RingIOShm communicates