![]() |
![]() |
Structure containing information required for mapping a memory region. More...
#include <_MemoryDefs.h>
Data Fields | |
UInt32 | src |
UInt32 | size |
UInt32 | dst |
Bool | isCached |
Ptr | drvHandle |
Structure containing information required for mapping a memory region.
Address to be mapped.
Size of memory region to be mapped.
Mapped address.
Whether the mapping is to a cached area or uncached area.
Handle to the driver that is implementing the mmap call. Ignored for Kernel-side version.