![]() |
![]() |
Stats structure for the HeapMultiBufMP_getExtendedStats API. More...
#include <HeapMultiBufMP.h>
Data Fields | |
UInt | numBuckets |
UInt | numBlocks [((UInt) 8)] |
UInt | blockSize [((UInt) 8)] |
UInt | align [((UInt) 8)] |
UInt | maxAllocatedBlocks [((UInt) 8)] |
UInt | numAllocatedBlocks [((UInt) 8)] |
Stats structure for the HeapMultiBufMP_getExtendedStats API.
Number of buffers after optimization
Number of blocks in each buffer
Block size of each buffer
Alignment of each buffer
The maximum number of blocks allocated from this heap at any single point in time during the lifetime of this HeapMultiBufMP instance
The total number of blocks currently allocated in this HeapMultiBufMP instance