![]() |
![]() |
Frame buffer param structure. More...
#include <FrameQBufMgr.h>
Data Fields | |
UInt32 | size |
UInt32 | pixelFormat |
UInt32 | height |
UInt32 | width |
UInt32 | align |
Frame buffer param structure.
size of the Frame buffer. valid if it is not a Tiler buffer
Pixel format.Valid for Tiler buffers
Height of buffer.Valid for Tiler buffers
Width of the buffer.Valid for Tiler buffers
Alignment of the buffer.Currently not used.