Data Fields

Frame_FrameBufInfo_tag Struct Reference

Structure to frame buffer informantion in frame header. More...

#include <FrameQDefs.h>

Data Fields

UInt32 bufPtr
UInt32 bufSize
UInt32 startOffset
UInt32 validSize
UInt32 pixelFormat
UInt32 height
UInt32 width
UInt32 stride

Detailed Description

Structure to frame buffer informantion in frame header.


Field Documentation

Pointer to the frame buffer.

Size of the buffer.

Start offset in the buffer from where valid data starts.

Valid size in the buffer from the zeroth offset in the frame buffer


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated