![]() |
![]() |
Process level gate.
Go to the source code of this file.
Data Structures | |
struct | GateProcess_Params |
Create parameter structure. More... | |
struct | GateProcess_ShMem |
Shared memory structure used by instance. More... | |
Defines | |
#define | GateProcess_E_INVALIDARG (-1) |
Argument passed to a function is invalid. | |
#define | GateProcess_E_MEMORY (-2) |
Memory allocation failed. | |
#define | GateProcess_E_BUSY (-3) |
The name is already registered or not. | |
#define | GateProcess_E_FAIL (-4) |
Generic failure. | |
#define | GateProcess_E_NOTFOUND (-5) |
Name not found in the nameserver. | |
#define | GateProcess_E_INVALIDSTATE (-6) |
Module is not initialized. | |
#define | GateProcess_E_INUSE (-7) |
Indicates that the instance is in use. | |
#define | GateProcess_S_SUCCESS (0) |
Operation successful. | |
Typedefs | |
typedef struct GateProcess_Object | GateProcess_Object |
Object for GateProcess. | |
typedef GateProcess_Object * | GateProcess_Handle |
Handle for GateProcess. | |
Functions | |
IArg | GateProcess_enter (GateProcess_Handle handle) |
Void | GateProcess_leave (GateProcess_Handle handle, IArg key) |
Void | GateProcess_Params_init (GateProcess_Params *params) |
GateProcess_Handle | GateProcess_create (Ptr sharedAddr, const GateProcess_Params *params) |
Int | GateProcess_delete (GateProcess_Handle *pHandle) |
GateProcess_Handle | GateProcess_open (Ptr sharedAddr) |
Int | GateProcess_close (GateProcess_Handle *pHandle) |
SizeT | GateProcess_shMemSize (Void) |
#define GateProcess_E_INVALIDARG (-1) |
Argument passed to a function is invalid.
#define GateProcess_E_MEMORY (-2) |
Memory allocation failed.
#define GateProcess_E_BUSY (-3) |
The name is already registered or not.
#define GateProcess_E_FAIL (-4) |
Generic failure.
#define GateProcess_E_NOTFOUND (-5) |
Name not found in the nameserver.
#define GateProcess_E_INVALIDSTATE (-6) |
Module is not initialized.
#define GateProcess_E_INUSE (-7) |
Indicates that the instance is in use.
#define GateProcess_S_SUCCESS (0) |
Operation successful.
typedef struct GateProcess_Object GateProcess_Object |
Object for GateProcess.
typedef GateProcess_Object* GateProcess_Handle |
Handle for GateProcess.
IArg GateProcess_enter | ( | GateProcess_Handle | handle ) |
Void GateProcess_leave | ( | GateProcess_Handle | handle, |
IArg | key | ||
) |
Void GateProcess_Params_init | ( | GateProcess_Params * | params ) |
GateProcess_Handle GateProcess_create | ( | Ptr | sharedAddr, |
const GateProcess_Params * | params | ||
) |
Int GateProcess_delete | ( | GateProcess_Handle * | pHandle ) |
GateProcess_Handle GateProcess_open | ( | Ptr | sharedAddr ) |
Int GateProcess_close | ( | GateProcess_Handle * | pHandle ) |
SizeT GateProcess_shMemSize | ( | Void | ) |