Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure. More...
#include <FrameQ.h>
Data Fields | |
UInt32 | size |
FrameQ_Interface | ctrlInterfaceType |
String | name |
Bool | openFlag |
Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure.
Size of the paramstructure
Interface type
Name of the instance