Data Fields

SyslinkMemMgr_CreateParams_tag Struct Reference

Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params. More...

#include <SyslinkMemMgr.h>

Data Fields

UInt32 size
SyslinkMemMgr_Type memMgrType
UInt8 name [32u]

Detailed Description

Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params.


Field Documentation

Size of the param structure

type of implementation.

Name of the instance


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated