Data Structures | Defines | Typedefs | Enumerations | Functions

GateMP.h File Reference


Detailed Description

Multiple processor gate that provides local and remote context protection.

============================================================================

A GateMP instance can be used to enforce both local and remote context context protection. That is, entering a GateMP can prevent preemption by another thread running on the same processor and simultaneously prevent a remote processor from entering the same gate. GateMP's are typically used to protect reads/writes to a shared resource, such as shared memory.

Creating a GateMP requires supplying the following configuration

Once created GateMP allows the gate to be opened on another processor using GateMP_open and the name that was used in GateMP_create.

A GateMP can be entered and left using GateMP_enter and GateMP_leave like any other gate that implements the IGateProvider interface.

GateMP has the following proxies - RemoteSystemProxy, RemoteCustom1Proxy and RemoteCustom2Proxy which are automatically plugged with device-specific delegates that implement multiple processor mutexes using a variety of hardware mechanisms.

GateMP creates a default system gate whose handle may be obtained using GateMP_getDefaultRemote. Most IPC modules typically use this gate by default if they require gates and no instance gate is configured by the user.

The GateMP header should be included in an application as follows:

  #include <ti/ipc/GateMP.h>
Version:
0.00.01

============================================================================

Go to the source code of this file.

Data Structures

struct  GateMP_Params
 Structure defining parameters for the GateMP module. More...

Defines

#define GateMP_S_BUSY   2
 The resource is still in use.
#define GateMP_S_ALREADYSETUP   1
 The module has been already setup.
#define GateMP_S_SUCCESS   0
 Operation is successful.
#define GateMP_E_FAIL   -1
 Generic failure.
#define GateMP_E_INVALIDARG   -2
 Argument passed to function is invalid.
#define GateMP_E_MEMORY   -3
 Operation resulted in memory failure.
#define GateMP_E_ALREADYEXISTS   -4
 The specified entity already exists.
#define GateMP_E_NOTFOUND   -5
 Unable to find the specified entity.
#define GateMP_E_TIMEOUT   -6
 Operation timed out.
#define GateMP_E_INVALIDSTATE   -7
 Module is not initialized.
#define GateMP_E_OSFAILURE   -8
 A failure occurred in an OS-specific call.
#define GateMP_E_RESOURCE   -9
 Specified resource is not available.
#define GateMP_E_RESTART   -10
 Operation was interrupted. Please restart the operation.

Typedefs

typedef enum GateMP_LocalProtect GateMP_LocalProtect
 A set of local context protection levels.
typedef enum GateMP_RemoteProtect GateMP_RemoteProtect
 Type of remote Gate.
typedef struct GateMP_Object * GateMP_Handle
 GateMP_Handle type.
typedef struct GateMP_Params GateMP_Params
 Structure defining parameters for the GateMP module.

Enumerations

enum  GateMP_LocalProtect {
  GateMP_LocalProtect_NONE = 0,
  GateMP_LocalProtect_INTERRUPT = 1,
  GateMP_LocalProtect_TASKLET = 2,
  GateMP_LocalProtect_THREAD = 3,
  GateMP_LocalProtect_PROCESS = 4
}
 

A set of local context protection levels.

More...
enum  GateMP_RemoteProtect {
  GateMP_RemoteProtect_NONE = 0,
  GateMP_RemoteProtect_SYSTEM = 1,
  GateMP_RemoteProtect_CUSTOM1 = 2,
  GateMP_RemoteProtect_CUSTOM2 = 3
}
 

Type of remote Gate.

More...

Functions

Int GateMP_close (GateMP_Handle *handlePtr)
 Close an opened gate.
GateMP_Handle GateMP_create (const GateMP_Params *params)
 Create a GateMP instance.
Int GateMP_delete (GateMP_Handle *handlePtr)
 Delete a created GateMP instance.
GateMP_Handle GateMP_getDefaultRemote (Void)
 Get the default remote gate.
GateMP_LocalProtect GateMP_getLocalProtect (GateMP_Handle handle)
 Get the local protection level configured in a GateMP instance.
GateMP_RemoteProtect GateMP_getRemoteProtect (GateMP_Handle handle)
 Get the remote protection level configured in a GateMP instance.
Int GateMP_open (String name, GateMP_Handle *handlePtr)
 Open a created GateMP by name.
Void GateMP_Params_init (GateMP_Params *params)
 Initialize a GateMP parameters struct.
IArg GateMP_enter (GateMP_Handle handle)
 Enter the GateMP.
Void GateMP_leave (GateMP_Handle handle, IArg key)
 Leave the GateMP.

Define Documentation

#define GateMP_S_BUSY   2

The resource is still in use.

#define GateMP_S_ALREADYSETUP   1

The module has been already setup.

#define GateMP_S_SUCCESS   0

Operation is successful.

#define GateMP_E_FAIL   -1

Generic failure.

#define GateMP_E_INVALIDARG   -2

Argument passed to function is invalid.

#define GateMP_E_MEMORY   -3

Operation resulted in memory failure.

#define GateMP_E_ALREADYEXISTS   -4

The specified entity already exists.

#define GateMP_E_NOTFOUND   -5

Unable to find the specified entity.

#define GateMP_E_TIMEOUT   -6

Operation timed out.

#define GateMP_E_INVALIDSTATE   -7

Module is not initialized.

#define GateMP_E_OSFAILURE   -8

A failure occurred in an OS-specific call.

#define GateMP_E_RESOURCE   -9

Specified resource is not available.

#define GateMP_E_RESTART   -10

Operation was interrupted. Please restart the operation.


Typedef Documentation

A set of local context protection levels.

Each member corresponds to a specific local processor gates used for local protection.

In Linux user mode, the following are the mapping for the constants

  • INTERRUPT -> [N/A]
  • TASKLET -> [N/A]
  • THREAD -> GateMutex
  • PROCESS -> GateMutex

In Linux kernel mode, the following are the mapping for the constants

  • INTERRUPT -> [Interrupts disabled]
  • TASKLET -> GateMutex
  • THREAD -> GateMutex
  • PROCESS -> GateMutex

For SYS/BIOS users, the following are the mappings for the constants

  • INTERRUPT -> GateAll: disables interrupts, Swis and Tasks
  • TASKLET -> GateSwi: disables Swis and Tasks
  • THREAD -> GateMutexPri: based on Semaphores
  • PROCESS -> GateMutexPri: based on Semaphores

Type of remote Gate.

Each member corresponds to a specific type of remote gate. Each enum value corresponds to the following remote protection levels:

  • NONE -> No remote protection (the GateMP instance will exclusively offer local protection configured in GateMP_Params::localProtect
  • SYSTEM -> Use the SYSTEM remote protection level (default for remote protection
  • CUSTOM1 -> Use the CUSTOM1 remote protection level
  • CUSTOM2 -> Use the CUSTOM2 remote protection level
typedef struct GateMP_Object* GateMP_Handle

GateMP_Handle type.

typedef struct GateMP_Params GateMP_Params

Structure defining parameters for the GateMP module.


Enumeration Type Documentation

A set of local context protection levels.

Each member corresponds to a specific local processor gates used for local protection.

In Linux user mode, the following are the mapping for the constants

  • INTERRUPT -> [N/A]
  • TASKLET -> [N/A]
  • THREAD -> GateMutex
  • PROCESS -> GateMutex

In Linux kernel mode, the following are the mapping for the constants

  • INTERRUPT -> [Interrupts disabled]
  • TASKLET -> GateMutex
  • THREAD -> GateMutex
  • PROCESS -> GateMutex

For SYS/BIOS users, the following are the mappings for the constants

  • INTERRUPT -> GateAll: disables interrupts, Swis and Tasks
  • TASKLET -> GateSwi: disables Swis and Tasks
  • THREAD -> GateMutexPri: based on Semaphores
  • PROCESS -> GateMutexPri: based on Semaphores
Enumerator:
GateMP_LocalProtect_NONE 

Use no local protection

GateMP_LocalProtect_INTERRUPT 

Use the INTERRUPT local protection level

GateMP_LocalProtect_TASKLET 

Use the TASKLET local protection level

GateMP_LocalProtect_THREAD 

Use the THREAD local protection level

GateMP_LocalProtect_PROCESS 

Use the PROCESS local protection level

Type of remote Gate.

Each member corresponds to a specific type of remote gate. Each enum value corresponds to the following remote protection levels:

  • NONE -> No remote protection (the GateMP instance will exclusively offer local protection configured in GateMP_Params::localProtect
  • SYSTEM -> Use the SYSTEM remote protection level (default for remote protection
  • CUSTOM1 -> Use the CUSTOM1 remote protection level
  • CUSTOM2 -> Use the CUSTOM2 remote protection level
Enumerator:
GateMP_RemoteProtect_NONE 

No remote protection (the GateMP instance will exclusively offer local protection configured in GateMP_Params::localProtect)

GateMP_RemoteProtect_SYSTEM 

Use the SYSTEM remote protection level (default remote protection)

GateMP_RemoteProtect_CUSTOM1 

Use the CUSTOM1 remote protection level

GateMP_RemoteProtect_CUSTOM2 

Use the CUSTOM2 remote protection level


Function Documentation

Int GateMP_close ( GateMP_Handle handlePtr )

Close an opened gate.

Parameters:
[in,out]handlePtrPointer to handle to opened GateMP instance
Returns:
GateMP status
GateMP_Handle GateMP_create ( const GateMP_Params params )

Create a GateMP instance.

The params structure should be initialized using GateMP_Params_init.

Parameters:
[in]paramsGateMP parameters
Returns:
GateMP Handle
Int GateMP_delete ( GateMP_Handle handlePtr )

Delete a created GateMP instance.

Parameters:
[in,out]handlePtrPointer to GateMP handle
Returns:
GateMP Status
GateMP_Handle GateMP_getDefaultRemote ( Void   )

Get the default remote gate.

Returns:
GateMP handle
GateMP_LocalProtect GateMP_getLocalProtect ( GateMP_Handle  handle )

Get the local protection level configured in a GateMP instance.

Returns:
GateMP_LocalProtect corresponding to local protection level
GateMP_RemoteProtect GateMP_getRemoteProtect ( GateMP_Handle  handle )

Get the remote protection level configured in a GateMP instance.

Returns:
GateMP_RemoteProtect corresponding to remote protection level
Int GateMP_open ( String  name,
GateMP_Handle handlePtr 
)

Open a created GateMP by name.

Parameters:
[in]nameName of the GateMP instance
[out]handlePtrPointer to GateMP handle to be opened
Returns:
GateMP status:
Void GateMP_Params_init ( GateMP_Params params )

Initialize a GateMP parameters struct.

Parameters:
[out]paramsPointer to GateMP parameters
IArg GateMP_enter ( GateMP_Handle  handle )

Enter the GateMP.

Parameters:
[in]handleGateMP handle
Returns:
key that must be used to leave the gate
Void GateMP_leave ( GateMP_Handle  handle,
IArg  key 
)

Leave the GateMP.

Parameters:
[in]handleGateMP handle
[in]keykey returned from GateMP_enter
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated