![]() |
![]() |
Structure defining config parameters for the FrameQ module. More...
#include <FrameQ.h>
Data Fields | |
UInt32 | eventNo |
UInt8 | maxInstances |
UInt32 | usedefaultgate |
Structure defining config parameters for the FrameQ module.
Notify event number used for client notifications
Maximum instances
If set to TRUE, FrameQ instances will use dafault gate set in FrameQ. If default gate is not set in FrameQ, it uses GateMP's default gate. Set it to zero if FrameQ needs to create gate for a instance (remoteProtect and localProtect flags should be valid in params in this case).