Data Fields

IpcMemMgr_Config_t Struct Reference

Structure defining config parameters for overall System. More...

#include <IpcMemMgr.h>

Data Fields

UInt32 size
UInt32 minAlign
UInt32 gateOffset

Detailed Description

Structure defining config parameters for overall System.


Field Documentation

Size of the shared memory to create


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated