Data Fields

FrameQBufMgr_Config_Tag Struct Reference

Structure defining module config parameters for the FrameQBufMgr module. More...

#include <FrameQBufMgr.h>

Data Fields

UInt32 eventNo
Bool maxInstances
UInt32 usedefaultgate

Detailed Description

Structure defining module config parameters for the FrameQBufMgr module.


Field Documentation

Event number used for notification

Maximum instances of the module


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated