Data Structures | Typedefs | Functions

FrameQ_ShMem.h File Reference


Detailed Description

Header file for FrameQ on SharedMemory interface.

#include <ti/ipc/GateMP.h>
Include dependency graph for FrameQ_ShMem.h:

Go to the source code of this file.

Data Structures

struct  FrameQ_ShMem_Params_tag
 Structure defining instance create parameters for the FrameQ on shared memory(inter core and intra core). More...
struct  FrameQ_ShMem_OpenParams_tag
 Structure defining open parameters for the FrameQ instance on ShMem (shared memory interface). More...

Typedefs

typedef FrameQ_Config FrameQ_ShMem_Config
typedef struct
FrameQ_ShMem_Params_tag 
FrameQ_ShMem_Params
 Structure defining instance create parameters for the FrameQ on shared memory(inter core and intra core).
typedef struct
FrameQ_ShMem_OpenParams_tag 
FrameQ_ShMem_OpenParams
 Structure defining open parameters for the FrameQ instance on ShMem (shared memory interface).

Functions

void FrameQ_ShMem_Params_init (FrameQ_ShMem_Params *params)
 Function to initiallze the params with the default params.
UInt32 FrameQ_ShMem_sharedMemReq (const FrameQ_ShMem_Params *params)
 Function to find out the shared memory requirements.
Void FrameQ_ShMem_getConfig (FrameQ_ShMem_Config *cfg)
Int32 FrameQ_ShMem_setup (FrameQ_ShMem_Config *cfg)
Int32 FrameQ_ShMem_destroy (void)

Typedef Documentation

Structure defining instance create parameters for the FrameQ on shared memory(inter core and intra core).

Structure defining open parameters for the FrameQ instance on ShMem (shared memory interface).


Function Documentation

void FrameQ_ShMem_Params_init ( FrameQ_ShMem_Params params )

Function to initiallze the params with the default params.

Parameters:
paramspointer to FrameQ_ShMem_Params.
See also:
FrameQ_create
UInt32 FrameQ_ShMem_sharedMemReq ( const FrameQ_ShMem_Params params )

Function to find out the shared memory requirements.

This function returns size of the shared memory required for the instance based on the params provided.

Parameters:
paramspointer to FrameQ_ShMem_Params.
Return values:
sizeshared memory reqired for the instance
See also:
FrameQ_ShMem_Params_init(), FrameQ_create()
Void FrameQ_ShMem_getConfig ( FrameQ_ShMem_Config cfg )
Int32 FrameQ_ShMem_setup ( FrameQ_ShMem_Config cfg )
Int32 FrameQ_ShMem_destroy ( void   )
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated