![]() |
![]() |
Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure . More...
#include <FrameQ.h>
Data Fields | |
UInt32 | size |
FrameQ_Interface | ctrlInterfaceType |
String | name |
Bool | openFlag |
Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure .
Size of the paramstructure
Interface type
Name of the instance