![]() |
![]() |
Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure . More...
#include <FrameQ.h>
Data Fields | |
FrameQ_CreateParams | commonCreateParams |
Ptr | impParams |
UInt32 | impParamsSize |
Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure .
Pointer to implementation specific parameters
Size of the implementation specific structure pointed by impParams.