This module contains common definitions, types, structures and functions used by SysLink.
Go to the source code of this file.
Data Structures | |
struct | SysLink_MemEntry_tag |
Structure for memEntry. More... | |
struct | SysLink_MemEntry_Block_tag |
Structure for memEntry block for one core. More... | |
struct | SysLink_MemoryMap_tag |
Structure for memEntry block for one core. More... | |
Defines | |
#define | IPC_BUFFER_ALIGN(x, y) (UInt32)((UInt32)((x + y - 1) / y) * y) |
#define | SYSLINK_MAX_MEMENTRIES 10 |
Signifies maximum number of mem entries for each core for one platform. | |
#define | SYSLINK_MAX_NAMELENGTH 32 |
Max name length. | |
#define | SysLink_MASTERKNLVIRT (SysLink_MapMask)(1 << 0) |
Kernel Virtual address on master processor. | |
#define | SysLink_MASTERUSRVIRT (SysLink_MapMask)(1 << 1) |
User Virtual address on master processor. | |
#define | SysLink_SLAVEVIRT (SysLink_MapMask)(1 << 2) |
Virtual address on slave processor. | |
Typedefs | |
typedef UInt32 | SysLink_MapMask |
typedef enum SysLink_NotifyType_tag | SysLink_NotifyType |
Enumeration of Client notifyMgr notification types. | |
typedef struct SysLink_MemEntry_tag | SysLink_MemEntry |
Structure for memEntry. | |
typedef struct SysLink_MemEntry_Block_tag | SysLink_MemEntry_Block |
Structure for memEntry block for one core. | |
typedef struct SysLink_MemoryMap_tag | SysLink_MemoryMap |
Structure for memEntry block for one core. | |
Enumerations | |
enum | SysLink_NotifyType_tag { SysLink_NOTIFICATION_NONE = 0, SysLink_NOTIFICATION_ALWAYS = 1, SysLink_NOTIFICATION_ONCE = 2, SysLink_NOTIFICATION_HDWRFIFO_ALWAYS = 3, SysLink_NOTIFICATION_HDWRFIFO_ONCE = 4 } |
Enumeration of Client notifyMgr notification types. More... | |
Functions | |
Void | SysLink_setup (Void) |
Function to initialize SysLink. | |
Void | SysLink_destroy (Void) |
Function to finalize SysLink. | |
Variables | |
String | SysLink_params |
============================================================================ IPC_BUFFER_ALIGN
Macro to align a number. x: The number to be aligned y: The value that the number should be aligned to. ============================================================================
#define SYSLINK_MAX_MEMENTRIES 10 |
Signifies maximum number of mem entries for each core for one platform.
#define SYSLINK_MAX_NAMELENGTH 32 |
Max name length.
#define SysLink_MASTERKNLVIRT (SysLink_MapMask)(1 << 0) |
Kernel Virtual address on master processor.
#define SysLink_MASTERUSRVIRT (SysLink_MapMask)(1 << 1) |
User Virtual address on master processor.
#define SysLink_SLAVEVIRT (SysLink_MapMask)(1 << 2) |
Virtual address on slave processor.
typedef UInt32 SysLink_MapMask |
typedef enum SysLink_NotifyType_tag SysLink_NotifyType |
Enumeration of Client notifyMgr notification types.
typedef struct SysLink_MemEntry_tag SysLink_MemEntry |
Structure for memEntry.
typedef struct SysLink_MemEntry_Block_tag SysLink_MemEntry_Block |
Structure for memEntry block for one core.
typedef struct SysLink_MemoryMap_tag SysLink_MemoryMap |
Structure for memEntry block for one core.
Enumeration of Client notifyMgr notification types.
Function to initialize SysLink.
This function must be called in every user process before making calls to any other SysLink APIs.
Function to finalize SysLink.
This function must be called in every user process at the end after all usage of SysLink in that process is complete.