Structure for memEntry. More...
#include <SysLink.h>
Data Fields | |
UInt32 | slaveVirtAddr |
UInt32 | masterPhysAddr |
UInt32 | size |
SysLink_MapMask | mapMask |
Bool | map |
Bool | isCached |
Bool | isValid |
Structure for memEntry.
Virtual address
Physical address
Size of the entry
Used for entries for which map is TRUE
Flag indicating whether this region should be mapped to the slave MMU.
Flag indicating whether the cache is enabled for this region
Specifies if the memEntry is valid