Structure defining parameter structure for ListMP_create(). More...
#include <ListMP.h>
Data Fields | |
GateMP_Handle | gate |
String | name |
UInt16 | regionId |
Structure defining parameter structure for ListMP_create().
GateMP instance for critical region management of shared memory
Using the default value of NULL will result in use of the GateMP system gate for context protection.
Name of the instance
The name (if not NULL) must be unique among all ListMP instances in the entire system. When creating a new heap, it is necessary to supply an instance name.
The name does not have to be persistent. The supplied string is copied into persistent memory.
SharedRegion ID.
The ID corresponding to the index of the shared region in which this shared instance is to be placed. This is used in create() only when name is not null.