Structure to frame buffer informantion in frame header. More...
#include <FrameQDefs.h>
Data Fields | |
UInt32 | bufPtr |
UInt32 | bufSize |
UInt32 | startOffset |
UInt32 | validSize |
UInt32 | pixelFormat |
UInt32 | height |
UInt32 | width |
UInt32 | stride |
Structure to frame buffer informantion in frame header.
Pointer to the frame buffer.
Size of the buffer.
Start offset in the buffer from where valid data starts.
Valid size in the buffer from the zeroth offset in the frame buffer