This structure defines information about memory regions mapped by the ProcMgr module. More...
#include <ProcMgr.h>
Data Fields | |
UInt32 | addr [ProcMgr_AddrType_EndValue] |
UInt32 | size |
Bool | isCached |
Bool | isMapped |
ProcMgr_MapMask | mapMask |
UInt16 | refCount |
This structure defines information about memory regions mapped by the ProcMgr module.
UInt32 ProcMgr_AddrInfo_tag::addr[ProcMgr_AddrType_EndValue] |
Addresses for each type of address space
Size of the memory region in bytes
Region cached?
tells whether the entry is mapped
map type needed for default entries in translation table
To ensure entry is added/removed only in appropriate map/unmap