![]() |
![]() |
Structure of the base frame header. FrameQ maintains list of frames to be retrieved by FrameQ reader client. Application is expected to use Helper API to extract fileds and exteneded header pointer. More...
#include <FrameQDefs.h>
Structure of the base frame header. FrameQ maintains list of frames to be retrieved by FrameQ reader client. Application is expected to use Helper API to extract fileds and exteneded header pointer.
reserverd field
reserverd field
Size of the base frame header.
Size of the frame header(total size of base header and extended header).
Denotes the FrameQBufMgr Id from which frame is allocated.
Free quque No from which frame is allocated in FrameQBufMgr.
Number of framebuffers in frame.
Information of Frame buffers. see Frame_FrameBufInfo