module xdc.runtime.Timestamp |
![](../../Arrow_left.png) |
![](../../Arrow_up.png) |
![](../../Arrow_right.png) |
Timestamp services
#include <xdc/runtime/Timestamp.h>
Functions common to all ITimestampClient modules |
Bits32 | |
Void | |
Void | |
Functions common to all target modules |
|
|
DETAILS
This module provides
xdc.runtime.ITimestampClient APIs for
the xdc Runtime Support Library. Calls to these APIs are forwarded
to a platform specific
xdc.runtime.ITimestampProvider
implementation.
A user can attach their own ITimestampProvider module
using the following config file command:
xdc.runtime.Timestamp.SupportProxy = xdc.useModule("usersTimestampProvider");
If no such
SupportProxy initialization is done,
the
xdc.runtime.TimestampNull ITimestampProvider implementation,
which provides null stubs for the APIs, will be attached by default.
If the user is developing code using CCS, the
xdc.runtime.TimestampStd
ITimestampProvider implementation, which uses the ANSI C clock()
function, may provide a satisfactory timestamp source (remember to
enable the profile clock in CCS).
To use the TimestampStd implementation, add the following to
your config script:
xdc.runtime.Timestamp.SupportProxy = xdc.useModule("xdc.runtime.TimestampStd");
Timestamp_get32() // module-wide |
![](../../Arrow_up.png) |
Return a 32-bit timestamp
Bits32 Timestamp_get32();
RETURNS
Returns a 32-bit timestamp value.
Use
getFreq to convert this value into units of real time.
SEE
Timestamp_get64() // module-wide |
![](../../Arrow_up.png) |
Return a 64-bit timestamp
ARGUMENTS
result
pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit
wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the
hi field of
result is always set to 0; see
xdc.runtime.Types.Timestamp64. So, it is possible for
the
lo field to wrap around without any change to the
hi field.
Use
getFreq to convert this value into units of real
time.
SEE
Timestamp_getFreq() // module-wide |
![](../../Arrow_up.png) |
Get the timestamp timer's frequency (in Hz)
ARGUMENTS
freq
pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit
wide frequency value where the timer's frequency (in Hz)
is written; see
xdc.runtime.Types.FreqHz.
This function provides a way of converting timestamp
values into units of real time.
SEE
Module-Wide Built-Ins |
![](../../Arrow_up.png) |
// Get this module's unique id
Bool Timestamp_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Timestamp_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Timestamp_Module_getMask();
// Returns the diagnostics mask for this module
Void Timestamp_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var Timestamp = xdc.useModule('xdc.runtime.Timestamp');
local proxy modules
module-wide config parameters
generated on Fri, 07 Sep 2012 20:20:19 GMT