const Timer_ANY |
![](../../../../Arrow_up.png) |
Const used to specify any timer
#define Timer_ANY (UInt)~0
const Timer_MAX_PERIOD |
![](../../../../Arrow_up.png) |
Max value of Timer period for PeriodType_COUNTS
#define Timer_MAX_PERIOD (UInt)0xffffffff
const Timer_NUM_TIMER_DEVICES |
![](../../../../Arrow_up.png) |
Number of timer peripherals on chip
#define Timer_NUM_TIMER_DEVICES (Int)3
enum Timer_PeriodType |
![](../../../../Arrow_up.png) |
Timer period units
typedef enum Timer_PeriodType {
Timer_PeriodType_MICROSECS,
// period in microsecs
Timer_PeriodType_COUNTS
// period in counts
} Timer_PeriodType;
VALUES
PeriodType_MICROSECS
Period value is in microseconds.
PeriodType_COUNTS
Period value is in counts.
enum Timer_RunMode |
![](../../../../Arrow_up.png) |
Timer Run Modes
typedef enum Timer_RunMode {
Timer_RunMode_CONTINUOUS,
// periodic and continuous
Timer_RunMode_ONESHOT,
// one-shot
Timer_RunMode_DYNAMIC
// dynamically reprogrammed (available on subset of devices)
} Timer_RunMode;
VALUES
RunMode_CONTINUOUS
Timer is periodic and runs continuously.
RunMode_ONESHOT
Timer runs for a single period value and stops.
RunMode_DYNAMIC
Timer is dynamically reprogrammed for the next required tick.
enum Timer_StartMode |
![](../../../../Arrow_up.png) |
Timer Start Modes
typedef enum Timer_StartMode {
Timer_StartMode_AUTO,
// timer starts automatically
Timer_StartMode_USER
// timer will be started by user
} Timer_StartMode;
VALUES
StartMode_AUTO
Statically created/constructed Timers will be started in BIOS_start().
Dynamically created Timers will start at create() time. This includes
timers created before BIOS_start().
StartMode_USER
Timer will be started by the user using start().
enum Timer_Status |
![](../../../../Arrow_up.png) |
Timer Status
typedef enum Timer_Status {
Timer_Status_INUSE,
// timer in use
Timer_Status_FREE
// timer is free
} Timer_Status;
VALUES
Status_INUSE
Timer is in use. A timer is marked in use from the time it gets
created to the time it gets deleted.
Status_FREE
Timer is free and can be acquired using create.
typedef Timer_FuncPtr |
![](../../../../Arrow_up.png) |
Timer tick function prototype
typedef Void (*Timer_FuncPtr)(UArg);
struct Timer_EmulationMode |
![](../../../../Arrow_up.png) |
Timer Emulation Mode
typedef struct Timer_EmulationMode {
UInt free;
// At sw breakpoint, stop or free-run the timer
UInt soft;
// At sw breakpoint, hard stop or run down timer
} Timer_EmulationMode;
config Timer_A_invalidHwiMask // module-wide |
![](../../../../Arrow_up.png) |
Assert raised in Timer_create when Hwi Params does not mask 'self'
extern const Assert_Id Timer_A_invalidHwiMask;
DETAILS
This is not allowed because the timers on this platform do not
inherently support one-shot mode. Instead, a stub is used to stop the
timer, so it is important that the timer interrupt not occur again
before the stub has stopped the timer.
config Timer_A_invalidRunMode // module-wide |
![](../../../../Arrow_up.png) |
Assert raised in Timer_create if an invalid RunMode is requested
extern const Assert_Id Timer_A_invalidRunMode;
config Timer_A_invalidTimer // module-wide |
![](../../../../Arrow_up.png) |
Assert raised in Timer_create when timer id specified is not supported
config Timer_E_cannotSupport // module-wide |
![](../../../../Arrow_up.png) |
Assert raised when period requested is not supported
extern const Assert_Id Timer_E_cannotSupport;
config Timer_E_notAvailable // module-wide |
![](../../../../Arrow_up.png) |
Error raised in Timer_create when timer requested is in use
extern const Error_Id Timer_E_notAvailable;
config Timer_anyMask // module-wide |
![](../../../../Arrow_up.png) |
Available mask to be used when select = Timer_ANY
extern const UInt Timer_anyMask;
Timer_getNumTimers() // module-wide |
![](../../../../Arrow_up.png) |
Returns number of timer peripherals on the platform
UInt Timer_getNumTimers();
RETURNS
Number of timer peripherals.
Timer_getStatus() // module-wide |
![](../../../../Arrow_up.png) |
Returns timer status (free or in use)
RETURNS
timer status
Module-Wide Built-Ins |
![](../../../../Arrow_up.png) |
// Get this module's unique id
Bool Timer_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Timer_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Timer_Module_getMask();
// Returns the diagnostics mask for this module
Void Timer_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
![](../../../../Arrow_up.png) |
typedef struct Timer_Object Timer_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct Timer_Struct Timer_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
![](../../../../Arrow_up.png) |
typedef struct Timer_Params {
// Instance config-params structure
// Common per-instance configs
UArg arg;
// Argument for tick function
// Initial timer emulation mode. Default hard stop
// Timer frequency
// Parameters for the Hwi object created for the Timer ISR
UInt32 period;
// Period of a tick
// Period type
UInt16 prescale;
// Prescale factor
// Timer run mode
// Timer start mode
} Timer_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config Timer_arg // instance |
![](../../../../Arrow_up.png) |
Argument for tick function
DETAILS
Default is null.
config Timer_emulationModeInit // instance |
![](../../../../Arrow_up.png) |
Initial timer emulation mode. Default hard stop
DETAILS
Determines timer state at a software breakpoint. If 'free' is 1, the
timer will continue to run, and the value of 'soft' doesn't matter.
When 'free' is 0 and 'soft' is 1, the timer runs down to 0 then stops.
When 'free' is 0 and 'soft' is 0, the timer halts.
FREE SOFT
0 0 Stop after next timer decrement. (Hard stop)
0 1 Stop after timer runs down to 0. (Soft stop)
1 x Continue running the timer.
config Timer_extFreq // instance |
![](../../../../Arrow_up.png) |
Timer frequency
DETAILS
This parameter is meaningfull only on platforms where the timer's
input clock can be changed. If value is left at zero, then input clock
to the timer clock is assumed.
This value is used to convert timer ticks to real time units; seconds,
milliseconds, etc.
config Timer_hwiParams // instance |
![](../../../../Arrow_up.png) |
Parameters for the Hwi object created for the Timer ISR
DETAILS
The mask setting for the Hwi object should include SELF to prevent
nested timer interrupts.
config Timer_period // instance |
![](../../../../Arrow_up.png) |
Period of a tick
DETAILS
The period can be specified in timer counts or microseconds
and its default value is 0.
The implementation of ITimer will support a period of UInt32
timer counts and use pre-scalars if necessary.
config Timer_periodType // instance |
![](../../../../Arrow_up.png) |
Period type
DETAILS
Default is PeriodType_MICROSECS
config Timer_prescale // instance |
![](../../../../Arrow_up.png) |
Prescale factor
DETAILS
The prescale factor determines the length of a timer tick.
If a prescale of 10 is specified, a timer tick will occur
every 11 cycles.
If the timer is used as a counter, the prescale factor determines
the period between counts. Otherwise, the prescale factor can be used
to achieve longer timer periods: with a prescale specified, the actual
period is (period * prescale+1).
config Timer_runMode // instance |
![](../../../../Arrow_up.png) |
Timer run mode
DETAILS
config Timer_startMode // instance |
![](../../../../Arrow_up.png) |
Timer start mode
DETAILS
Instance Creation |
![](../../../../Arrow_up.png) |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
id
Timer id ranging from 0 to a platform specific value,
or ANY
tickFxn
function that runs upon timer expiry.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
Create could fail if timer peripheral is unavailable. To
request any available timer use
ANY as the id.
TimerId's are logical ids. The family-specific implementations
map the ids to physical peripherals.
Instance Deletion |
![](../../../../Arrow_up.png) |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
Timer_getCount() // instance |
![](../../../../Arrow_up.png) |
Returns the number of counts that have passed
ARGUMENTS
handle
handle of a previously-created Timer instance object
RETURNS
timer counter value
timer counts, counting upward from 0
DETAILS
The 28x timer counts downward from the period to 0, but getCount
subtracts the timer counter value from the period so that getCount
counts upward instead of downward.
Timer_getFreq() // instance |
![](../../../../Arrow_up.png) |
Return timer frequency in Hz
ARGUMENTS
handle
handle of a previously-created Timer instance object
freq
frequency in Hz
DETAILS
This is the effective frequency of the clock incrementing the timer
counter register after all scaling factors are taken into account.
(including pre-scalars).
Timer_getFunc() // instance |
![](../../../../Arrow_up.png) |
Get Timer function and arg
ARGUMENTS
handle
handle of a previously-created Timer instance object
arg
pointer for returning Timer's function argument
RETURNS
Timer's function
Timer_getPeriod() // instance |
![](../../../../Arrow_up.png) |
Get timer period in timer counts
ARGUMENTS
handle
handle of a previously-created Timer instance object
RETURNS
period in timer counts
Timer_getPrescale() // instance |
![](../../../../Arrow_up.png) |
Get timer prescale value
ARGUMENTS
handle
handle of a previously-created Timer instance object
RETURNS
prescale value
DETAILS
This is not the prescale count, but the period of the prescalar.
Timer_getPrescaleCount() // instance |
![](../../../../Arrow_up.png) |
Reads timer prescale counter
ARGUMENTS
handle
handle of a previously-created Timer instance object
RETURNS
prescale counter, counting upward from 0
DETAILS
The prescale counter counts down from prescale to 0, but
getPrescaleCount subtracts the counter value from the period so that
this function counts upward instead of downward.
Timer_setFunc() // instance |
![](../../../../Arrow_up.png) |
Overwrite Timer function and arg
ARGUMENTS
handle
handle of a previously-created Timer instance object
fxn
pointer to function
arg
argument to function
DETAILS
Replaces a Timer object's tickFxn function originally
provided in
create.
Timer_setPeriod() // instance |
![](../../../../Arrow_up.png) |
Set timer period specified in timer counts
ARGUMENTS
handle
handle of a previously-created Timer instance object
period
period in timer counts
DETAILS
Timer_setPeriod() invokes Timer_stop() prior to setting the period
and leaves the timer in the stopped state.
To dynamically change the period of a timer you must
protect against re-entrancy by disabling interrupts.
Use the following call sequence to guarantee proper results:
// disable interrupts if an interrupt could lead to
// another call to Timer_start().
key = Hwi_disable();
Timer_setPeriod(period);
Timer_start();
Hwi_restore(key);
ITimer implementation must support UInt32 and use pre-scalars whenever
necessary
SIDE EFFECTS
Calls Timer_stop(), and disables the timer's interrupt.
Timer_setPeriodMicroSecs() // instance |
![](../../../../Arrow_up.png) |
Set timer period specified in microseconds
Bool Timer_setPeriodMicroSecs(
Timer_Handle handle,
UInt32 microsecs);
ARGUMENTS
handle
handle of a previously-created Timer instance object
period
period in microseconds
DETAILS
A best-effort method will be used to set the period register.
There might be a slight rounding error based on resolution of timer
period register. If the timer frequency cannot support the requested
period, i.e. the timer period register cannot support the requested
period, then this function returns false.
Timer_setPeriodMicroSecs() invokes Timer_stop() prior to setting
the period and leaves the timer in the stopped state.
To dynamically change the period of a timer you must
protect against re-entrancy by disabling interrupts.
Use the following call sequence to guarantee proper results:
// disable interrupts if an interrupt could lead to
// another call to Timer_start().
key = Hwi_disable();
Timer_setPeriodMicroSecs(period);
Timer_start();
Hwi_restore(key);
Timer_setPrescale() // instance |
![](../../../../Arrow_up.png) |
Set timer prescale value
Void Timer_setPrescale(
Timer_Handle handle,
UInt16 preScalar);
ARGUMENTS
handle
handle of a previously-created Timer instance object
preScalar
The value to set the prescale period to.
DETAILS
This function sets the value of the prescalar, and will also reload
the timer counter and prescale registers.
The prescalar decrements with each timer clock source cycle until it
reaches zero, then the timer's count is decremented by one. The
prescalar has the effect of setting the rate of the timer tick.
Timer_start() // instance |
![](../../../../Arrow_up.png) |
Reload and start the timer
ARGUMENTS
handle
handle of a previously-created Timer instance object
DETAILS
Thread safety must be observed when using the
start
and
stop APIs to avoid possible miss-
configuration of the timers and unintended behaviors.
To protect against re-entrancy, surround the start/stop invocations
with
Hwi_disable() and
Hwi_restore() calls:
// disable interrupts if an interrupt could lead to
// another call to Timer_start().
key = Hwi_disable();
Timer_stop();
...
Timer_start();
Hwi_restore(key);
SIDE EFFECTS
Enables the timer's interrupt.
Timer_stop() // instance |
![](../../../../Arrow_up.png) |
Stop the timer
ARGUMENTS
handle
handle of a previously-created Timer instance object
DETAILS
Thread safety must be observed when using the
start
and
stop APIs to avoid possible miss-
configuration of the timers and unintended behaviors.
To protect against re-entrancy, surround the start/stop invocations
with
Hwi_disable() and
Hwi_restore() calls:
// disable interrupts if an interrupt could lead to
// another call to Timer_start().
key = Hwi_disable();
Timer_stop();
...
Timer_start();
Hwi_restore(key);
SIDE EFFECTS
Disables the timer's interrupt.
Instance Convertors |
![](../../../../Arrow_up.png) |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
![](../../../../Arrow_up.png) |
Int Timer_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
const Timer.ANY |
![](../../../../Arrow_up.png) |
Const used to specify any timer
XDCscript usage |
meta-domain |
C SYNOPSIS
const Timer.MAX_PERIOD |
![](../../../../Arrow_up.png) |
Max value of Timer period for PeriodType_COUNTS
XDCscript usage |
meta-domain |
const Timer.MAX_PERIOD = 0xffffffff;
C SYNOPSIS
const Timer.NUM_TIMER_DEVICES |
![](../../../../Arrow_up.png) |
Number of timer peripherals on chip
XDCscript usage |
meta-domain |
const Timer.NUM_TIMER_DEVICES = 3;
C SYNOPSIS
enum Timer.PeriodType |
![](../../../../Arrow_up.png) |
Timer period units
XDCscript usage |
meta-domain |
values of type Timer.PeriodType
const Timer.PeriodType_MICROSECS;
// period in microsecs
const Timer.PeriodType_COUNTS;
// period in counts
VALUES
PeriodType_MICROSECS
Period value is in microseconds.
PeriodType_COUNTS
Period value is in counts.
C SYNOPSIS
enum Timer.RunMode |
![](../../../../Arrow_up.png) |
Timer Run Modes
XDCscript usage |
meta-domain |
values of type Timer.RunMode
const Timer.RunMode_CONTINUOUS;
// periodic and continuous
const Timer.RunMode_ONESHOT;
// one-shot
const Timer.RunMode_DYNAMIC;
// dynamically reprogrammed (available on subset of devices)
VALUES
RunMode_CONTINUOUS
Timer is periodic and runs continuously.
RunMode_ONESHOT
Timer runs for a single period value and stops.
RunMode_DYNAMIC
Timer is dynamically reprogrammed for the next required tick.
C SYNOPSIS
enum Timer.StartMode |
![](../../../../Arrow_up.png) |
Timer Start Modes
XDCscript usage |
meta-domain |
values of type Timer.StartMode
const Timer.StartMode_AUTO;
// timer starts automatically
const Timer.StartMode_USER;
// timer will be started by user
VALUES
StartMode_AUTO
Statically created/constructed Timers will be started in BIOS_start().
Dynamically created Timers will start at create() time. This includes
timers created before BIOS_start().
StartMode_USER
Timer will be started by the user using start().
C SYNOPSIS
enum Timer.Status |
![](../../../../Arrow_up.png) |
Timer Status
XDCscript usage |
meta-domain |
values of type Timer.Status
const Timer.Status_INUSE;
// timer in use
const Timer.Status_FREE;
// timer is free
VALUES
Status_INUSE
Timer is in use. A timer is marked in use from the time it gets
created to the time it gets deleted.
Status_FREE
Timer is free and can be acquired using create.
C SYNOPSIS
struct Timer.EmulationMode |
![](../../../../Arrow_up.png) |
Timer Emulation Mode
XDCscript usage |
meta-domain |
var obj = new Timer.EmulationMode;
obj.free = UInt ...
// At sw breakpoint, stop or free-run the timer
obj.soft = UInt ...
// At sw breakpoint, hard stop or run down timer
C SYNOPSIS
config Timer.A_invalidHwiMask // module-wide |
![](../../../../Arrow_up.png) |
Assert raised in Timer_create when Hwi Params does not mask 'self'
XDCscript usage |
meta-domain |
msg: "A_InvalidMask: Mask in hwiParams cannot enable self"
};
DETAILS
This is not allowed because the timers on this platform do not
inherently support one-shot mode. Instead, a stub is used to stop the
timer, so it is important that the timer interrupt not occur again
before the stub has stopped the timer.
C SYNOPSIS
config Timer.A_invalidRunMode // module-wide |
![](../../../../Arrow_up.png) |
Assert raised in Timer_create if an invalid RunMode is requested
XDCscript usage |
meta-domain |
msg: "A_invalidRunMode: Invalid RunMode"
};
C SYNOPSIS
config Timer.A_invalidTimer // module-wide |
![](../../../../Arrow_up.png) |
Assert raised in Timer_create when timer id specified is not supported
XDCscript usage |
meta-domain |
msg: "A_invalidTimer: Timer id must be 0-2"
};
C SYNOPSIS
config Timer.E_cannotSupport // module-wide |
![](../../../../Arrow_up.png) |
Assert raised when period requested is not supported
XDCscript usage |
meta-domain |
msg: "E_cannotSupport: Timer cannot support requested period"
};
C SYNOPSIS
config Timer.E_notAvailable // module-wide |
![](../../../../Arrow_up.png) |
Error raised in Timer_create when timer requested is in use
XDCscript usage |
meta-domain |
msg: "E_notAvailable: Timer not available %d"
};
C SYNOPSIS
config Timer.anyMask // module-wide |
![](../../../../Arrow_up.png) |
Available mask to be used when select = Timer_ANY
XDCscript usage |
meta-domain |
Timer.anyMask = UInt 0x7;
C SYNOPSIS
metaonly config Timer.common$ // module-wide |
![](../../../../Arrow_up.png) |
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
Instance Config Parameters |
![](../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new Timer.Params;
// Instance config-params object
params.arg = UArg null;
// Argument for tick function
// Initial timer emulation mode. Default hard stop
free: 0,
soft: 0
};
// Timer frequency
lo: 0,
hi: 0
};
// Parameters for the Hwi object created for the Timer ISR
params.period = UInt32 0;
// Period of a tick
// Period type
params.prescale = UInt16 0;
// Prescale factor
// Timer run mode
// Timer start mode
config Timer.arg // instance |
![](../../../../Arrow_up.png) |
Argument for tick function
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
params.arg = UArg null;
DETAILS
Default is null.
C SYNOPSIS
config Timer.emulationModeInit // instance |
![](../../../../Arrow_up.png) |
Initial timer emulation mode. Default hard stop
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
free: 0,
soft: 0
};
DETAILS
Determines timer state at a software breakpoint. If 'free' is 1, the
timer will continue to run, and the value of 'soft' doesn't matter.
When 'free' is 0 and 'soft' is 1, the timer runs down to 0 then stops.
When 'free' is 0 and 'soft' is 0, the timer halts.
FREE SOFT
0 0 Stop after next timer decrement. (Hard stop)
0 1 Stop after timer runs down to 0. (Soft stop)
1 x Continue running the timer.
C SYNOPSIS
config Timer.extFreq // instance |
![](../../../../Arrow_up.png) |
Timer frequency
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
lo: 0,
hi: 0
};
DETAILS
This parameter is meaningfull only on platforms where the timer's
input clock can be changed. If value is left at zero, then input clock
to the timer clock is assumed.
This value is used to convert timer ticks to real time units; seconds,
milliseconds, etc.
C SYNOPSIS
config Timer.hwiParams // instance |
![](../../../../Arrow_up.png) |
Parameters for the Hwi object created for the Timer ISR
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
DETAILS
The mask setting for the Hwi object should include SELF to prevent
nested timer interrupts.
C SYNOPSIS
config Timer.period // instance |
![](../../../../Arrow_up.png) |
Period of a tick
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
params.period = UInt32 0;
DETAILS
The period can be specified in timer counts or microseconds
and its default value is 0.
The implementation of ITimer will support a period of UInt32
timer counts and use pre-scalars if necessary.
C SYNOPSIS
config Timer.periodType // instance |
![](../../../../Arrow_up.png) |
Period type
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
DETAILS
Default is PeriodType_MICROSECS
C SYNOPSIS
config Timer.prescale // instance |
![](../../../../Arrow_up.png) |
Prescale factor
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
params.prescale = UInt16 0;
DETAILS
The prescale factor determines the length of a timer tick.
If a prescale of 10 is specified, a timer tick will occur
every 11 cycles.
If the timer is used as a counter, the prescale factor determines
the period between counts. Otherwise, the prescale factor can be used
to achieve longer timer periods: with a prescale specified, the actual
period is (period * prescale+1).
C SYNOPSIS
config Timer.runMode // instance |
![](../../../../Arrow_up.png) |
Timer run mode
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
DETAILS
C SYNOPSIS
config Timer.startMode // instance |
![](../../../../Arrow_up.png) |
Timer start mode
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
DETAILS
C SYNOPSIS
Instance Creation |
![](../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params =
new Timer.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = Timer.create(Int id, Void(*)(UArg) tickFxn, params);
// Create an instance-object
ARGUMENTS
id
Timer id ranging from 0 to a platform specific value,
or ANY
tickFxn
function that runs upon timer expiry.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
Create could fail if timer peripheral is unavailable. To
request any available timer use
ANY as the id.
TimerId's are logical ids. The family-specific implementations
map the ids to physical peripherals.