module ti.sysbios.family.c64p.omap3430.Wugen

Wugen Module

Unconstrained Functions All functions [ more ... ]
C synopsis target-domain sourced in ti/sysbios/family/c64p/omap3430/Wugen.xdc
#include <ti/sysbios/family/c64p/omap3430/Wugen.h>
Functions
Void 
Void 
Void 
Void 
Void 
Void 
Void 
Functions common to all target modules
 
DETAILS
Unconstrained Functions All functions

Calling Context

Function Hwi Swi Task Main Startup
applyMasks Y Y Y Y Y
disableDma Y Y Y Y Y
disableEvent Y Y Y Y Y
enableDma Y Y Y Y Y
enableEvent Y Y Y Y Y
getMasks Y Y Y Y Y
ierToMasks Y Y Y Y Y
Definitions:
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • In your module startup after this module is started (e.g. Mod_Module_startupDone() returns TRUE).
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.
    • In your module startup before this module is started (e.g. Mod_Module_startupDone() returns FALSE).
 
Wugen_applyMasks()  // module-wide

This function takes an array of 3 integers and applies the specified mask to the WUGEN interrupt mask registers. If the bit in the mask is enabled, the corresponding interrupt in the WUGEN will be blocked

C synopsis target-domain
Void Wugen_applyMasks(UInt32 mask[]);
 
ARGUMENTS
mask — array of three integers for applying to the WUGEN interrupt mask register. First mask consists of IRQ 0-31 Second mask consists of IRQ 32-47 Third mask consists of DMA requests
 
Wugen_disableDma()  // module-wide

Disables the specified DMA source in the WUGEN

C synopsis target-domain
Void Wugen_disableDma(UInt dmaid);
 
ARGUMENTS
dmaid — the DMA id for a particular EDMA source.
 
Wugen_disableEvent()  // module-wide

Disables the specified interrupt event source in the WUGEN

C synopsis target-domain
Void Wugen_disableEvent(UInt eventid);
 
ARGUMENTS
eventid — the event number of an interrupt source
 
Wugen_enableDma()  // module-wide

Enables the specified DMA source in the WUGEN

C synopsis target-domain
Void Wugen_enableDma(UInt dmaid);
 
ARGUMENTS
dmaid — the DMA id for a particular EDMA source.
 
Wugen_enableEvent()  // module-wide

Enables the specified interrupt event source in the WUGEN

C synopsis target-domain
Void Wugen_enableEvent(UInt eventid);
 
ARGUMENTS
eventid — the event number of an interrupt source
 
Wugen_getMasks()  // module-wide

This function returns the WUGEN interrupt mask registers

C synopsis target-domain
Void Wugen_getMasks(UInt32 mask[]);
 
ARGUMENTS
mask — array of three integers used to return the WUGEN interrupt mask registers First mask consists of IRQ 0-31 Second mask consists of IRQ 32-47 Third mask consists of DMA requests
 
Wugen_ierToMasks()  // module-wide

Compute the WUGEN masks needed to allow the interrupts set in the IER register to propagate through the WUGEN. This function does not enable external DMA requests. You must set these explicitly to configure a DMA request as a wakeup event

C synopsis target-domain
Void Wugen_ierToMasks(UInt32 mask[]);
 
ARGUMENTS
mask — array of three integers for returning WUGEN masks. First mask consists of IRQ 0-31 Second mask consists of IRQ 32-47 Third mask consists of DMA requests
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId Wugen_Module_id();
// Get this module's unique id
 
Bool Wugen_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle Wugen_Module_heap();
// The heap from which this module allocates memory
 
Bool Wugen_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 Wugen_Module_getMask();
// Returns the diagnostics mask for this module
 
Void Wugen_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
XDCscript usage meta-domain sourced in ti/sysbios/family/c64p/omap3430/Wugen.xdc
var Wugen = xdc.useModule('ti.sysbios.family.c64p.omap3430.Wugen');
module-wide config parameters
 
 
metaonly config Wugen.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
Wugen.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Thu, 01 Mar 2012 16:57:11 GMT