metaonly module ti.bios.GIO

GIO Manager

This module aids in the creation of GIO devices. [ more ... ]
XDCspec summary sourced in ti/bios/GIO.xdc
metaonly module GIO {  ...
XDCscript usage meta-domain
XDCspec declarations sourced in ti/bios/GIO.xdc
package ti.bios;
 
metaonly module GIO {
module-wide config parameters
}
DETAILS
This module aids in the creation of GIO devices.
legacy module to support BIOS 5.x, see BIOS 5.x docs for more info
 
config GIO.CREATEFXN  // module-wide

The function the GIO module should use to create a sync object

XDCscript usage meta-domain
GIO.CREATEFXN = String "SEM_create";
 
 
config GIO.DELETEFXN  // module-wide

The function the GIO module should use to delete the sync object

XDCscript usage meta-domain
GIO.DELETEFXN = String "SEM_delete";
 
 
config GIO.ENABLEGIO  // module-wide

Set this property to true to enable use of the GIO module

XDCscript usage meta-domain
GIO.ENABLEGIO = Bool false;
 
 
config GIO.PENDFXN  // module-wide

The function the GIO module should use to pend on a sync object

XDCscript usage meta-domain
GIO.PENDFXN = String "SEM_pend";
 
 
config GIO.POSTFXN  // module-wide

The function the GIO module should use to post a sync object

XDCscript usage meta-domain
GIO.POSTFXN = String "SEM_post";
 
generated on Fri, 16 Oct 2009 20:56:44 GMT