metaonly interface ti.catalog.msp430.peripherals.adc.IADC |
|
|
MSP430 Analog to Digital Converter Interface
metaonly interface IADC { ...
instance: ...
module-wide constants & types
};
};
module-wide functions
instance:
per-instance config parameters
per-instance creation
}
typedef IADC.IPeripheralArray |
|
typedef IADC.StringArray |
|
typedef String StringArray[];
struct IADC.ForceSetDefaultRegister_t |
|
Force Set Default Register
metaonly struct ForceSetDefaultRegister_t {
String register;
Bool regForceSet;
};
DETAILS
Type to store if each register needs to be forced initialized
even if the register is in default state.
SEE
struct IADC.regIntVect_t |
|
Interrupt vector description
metaonly struct regIntVect_t {
String registerName;
String registerDescription;
String isrToggleString;
String priorityName;
Bool interruptEnable;
Bool interruptHandler;
Int priority;
};
DETAILS
Type to describe a single interrupt vector pin and all its possible
configurations.
SEE
IADC.getAll() // module-wide |
|
Find all peripherals of a certain type
DETAILS
The type of the peripherals returned is defined by the type of the
caller.
RETURNS
Returns an array of IPeripheral instances
IADC.getRegisters() // module-wide |
|
Find all registers defined by the peripheral
RETURNS
Returns an array of register names
config IADC.name // instance |
|
Specific peripheral name given by the device
DETAILS
Devices can have more than one peripheral of the same type. In such
cases, device data sheets give different names to the instances of a
same peripheral. For example, the name for a timer module could be
TimerA3, and a device that has two such timers can name them TA0
and TA1.
config IADC.owner // instance |
|
String specifying the entity that manages the peripheral
Instance Creation |
|
// Create an instance-object
generated on Tue, 16 Oct 2012 23:17:45 GMT