metaonly module xdc.services.global.Trace |
![](../../../Arrow_left.png) |
![](../../../Arrow_up.png) |
Trace support
This module allows system integrators to selectively enable trace
statements, from within XDCscripts. Trace statements can be selected
based on the file (capsule) and the package in which they are located.
For example, trace statements from file
Mod.xs in package
myPkgs.pkgA'
can be enabled either with Trace.capsuleEnable(["myPkgs/pkgA/Mod"])
or
with Trace.packageEnable(["myPkgs.pkgA"])`.
[
more ... ]
var Trace = xdc.useModule('xdc.services.global.Trace');
module-wide config parameters
module-wide functions
DETAILS
This module allows system integrators to selectively enable trace
statements, from within XDCscripts. Trace statements can be selected
based on the file (capsule) and the package in which they are located.
For example, trace statements from file Mod.xs in package myPkgs.pkgA'
can be enabled either with Trace.capsuleEnable(["myPkgs/pkgA/Mod"]) or
with Trace.packageEnable(["myPkgs.pkgA"])`.
Trace statements can also belong to groups, strings defined by package
producers when they need to group related trace statements, distributed
across different modules and packages, into trace units that can be
disabled or enabled as a whole. If some of the trace statements from file
Mod.xs are tagged to belong to a group "init", the following will
activate them:
Trace.groupEnable(["init"]);
Each trace statement by default belongs to the group "all". To activate
all trace statements:
Trace.setLevel(2);
Trace.groupEnable(["all"]);
config Trace.packageLoad // module-wide |
![](../../../Arrow_up.png) |
Enable trace of loaded packages
XDCscript usage |
meta-domain |
Trace.packageLoad = Bool false;
DETAILS
This setting enables the messages related to loading packages.
If true, whenever a package is loaded, the following info is
displayed:
- name of a package loading another package
- name of the loaded package
- repository from which the package is being loaded
config Trace.useModule // module-wide |
![](../../../Arrow_up.png) |
Enable trace of used modules
XDCscript usage |
meta-domain |
Trace.useModule = Bool false;
DETAILS
This setting enables the messages that inform when the function
xdc.useModule() is invoked on a module, and when a module's
module$use function is invoked.
Trace.addSupergroup() // module-wide |
![](../../../Arrow_up.png) |
Add a group that contains other groups
XDCscript usage |
meta-domain |
Trace.addSupergroup(String supergroup, String[] subgroups) returns Void
ARGUMENTS
supergroup
name of the new group
subgroups
array of the existing trace groups
DETAILS
This function allows giving a name to an array of existing
trace groups.
Trace.capsuleEnable() // module-wide |
![](../../../Arrow_up.png) |
Enable trace output from selected capsules
XDCscript usage |
meta-domain |
Trace.capsuleEnable(String[] capsules) returns String[]
ARGUMENTS
capsules
array of capsule names
DETAILS
Capsules are either XDCscript files or Java source files. The
function parameter is treated as an array of JavaScript
regular expressions, therefore it can contain partial capsule
names.
If this function is invoked repeatedly, each new call replaces
the array of currently enabled capsules with the array supplied
as the parameter. The array of the currently enabled capsules is
returned. If the function is invoked with a zero-length array, it
returns the currently enabled capsules, but it also leaves them
active. Therefore, the sequence of calls that would add new
capsules instead of replacing the current ones is:
var current = Trace.capsuleEnable([]);
current[current.length++] = "pkg/ModA.xs";
current[current.length++] = "pkg/ModB.xs";
Trace.capsuleEnable(current);
To disable trace for all capsules, the function must be invoked
with an empty string as the only element of the array.
Trace.capsuleEnable([""]);
RETURN
array of currently enabled capsule names
Trace.groupEnable() // module-wide |
![](../../../Arrow_up.png) |
Enable trace output from selected groups
XDCscript usage |
meta-domain |
Trace.groupEnable(String[] groups) returns String[]
ARGUMENTS
groups
array of groups
DETAILS
A group is a string defined by package producers when they need to
group related trace statements, distributed across different
modules and packages, into trace units that can be disabled or
enabled as a whole. The function parameter is treated as an array
of JavaScript regular expressions, therefore it can contain partial
group names.
If this function is invoked repeatedly, each new call replaces
the array of currently enabled groups with the array supplied
as the parameter. The array of the currently enabled groups is
returned. If the function is invoked with a zero-length array, it
returns the currently enabled groups, but it also leaves them
active. Therefore, the sequence of calls that would add new groups
instead of replacing the current ones is:
var current = Trace.groupEnable([]);
current[current.length++] = "libPkgs";
Trace.groupEnable(current);
To disable trace for all groups, the function must be invoked
with an empty string as the only element of the array.
RETURN
array of currently enabled groups
Trace.packageEnable() // module-wide |
![](../../../Arrow_up.png) |
Enable trace output from selected packages
XDCscript usage |
meta-domain |
Trace.packageEnable(String[] packages) returns String[]
ARGUMENTS
packages
array of package names
DETAILS
Packages that can be enabled through this function are RTSC
packages and Java packages. The function parameter is treated as
an array of JavaScript regular expressions, therefore it can
contain partial package names.
If this function is invoked repeatedly, each new call replaces
the array of currently enabled packages with the array supplied
as the parameter. The array of the currently enabled packages is
returned. If the function is invoked with a zero-length array, it
returns the currently enabled packages, but it also leaves them
active. Therefore, the sequence of calls that would add new
packages instead of replacing the current ones is:
var current = Trace.packageEnable([]);
current[current.length++] = "ti.targets";
Trace.packageEnable(current);
To disable trace for all packages, the function must be invoked
with an empty string as the only element of the array.
Trace.packageEnable([""]);
RETURN
array of currently enabled package names
Trace.setLevel() // module-wide |
![](../../../Arrow_up.png) |
Set the verbosity level
XDCscript usage |
meta-domain |
Trace.setLevel(Int level) returns Int
DETAILS
This function limits trace output to trace statement tagged with
level equal or lower than this function's parameter. By default,
the verbosity level is set to 0, which is the least verbose level.
The most verbose level is 2.
generated on Thu, 27 Sep 2012 23:21:23 GMT