module xdc.runtime.knl.GateThread

Provides protection of critical sections across threads

This module provides services through its proxy IGateThreadSupport interface. It has a module wide config parameter Proxy which needs to be bound to an OS specific delegate before this module can be used. [ more ... ]
C synopsis target-domain sourced in xdc/runtime/knl/GateThread.xdc
#include <xdc/runtime/knl/GateThread.h>
Functions
Void
Void
Void
Void
Functions common to all IGateProvider modules
IArg 
Void 
Bool 
Functions common to all target instances
Functions common to all target modules
Defines
#define
#define
Typedefs
typedef struct
typedef struct
typedef struct
 
DETAILS
This module provides services through its proxy IGateThreadSupport interface. It has a module wide config parameter Proxy which needs to be bound to an OS specific delegate before this module can be used.
Here is an example showing how the proxy is bound to an BIOS 6.x specific delegate.
  var GateThread = xdc.useModule('xdc.runtime.knl.GateThread');
  GateThread.Proxy = 
      xdc.useModule('ti.sysbios.xdcruntime.GateThreadSupport');
Typically the package containing the delegates have a Settings module that will bind all xdc.runtime.knl proxies. The following example sets up all the xdc.runtime.knl proxies.
  xdc.useModule("ti.sysbios.xdcruntime.Settings");
 
const GateThread_Q_BLOCKING

Blocking quality

C synopsis target-domain
#define GateThread_Q_BLOCKING (Int)1
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
 
const GateThread_Q_PREEMPTING

Preempting quality

C synopsis target-domain
#define GateThread_Q_PREEMPTING (Int)2
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
 
GateThread_query()  // module-wide

Runtime test for a particular gate quality

C synopsis target-domain
Bool GateThread_query(Int qual);
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId GateThread_Module_id();
// Get this module's unique id
 
Bool GateThread_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle GateThread_Module_heap();
// The heap from which this module allocates memory
 
Bool GateThread_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 GateThread_Module_getMask();
// Returns the diagnostics mask for this module
 
Void GateThread_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct GateThread_Object GateThread_Object;
// Opaque internal representation of an instance object
 
typedef GateThread_Object *GateThread_Handle;
// Client reference to an instance object
 
typedef struct GateThread_Struct GateThread_Struct;
// Opaque client structure large enough to hold an instance object
 
GateThread_Handle GateThread_handle(GateThread_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
GateThread_Struct *GateThread_struct(GateThread_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct GateThread_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
} GateThread_Params;
 
Void GateThread_Params_init(GateThread_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
Instance Creation

C synopsis target-domain
GateThread_Handle GateThread_create(const GateThread_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void GateThread_construct(GateThread_Struct *structP, const GateThread_Params *params, Error_Block *eb);
// Initialize a new instance object inside the provided structure
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
Instance Deletion

C synopsis target-domain
Void GateThread_delete(GateThread_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void GateThread_destruct(GateThread_Struct *structP);
// Finalize the instance object inside the provided structure
 
GateThread_enter()  // instance

Enter this gate

C synopsis target-domain
IArg GateThread_enter(GateThread_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created GateThread instance object
DETAILS
Each gate provider can implement mutual exclusion using different algorithms; e.g., disabling all scheduling, disabling the scheduling of all threads below a specified "priority level", suspending the caller when the gate has been entered by another thread and re-enabling it when the the other thread leaves the gate. However, in all cases, after this method returns that caller has exclusive access to the data protected by this gate.
A thread may reenter a gate without blocking or failing.
RETURNS
Returns a "key" that is used to leave this gate; this value is used to restore thread preemption to the state that existed just prior to entering this gate.
 
GateThread_leave()  // instance

Leave this gate

C synopsis target-domain
Void GateThread_leave(GateThread_Handle handle, IArg key);
 
ARGUMENTS
handle — handle of a previously-created GateThread instance object
key — the value returned by a matching call to enter
DETAILS
This method is only called by threads that have previously entered this gate via enter. After this method returns, the caller must not access the data structure protected by this gate (unless the caller has entered the gate more than once and other calls to leave remain to balance the number of previous calls to enter).
Instance Convertors

C synopsis target-domain
IGateProvider_Handle GateThread_Handle_upCast(GateThread_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
GateThread_Handle GateThread_Handle_downCast(IGateProvider_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int GateThread_Object_count();
// The number of statically-created instance objects
 
GateThread_Handle GateThread_Object_get(GateThread_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
GateThread_Handle GateThread_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
GateThread_Handle GateThread_Object_next(GateThread_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle GateThread_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *GateThread_Handle_label(GateThread_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String GateThread_Handle_name(GateThread_Handle handle);
// The name of this instance object
 
XDCscript usage meta-domain sourced in xdc/runtime/knl/GateThread.xdc
var GateThread = xdc.useModule('xdc.runtime.knl.GateThread');
local proxy modules
        GateThread.Proxy.delegate$ = IGateThreadSupport.Module null
        GateThread.Proxy.abstractInstances$ = false
module-wide constants & types
module-wide config parameters
module-wide functions
per-instance config parameters
    var params = new GateThread.Params// Instance config-params object;
per-instance creation
    var inst = GateThread.create// Create an instance-object(params);
 
 
proxy GateThread.Proxy

Proxy that needs to be bound to an OS specific delegate

XDCscript usage meta-domain
GateThread.Proxy = IGateThreadSupport.Module null
// some delegate module inheriting the IGateThreadSupport interface
    GateThread.Proxy.delegate$ = IGateThreadSupport.Module null
    // explicit access to the currently bound delegate module
    GateThread.Proxy.abstractInstances$ = false
    // use indirect runtime function calls if true
 
 
const GateThread.Q_BLOCKING

Blocking quality

XDCscript usage meta-domain
const GateThread.Q_BLOCKING = 1;
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
C SYNOPSIS
 
const GateThread.Q_PREEMPTING

Preempting quality

XDCscript usage meta-domain
const GateThread.Q_PREEMPTING = 2;
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
C SYNOPSIS
 
metaonly config GateThread.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
GateThread.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly GateThread.queryMeta()  // module-wide

Configuration time test for a particular gate quality

XDCscript usage meta-domain
GateThread.queryMeta(Int qual) returns Bool
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
Instance Config Parameters

XDCscript usage meta-domain
var params = new GateThread.Params;
// Instance config-params object
Instance Creation

XDCscript usage meta-domain
var params = new GateThread.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = GateThread.create(params);
// Create an instance-object
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
generated on Thu, 27 Sep 2012 23:21:09 GMT