metaonly module ti.catalog.msp430.peripherals.clock.UCS

MSP430 Unified Clock System

XDCscript usage meta-domain sourced in ti/catalog/msp430/peripherals/clock/UCS.xdc
var UCS = xdc.useModule('ti.catalog.msp430.peripherals.clock.UCS');
module-wide constants & types
 
    values of type UCS.DCO0_t// DCO0 Bit
        const UCS.DCO0_OFF// Disable DCO0 bit;
        const UCS.DCO0// Enable DCO0 bit;
 
    values of type UCS.DCO1_t// DCO1 Bit
        const UCS.DCO1_OFF// Disable DCO1 bit;
        const UCS.DCO1// Enable DCO1 bit;
 
    values of type UCS.DCO2_t// DCO2 Bit
        const UCS.DCO2_OFF// Disable DCO2 bit;
        const UCS.DCO2// Enable DCO2 bit;
 
    values of type UCS.DCO3_t// DCO3 Bit
        const UCS.DCO3_OFF// Disable DCO3 bit;
        const UCS.DCO3// Enable DCO3 bit;
 
    values of type UCS.DCO4_t// DCO4 Bit
        const UCS.DCO4_OFF// Disable DCO4 bit;
        const UCS.DCO4// Enable DCO4 bit;
 
    values of type UCS.DCOFFG_t// DCO fault flag
 
        const UCS.DCORSEL_0// DCORSEL_0;
        const UCS.DCORSEL_1// DCORSEL_1;
        const UCS.DCORSEL_2// DCORSEL_2;
        const UCS.DCORSEL_3// DCORSEL_3;
        const UCS.DCORSEL_4// DCORSEL_4;
        const UCS.DCORSEL_5// DCORSEL_5;
        const UCS.DCORSEL_6// DCORSEL_6;
        const UCS.DCORSEL_7// DCORSEL_7;
 
    values of type UCS.DISMOD_t// DISMOD Bit
        const UCS.DISMOD_OFF// Modulation enabled;
        const UCS.DISMOD// Modulation disabled;
 
    values of type UCS.DIVA_t// ACLK source divider
        const UCS.DIVA_0// Divide by 1;
        const UCS.DIVA_1// Divide by 2;
        const UCS.DIVA_2// Divide by 4;
        const UCS.DIVA_3// Divide by 8;
        const UCS.DIVA_4// Divide by 16;
        const UCS.DIVA_5// Divide by 32;
        const UCS.DIVA_6// Reserved;
        const UCS.DIVA_7// Reserved;
 
    values of type UCS.DIVM_t// MCLK source divider
        const UCS.DIVM_0// Divide by 1;
        const UCS.DIVM_1// Divide by 2;
        const UCS.DIVM_2// Divide by 4;
        const UCS.DIVM_3// Divide by 8;
        const UCS.DIVM_4// Divide by 16;
        const UCS.DIVM_5// Divide by 32;
        const UCS.DIVM_6// Reserved;
        const UCS.DIVM_7// Reserved;
 
        const UCS.DIVPA_0// Divide by 1;
        const UCS.DIVPA_1// Divide by 2;
        const UCS.DIVPA_2// Divide by 4;
        const UCS.DIVPA_3// Divide by 8;
        const UCS.DIVPA_4// Divide by 16;
        const UCS.DIVPA_5// Divide by 32;
        const UCS.DIVPA_6// Reserved;
        const UCS.DIVPA_7// Reserved;
 
    values of type UCS.DIVS_t// SMCLK source divider
        const UCS.DIVS_0// Divide by 1;
        const UCS.DIVS_1// Divide by 2;
        const UCS.DIVS_2// Divide by 4;
        const UCS.DIVS_3// Divide by 8;
        const UCS.DIVS_4// Divide by 16;
        const UCS.DIVS_5// Divide by 32;
        const UCS.DIVS_6// Reserved;
        const UCS.DIVS_7// Reserved;
 
    values of type UCS.FLLD_t// FLL Loop Divider
 
    values of type UCS.FLLN0_t// FLL Multiplier Bit 0
        const UCS.FLLN0_OFF// Disable FLLN bit 0;
        const UCS.FLLN0// Enable FLLN bit 0;
 
    values of type UCS.FLLN1_t// FLL Multiplier Bit 1
        const UCS.FLLN1_OFF// Disable FLLN bit 1;
        const UCS.FLLN1// Enable FLLN bit 1;
 
    values of type UCS.FLLN2_t// FLL Multiplier Bit 2
        const UCS.FLLN2_OFF// Disable FLLN bit 2;
        const UCS.FLLN2// Enable FLLN bit 2;
 
    values of type UCS.FLLN3_t// FLL Multiplier Bit 3
        const UCS.FLLN3_OFF// Disable FLLN bit 3;
        const UCS.FLLN3// Enable FLLN bit 3;
 
    values of type UCS.FLLN4_t// FLL Multiplier Bit 4
        const UCS.FLLN4_OFF// Disable FLLN bit 4;
        const UCS.FLLN4// Enable FLLN bit 4;
 
    values of type UCS.FLLN5_t// FLL Multiplier Bit 5
        const UCS.FLLN5_OFF// Disable FLLN bit 5;
        const UCS.FLLN5// Enable FLLN bit 5;
 
    values of type UCS.FLLN6_t// FLL Multiplier Bit 6
        const UCS.FLLN6_OFF// Disable FLLN bit 6;
        const UCS.FLLN6// Enable FLLN bit 6;
 
    values of type UCS.FLLN7_t// FLL Multiplier Bit 7
        const UCS.FLLN7_OFF// Disable FLLN bit 7;
        const UCS.FLLN7// Enable FLLN bit 7;
 
    values of type UCS.FLLN8_t// FLL Multiplier Bit 8
        const UCS.FLLN8_OFF// Disable FLLN bit 8;
        const UCS.FLLN8// Enable FLLN bit 8;
 
    values of type UCS.FLLN9_t// FLL Multiplier Bit 9
        const UCS.FLLN9_OFF// Disable FLLN bit 9;
        const UCS.FLLN9// Enable FLLN bit 9;
 
        const UCS.FLLREFDIV_0// f(FLLREFCLK) / 1;
        const UCS.FLLREFDIV_1// f(FLLREFCLK) / 2;
        const UCS.FLLREFDIV_2// f(FLLREFCLK) / 4;
        const UCS.FLLREFDIV_3// f(FLLREFCLK) / 8;
        const UCS.FLLREFDIV_4// f(FLLREFCLK) / 12;
        const UCS.FLLREFDIV_5// f(FLLREFCLK) / 16;
        const UCS.FLLREFDIV_6// Reserved;
        const UCS.FLLREFDIV_7// Reserved;
 
 
    values of type UCS.MOD0_t// MOD0 Bit
        const UCS.MOD0_OFF// Disable MOD0 bit;
        const UCS.MOD0// Enable MOD0 bit;
 
    values of type UCS.MOD1_t// MOD1 Bit
        const UCS.MOD1_OFF// Disable MOD1 bit;
        const UCS.MOD1// Enable MOD1 bit;
 
    values of type UCS.MOD2_t// MOD2 Bit
        const UCS.MOD2_OFF// Disable MOD2 bit;
        const UCS.MOD2// Enable MOD2 bit;
 
    values of type UCS.MOD3_t// MOD3 Bit
        const UCS.MOD3_OFF// Disable MOD3 bit;
        const UCS.MOD3// Enable MOD3 bit;
 
    values of type UCS.MOD4_t// MOD4 Bit
        const UCS.MOD4_OFF// Disable MOD4 bit;
        const UCS.MOD4// Enable MOD4 bit;
 
 
    values of type UCS.SELA_t// Select the ACLK source
        const UCS.SELA_0// XT1CLK;
        const UCS.SELA_1// VLOCLK;
        const UCS.SELA_2// REFOCLK;
        const UCS.SELA_3// DCOCLK;
        const UCS.SELA_4// DCOCLKDIV;
        const UCS.SELA_5// XT2CLK;
        const UCS.SELA_6// Reserved;
        const UCS.SELA_7// Reserved;
 
    values of type UCS.SELM_t// Select the MCLK source
        const UCS.SELM_0// XT1CLK;
        const UCS.SELM_1// VLOCLK;
        const UCS.SELM_2// REFOCLK;
        const UCS.SELM_3// DCOCLK;
        const UCS.SELM_4// DCOCLKDIV;
        const UCS.SELM_5// XT2CLK;
        const UCS.SELM_6// Reserved;
        const UCS.SELM_7// Reserved;
 
    values of type UCS.SELREF_t// FLL Reference Select
        const UCS.SELREF_1// Reserved;
        const UCS.SELREF_3// Reserved;
        const UCS.SELREF_4// Reserved;
        const UCS.SELREF_6// Reserved;
        const UCS.SELREF_7// Reserved;
 
    values of type UCS.SELS_t// Select the SMCLK source
        const UCS.SELS_0// XT1CLK;
        const UCS.SELS_1// VLOCLK;
        const UCS.SELS_2// REFOCLK;
        const UCS.SELS_3// DCOCLK;
        const UCS.SELS_4// DCOCLKDIV;
        const UCS.SELS_5// XT2CLK;
        const UCS.SELS_6// Reserved;
        const UCS.SELS_7// Reserved;
 
    values of type UCS.SMCLKOFF_t// SMCLK off
        const UCS.SMCLKOFF_OFF// SMCLK on;
        const UCS.SMCLKOFF// SMCLK off;
 
 
        const UCS.UCS_XT1CLK_SELECT// XT1CLK;
        const UCS.UCS_VLOCLK_SELECT// VLOCLK;
        const UCS.UCS_REFOCLK_SELECT// REFOCLK;
        const UCS.UCS_DCOCLK_SELECT// DCOCLK;
        const UCS.UCS_DCOCLKDIV_SELECT// DCOCLKDIV;
        const UCS.UCS_XT2CLK_SELECT// XT2CLK;
 
 
        const UCS.UCS_XCAP_0// ~ 2 pF;
        const UCS.UCS_XCAP_1// ~ 5.5 pF;
        const UCS.UCS_XCAP_2// ~ 8.5 pF;
        const UCS.UCS_XCAP_3// ~ 12 pF;
 
        const UCS.XCAP_0// XT1 Cap 0;
        const UCS.XCAP_1// XT1 Cap 1;
        const UCS.XCAP_2// XT1 Cap 2;
        const UCS.XCAP_3// XT1 Cap 3;
 
 
    values of type UCS.XT1BYPASS_t// XT1 bypass select
 
        const UCS.XT1DRIVE_0// XT1 drive 0;
        const UCS.XT1DRIVE_1// XT1 drive 1;
        const UCS.XT1DRIVE_2// XT1 drive 2;
        const UCS.XT1DRIVE_3// XT1 drive 3;
 
 
 
        const UCS.XT1OFF_OFF// Enable XT1;
        const UCS.XT1OFF// Disable XT1;
 
 
    values of type UCS.XT2BYPASS_t// XT2 bypass select
 
        const UCS.XT2DRIVE_0// 4 MHz to 8 MHz;
        const UCS.XT2DRIVE_1// 8 MHz to 16 MHz;
        const UCS.XT2DRIVE_2// 16 MHz to 24 MHz;
        const UCS.XT2DRIVE_3// 24 MHz to 32 MHz;
 
 
        const UCS.XT2OFF_OFF// Enable XT2;
        const UCS.XT2OFF// Disable XT2;
 
    values of type UCS.XTS_t// XTS mode select
        const UCS.XTS_OFF// Low Frequency;
        const UCS.XTS// High Frequency;
 
        obj.clockType = String  ...
        obj.hasClock = Bool  ...
 
        obj.register = String  ...
        obj.regForceSet = Bool  ...
 
        obj.DCO0// DCO tap selection bit 0 = UCS.DCO0_t  ...
        obj.DCO1// DCO tap selection bit 1 = UCS.DCO1_t  ...
        obj.DCO2// DCO tap selection bit 2 = UCS.DCO2_t  ...
        obj.DCO3// DCO tap selection bit 3 = UCS.DCO3_t  ...
        obj.DCO4// DCO tap selection bit 4 = UCS.DCO4_t  ...
        obj.MOD0// Modulation bit counter bit 0 = UCS.MOD0_t  ...
        obj.MOD1// Modulation bit counter bit 1 = UCS.MOD1_t  ...
        obj.MOD2// Modulation bit counter bit 2 = UCS.MOD2_t  ...
        obj.MOD3// Modulation bit counter bit 3 = UCS.MOD3_t  ...
        obj.MOD4// Modulation bit counter bit 4 = UCS.MOD4_t  ...
 
 
        obj.FLLN0// Multiplier bit 0 = UCS.FLLN0_t  ...
        obj.FLLN1// Multiplier bit 1 = UCS.FLLN1_t  ...
        obj.FLLN2// Multiplier bit 2 = UCS.FLLN2_t  ...
        obj.FLLN3// Multiplier bit 3 = UCS.FLLN3_t  ...
        obj.FLLN4// Multiplier bit 4 = UCS.FLLN4_t  ...
        obj.FLLN5// Multiplier bit 5 = UCS.FLLN5_t  ...
        obj.FLLN6// Multiplier bit 6 = UCS.FLLN6_t  ...
        obj.FLLN7// Multiplier bit 7 = UCS.FLLN7_t  ...
        obj.FLLN8// Multiplier bit 8 = UCS.FLLN8_t  ...
        obj.FLLN9// Multiplier bit 9 = UCS.FLLN9_t  ...
 
 
 
 
 
 
 
module-wide functions
per-instance config parameters
    var params = new UCS.Params// Instance config-params object;
        params.ACLKHz// ACLK frequency in Hertz = Float undefined;
        params.DCOCLKDIVHz// Divided DCO clock frequency in Hertz = Float undefined;
        params.DCOCLKHz// DCO clock frequency in Hertz = Float 1000000;
        params.MCLKHz// MCLK frequency in Hertz = Float undefined;
        params.REFOCLKHz//  = Float 32768;
        params.SMCLKHz// SMCLK frequency in Hertz = Float undefined;
            DCO0: UCS.DCO0_OFF,
            DCO1: UCS.DCO1_OFF,
            DCO2: UCS.DCO2_OFF,
            DCO3: UCS.DCO3_OFF,
            DCO4: UCS.DCO4_OFF,
            MOD0: UCS.MOD0_OFF,
            MOD1: UCS.MOD1_OFF,
            MOD2: UCS.MOD2_OFF,
            MOD3: UCS.MOD3_OFF,
            MOD4: UCS.MOD4_OFF
        };
            DCORSEL: UCS.DCORSEL_2,
            DISMOD: UCS.DISMOD_OFF
        };
            FLLD: UCS.FLLD_1,
            FLLN0: UCS.FLLN0,
            FLLN1: UCS.FLLN1,
            FLLN2: UCS.FLLN2,
            FLLN3: UCS.FLLN3,
            FLLN4: UCS.FLLN4,
            FLLN5: UCS.FLLN5_OFF,
            FLLN6: UCS.FLLN6_OFF,
            FLLN7: UCS.FLLN7_OFF,
            FLLN8: UCS.FLLN8_OFF,
            FLLN9: UCS.FLLN9_OFF
        };
            SELREF: UCS.SELREF_0,
            FLLREFDIV: UCS.FLLREFDIV_0
        };
            SELA: UCS.SELA_0,
            SELS: UCS.SELS_4,
            SELM: UCS.SELM_4
        };
            DIVPA: UCS.DIVPA_0,
            DIVA: UCS.DIVA_0,
            DIVS: UCS.DIVS_0,
            DIVM: UCS.DIVM_0
        };
            XT2DRIVE: UCS.XT2DRIVE_3,
            XT2BYPASS: UCS.XT2BYPASS_OFF,
            XT2OFF: UCS.XT2OFF,
            XT1DRIVE: UCS.XT1DRIVE_3,
            XTS: UCS.XTS,
            XT1BYPASS: UCS.XT1BYPASS,
            XCAP: UCS.XCAP_3,
            SMCLKOFF: UCS.SMCLKOFF_OFF,
            XT1OFF: UCS.XT1OFF
        };
            XT2OFFG: UCS.XT2OFFG_OFF,
            XT1HFOFFG: UCS.XT1HFOFFG_OFF,
            XT1LFOFFG: UCS.XT1LFOFFG,
            DCOFFG: UCS.DCOFFG
        };
            MODOSCREQEN: UCS.MODOSCREQEN_OFF,
            SMCLKREQEN: UCS.SMCLKREQEN,
            MCLKREQEN: UCS.MCLKREQEN,
            ACLKREQEN: UCS.ACLKREQEN
        };
            XT2BYPASSLV: UCS.XT2BYPASSLV_OFF,
            XT1BYPASSLV: UCS.XT1BYPASSLV_OFF
        };
        params.UCS_FLL_FREQ// Set FLL target frequency = Float 0;
        params.UCS_FLL_RATIO// FLLN value = UInt 31;
        params.VLOCLKHz//  = Float 12000;
        params.WATCHCRYSTALCLKHz//  = Float 32768;
        params.XT1CLKHz//  = Float 0;
        params.XT2CLKHz//  = Float 0;
        params.baseAddr// Address of the peripheral's control register = UInt undefined;
        params.baseAddress// UCS base address = String "__MSP430_BASEADDRESS_UCS__";
            {
                register: "UCS_SMCLKREQEN",
                regForceSet: false
            },
            {
                register: "UCS_MCLKREQEN",
                regForceSet: false
            },
            {
                register: "UCS_ACLKREQEN",
                regForceSet: false
            },
            {
                register: "UCS_MODOSCREQEN",
                regForceSet: false
            }
        ];
        params.hasHFXT1// Specify if HFXT1 is available on the device = Bool false;
        params.hasRosc// Specify if Rosc is available on the device = Bool false;
        params.hasVLO// Specify if VLO is available on the device = Bool false;
        params.hasXT2// Specify if XT2 is available on the device = Bool false;
        params.maxCpuFrequency// Maximum CPU frequency in Hertz = Float 0;
        params.name// Specific peripheral name given by the device = String undefined;
        params.owner// String specifying the entity that manages the peripheral = String undefined;
per-instance functions
 
 
enum UCS.ACLKREQEN_t

ACLK clock request enable

XDCscript usage meta-domain
values of type UCS.ACLKREQEN_t
    const UCS.ACLKREQEN_OFF;
    // ACLK conditional requests are disabled
    const UCS.ACLKREQEN;
    // ACLK conditional requests are enabled
 
 
enum UCS.DCO0_t

DCO0 Bit

XDCscript usage meta-domain
values of type UCS.DCO0_t
    const UCS.DCO0_OFF;
    // Disable DCO0 bit
    const UCS.DCO0;
    // Enable DCO0 bit
 
 
enum UCS.DCO1_t

DCO1 Bit

XDCscript usage meta-domain
values of type UCS.DCO1_t
    const UCS.DCO1_OFF;
    // Disable DCO1 bit
    const UCS.DCO1;
    // Enable DCO1 bit
 
 
enum UCS.DCO2_t

DCO2 Bit

XDCscript usage meta-domain
values of type UCS.DCO2_t
    const UCS.DCO2_OFF;
    // Disable DCO2 bit
    const UCS.DCO2;
    // Enable DCO2 bit
 
 
enum UCS.DCO3_t

DCO3 Bit

XDCscript usage meta-domain
values of type UCS.DCO3_t
    const UCS.DCO3_OFF;
    // Disable DCO3 bit
    const UCS.DCO3;
    // Enable DCO3 bit
 
 
enum UCS.DCO4_t

DCO4 Bit

XDCscript usage meta-domain
values of type UCS.DCO4_t
    const UCS.DCO4_OFF;
    // Disable DCO4 bit
    const UCS.DCO4;
    // Enable DCO4 bit
 
 
enum UCS.DCOFFG_t

DCO fault flag

XDCscript usage meta-domain
values of type UCS.DCOFFG_t
    const UCS.DCOFFG_OFF;
    // No fault condition present
    const UCS.DCOFFG;
    // DCO fault condition present
 
 
enum UCS.DCORSEL_t

DCO frequency range select

XDCscript usage meta-domain
values of type UCS.DCORSEL_t
    const UCS.DCORSEL_0;
    // DCORSEL_0
    const UCS.DCORSEL_1;
    // DCORSEL_1
    const UCS.DCORSEL_2;
    // DCORSEL_2
    const UCS.DCORSEL_3;
    // DCORSEL_3
    const UCS.DCORSEL_4;
    // DCORSEL_4
    const UCS.DCORSEL_5;
    // DCORSEL_5
    const UCS.DCORSEL_6;
    // DCORSEL_6
    const UCS.DCORSEL_7;
    // DCORSEL_7
 
 
enum UCS.DISMOD_t

DISMOD Bit

XDCscript usage meta-domain
values of type UCS.DISMOD_t
    const UCS.DISMOD_OFF;
    // Modulation enabled
    const UCS.DISMOD;
    // Modulation disabled
 
 
enum UCS.DIVA_t

ACLK source divider

XDCscript usage meta-domain
values of type UCS.DIVA_t
    const UCS.DIVA_0;
    // Divide by 1
    const UCS.DIVA_1;
    // Divide by 2
    const UCS.DIVA_2;
    // Divide by 4
    const UCS.DIVA_3;
    // Divide by 8
    const UCS.DIVA_4;
    // Divide by 16
    const UCS.DIVA_5;
    // Divide by 32
    const UCS.DIVA_6;
    // Reserved
    const UCS.DIVA_7;
    // Reserved
 
 
enum UCS.DIVM_t

MCLK source divider

XDCscript usage meta-domain
values of type UCS.DIVM_t
    const UCS.DIVM_0;
    // Divide by 1
    const UCS.DIVM_1;
    // Divide by 2
    const UCS.DIVM_2;
    // Divide by 4
    const UCS.DIVM_3;
    // Divide by 8
    const UCS.DIVM_4;
    // Divide by 16
    const UCS.DIVM_5;
    // Divide by 32
    const UCS.DIVM_6;
    // Reserved
    const UCS.DIVM_7;
    // Reserved
 
 
enum UCS.DIVPA_t

ACLK source divider available at external pin

XDCscript usage meta-domain
values of type UCS.DIVPA_t
    const UCS.DIVPA_0;
    // Divide by 1
    const UCS.DIVPA_1;
    // Divide by 2
    const UCS.DIVPA_2;
    // Divide by 4
    const UCS.DIVPA_3;
    // Divide by 8
    const UCS.DIVPA_4;
    // Divide by 16
    const UCS.DIVPA_5;
    // Divide by 32
    const UCS.DIVPA_6;
    // Reserved
    const UCS.DIVPA_7;
    // Reserved
 
 
enum UCS.DIVS_t

SMCLK source divider

XDCscript usage meta-domain
values of type UCS.DIVS_t
    const UCS.DIVS_0;
    // Divide by 1
    const UCS.DIVS_1;
    // Divide by 2
    const UCS.DIVS_2;
    // Divide by 4
    const UCS.DIVS_3;
    // Divide by 8
    const UCS.DIVS_4;
    // Divide by 16
    const UCS.DIVS_5;
    // Divide by 32
    const UCS.DIVS_6;
    // Reserved
    const UCS.DIVS_7;
    // Reserved
 
 
enum UCS.FLLD_t

FLL Loop Divider

XDCscript usage meta-domain
values of type UCS.FLLD_t
    const UCS.FLLD_0;
    // Multiply Selected Loop Freq. 1
    const UCS.FLLD_1;
    // Multiply Selected Loop Freq. 2
    const UCS.FLLD_2;
    // Multiply Selected Loop Freq. 4
    const UCS.FLLD_3;
    // Multiply Selected Loop Freq. 8
    const UCS.FLLD_4;
    // Multiply Selected Loop Freq. 16
    const UCS.FLLD_5;
    // Multiply Selected Loop Freq. 32
    const UCS.FLLD_6;
    // Multiply Selected Loop Freq. 32
    const UCS.FLLD_7;
    // Multiply Selected Loop Freq. 32
 
 
enum UCS.FLLN0_t

FLL Multiplier Bit 0

XDCscript usage meta-domain
values of type UCS.FLLN0_t
    const UCS.FLLN0_OFF;
    // Disable FLLN bit 0
    const UCS.FLLN0;
    // Enable FLLN bit 0
 
 
enum UCS.FLLN1_t

FLL Multiplier Bit 1

XDCscript usage meta-domain
values of type UCS.FLLN1_t
    const UCS.FLLN1_OFF;
    // Disable FLLN bit 1
    const UCS.FLLN1;
    // Enable FLLN bit 1
 
 
enum UCS.FLLN2_t

FLL Multiplier Bit 2

XDCscript usage meta-domain
values of type UCS.FLLN2_t
    const UCS.FLLN2_OFF;
    // Disable FLLN bit 2
    const UCS.FLLN2;
    // Enable FLLN bit 2
 
 
enum UCS.FLLN3_t

FLL Multiplier Bit 3

XDCscript usage meta-domain
values of type UCS.FLLN3_t
    const UCS.FLLN3_OFF;
    // Disable FLLN bit 3
    const UCS.FLLN3;
    // Enable FLLN bit 3
 
 
enum UCS.FLLN4_t

FLL Multiplier Bit 4

XDCscript usage meta-domain
values of type UCS.FLLN4_t
    const UCS.FLLN4_OFF;
    // Disable FLLN bit 4
    const UCS.FLLN4;
    // Enable FLLN bit 4
 
 
enum UCS.FLLN5_t

FLL Multiplier Bit 5

XDCscript usage meta-domain
values of type UCS.FLLN5_t
    const UCS.FLLN5_OFF;
    // Disable FLLN bit 5
    const UCS.FLLN5;
    // Enable FLLN bit 5
 
 
enum UCS.FLLN6_t

FLL Multiplier Bit 6

XDCscript usage meta-domain
values of type UCS.FLLN6_t
    const UCS.FLLN6_OFF;
    // Disable FLLN bit 6
    const UCS.FLLN6;
    // Enable FLLN bit 6
 
 
enum UCS.FLLN7_t

FLL Multiplier Bit 7

XDCscript usage meta-domain
values of type UCS.FLLN7_t
    const UCS.FLLN7_OFF;
    // Disable FLLN bit 7
    const UCS.FLLN7;
    // Enable FLLN bit 7
 
 
enum UCS.FLLN8_t

FLL Multiplier Bit 8

XDCscript usage meta-domain
values of type UCS.FLLN8_t
    const UCS.FLLN8_OFF;
    // Disable FLLN bit 8
    const UCS.FLLN8;
    // Enable FLLN bit 8
 
 
enum UCS.FLLN9_t

FLL Multiplier Bit 9

XDCscript usage meta-domain
values of type UCS.FLLN9_t
    const UCS.FLLN9_OFF;
    // Disable FLLN bit 9
    const UCS.FLLN9;
    // Enable FLLN bit 9
 
 
enum UCS.FLLREFDIV_t

FLL Reference Divider

XDCscript usage meta-domain
values of type UCS.FLLREFDIV_t
    const UCS.FLLREFDIV_0;
    // f(FLLREFCLK) / 1
    const UCS.FLLREFDIV_1;
    // f(FLLREFCLK) / 2
    const UCS.FLLREFDIV_2;
    // f(FLLREFCLK) / 4
    const UCS.FLLREFDIV_3;
    // f(FLLREFCLK) / 8
    const UCS.FLLREFDIV_4;
    // f(FLLREFCLK) / 12
    const UCS.FLLREFDIV_5;
    // f(FLLREFCLK) / 16
    const UCS.FLLREFDIV_6;
    // Reserved
    const UCS.FLLREFDIV_7;
    // Reserved
 
 
enum UCS.MCLKREQEN_t

MCLK clock request enable

XDCscript usage meta-domain
values of type UCS.MCLKREQEN_t
    const UCS.MCLKREQEN_OFF;
    // MCLK conditional requests are disabled
    const UCS.MCLKREQEN;
    // MCLK conditional requests are enabled
 
 
enum UCS.MOD0_t

MOD0 Bit

XDCscript usage meta-domain
values of type UCS.MOD0_t
    const UCS.MOD0_OFF;
    // Disable MOD0 bit
    const UCS.MOD0;
    // Enable MOD0 bit
 
 
enum UCS.MOD1_t

MOD1 Bit

XDCscript usage meta-domain
values of type UCS.MOD1_t
    const UCS.MOD1_OFF;
    // Disable MOD1 bit
    const UCS.MOD1;
    // Enable MOD1 bit
 
 
enum UCS.MOD2_t

MOD2 Bit

XDCscript usage meta-domain
values of type UCS.MOD2_t
    const UCS.MOD2_OFF;
    // Disable MOD2 bit
    const UCS.MOD2;
    // Enable MOD2 bit
 
 
enum UCS.MOD3_t

MOD3 Bit

XDCscript usage meta-domain
values of type UCS.MOD3_t
    const UCS.MOD3_OFF;
    // Disable MOD3 bit
    const UCS.MOD3;
    // Enable MOD3 bit
 
 
enum UCS.MOD4_t

MOD4 Bit

XDCscript usage meta-domain
values of type UCS.MOD4_t
    const UCS.MOD4_OFF;
    // Disable MOD4 bit
    const UCS.MOD4;
    // Enable MOD4 bit
 
 
enum UCS.MODOSCREQEN_t

MODOSC clock request enable

XDCscript usage meta-domain
values of type UCS.MODOSCREQEN_t
    const UCS.MODOSCREQEN_OFF;
    // MODOSC conditional requests are disabled
    const UCS.MODOSCREQEN;
    // MODOSC conditional requests are enabled
 
 
enum UCS.SELA_t

Select the ACLK source

XDCscript usage meta-domain
values of type UCS.SELA_t
    const UCS.SELA_0;
    // XT1CLK
    const UCS.SELA_1;
    // VLOCLK
    const UCS.SELA_2;
    // REFOCLK
    const UCS.SELA_3;
    // DCOCLK
    const UCS.SELA_4;
    // DCOCLKDIV
    const UCS.SELA_5;
    // XT2CLK
    const UCS.SELA_6;
    // Reserved
    const UCS.SELA_7;
    // Reserved
 
 
enum UCS.SELM_t

Select the MCLK source

XDCscript usage meta-domain
values of type UCS.SELM_t
    const UCS.SELM_0;
    // XT1CLK
    const UCS.SELM_1;
    // VLOCLK
    const UCS.SELM_2;
    // REFOCLK
    const UCS.SELM_3;
    // DCOCLK
    const UCS.SELM_4;
    // DCOCLKDIV
    const UCS.SELM_5;
    // XT2CLK
    const UCS.SELM_6;
    // Reserved
    const UCS.SELM_7;
    // Reserved
 
 
enum UCS.SELREF_t

FLL Reference Select

XDCscript usage meta-domain
values of type UCS.SELREF_t
    const UCS.SELREF_0;
    // FLL Reference by XT1CLK
    const UCS.SELREF_1;
    // Reserved
    const UCS.SELREF_2;
    // FLL Reference by REFOCLK
    const UCS.SELREF_3;
    // Reserved
    const UCS.SELREF_4;
    // Reserved
    const UCS.SELREF_5;
    // FLL Reference by XT2CLK
    const UCS.SELREF_6;
    // Reserved
    const UCS.SELREF_7;
    // Reserved
 
 
enum UCS.SELS_t

Select the SMCLK source

XDCscript usage meta-domain
values of type UCS.SELS_t
    const UCS.SELS_0;
    // XT1CLK
    const UCS.SELS_1;
    // VLOCLK
    const UCS.SELS_2;
    // REFOCLK
    const UCS.SELS_3;
    // DCOCLK
    const UCS.SELS_4;
    // DCOCLKDIV
    const UCS.SELS_5;
    // XT2CLK
    const UCS.SELS_6;
    // Reserved
    const UCS.SELS_7;
    // Reserved
 
 
enum UCS.SMCLKOFF_t

SMCLK off

XDCscript usage meta-domain
values of type UCS.SMCLKOFF_t
    const UCS.SMCLKOFF_OFF;
    // SMCLK on
    const UCS.SMCLKOFF;
    // SMCLK off
 
 
enum UCS.SMCLKREQEN_t

SMCLK clock request enable

XDCscript usage meta-domain
values of type UCS.SMCLKREQEN_t
    const UCS.SMCLKREQEN_OFF;
    // SMCLK conditional requests are disabled
    const UCS.SMCLKREQEN;
    // SMCLK conditional requests are enabled
 
 
enum UCS.UCS_CLK_SOURCE_t

Select the clock source

XDCscript usage meta-domain
values of type UCS.UCS_CLK_SOURCE_t
    const UCS.UCS_XT1CLK_SELECT;
    // XT1CLK
    const UCS.UCS_VLOCLK_SELECT;
    // VLOCLK
    const UCS.UCS_REFOCLK_SELECT;
    // REFOCLK
    const UCS.UCS_DCOCLK_SELECT;
    // DCOCLK
    const UCS.UCS_DCOCLKDIV_SELECT;
    // DCOCLKDIV
    const UCS.UCS_XT2CLK_SELECT;
    // XT2CLK
 
 
enum UCS.UCS_CLK_SRC_DIVIDER_t

Select clock source divider

XDCscript usage meta-domain
values of type UCS.UCS_CLK_SRC_DIVIDER_t
    const UCS.UCS_CLOCK_DIVIDER_1;
    // Divide by 1
    const UCS.UCS_CLOCK_DIVIDER_2;
    // Divide by 2
    const UCS.UCS_CLOCK_DIVIDER_4;
    // Divide by 4
    const UCS.UCS_CLOCK_DIVIDER_8;
    // Divide by 8
    const UCS.UCS_CLOCK_DIVIDER_12;
    // Divide by 12
    const UCS.UCS_CLOCK_DIVIDER_16;
    // Divide by 16
    const UCS.UCS_CLOCK_DIVIDER_32;
    // Divide by 32
 
 
enum UCS.UCS_XCAP_t

XT1 oscillator capacitor select

XDCscript usage meta-domain
values of type UCS.UCS_XCAP_t
    const UCS.UCS_XCAP_0;
    // ~ 2 pF
    const UCS.UCS_XCAP_1;
    // ~ 5.5 pF
    const UCS.UCS_XCAP_2;
    // ~ 8.5 pF
    const UCS.UCS_XCAP_3;
    // ~ 12 pF
 
 
enum UCS.XCAP_t

XT1 oscillator capacitor select

XDCscript usage meta-domain
values of type UCS.XCAP_t
    const UCS.XCAP_0;
    // XT1 Cap 0
    const UCS.XCAP_1;
    // XT1 Cap 1
    const UCS.XCAP_2;
    // XT1 Cap 2
    const UCS.XCAP_3;
    // XT1 Cap 3
 
 
enum UCS.XT1BYPASSLV_t

Selects XT1 bypass input swing level

XDCscript usage meta-domain
values of type UCS.XT1BYPASSLV_t
    const UCS.XT1BYPASSLV_OFF;
    // Input range from 0 to DVCC
    const UCS.XT1BYPASSLV;
    // Input range from 0 to DVIO
 
 
enum UCS.XT1BYPASS_t

XT1 bypass select

XDCscript usage meta-domain
values of type UCS.XT1BYPASS_t
    const UCS.XT1BYPASS_OFF;
    // XT1 sourced internally
    const UCS.XT1BYPASS;
    // XT1 sourced externally from pin
 
 
enum UCS.XT1DRIVE_t

XT1 oscillator current

XDCscript usage meta-domain
values of type UCS.XT1DRIVE_t
    const UCS.XT1DRIVE_0;
    // XT1 drive 0
    const UCS.XT1DRIVE_1;
    // XT1 drive 1
    const UCS.XT1DRIVE_2;
    // XT1 drive 2
    const UCS.XT1DRIVE_3;
    // XT1 drive 3
 
 
enum UCS.XT1HFOFFG_t

XT1 high frequency oscillator fault flag

XDCscript usage meta-domain
values of type UCS.XT1HFOFFG_t
    const UCS.XT1HFOFFG_OFF;
    // No fault condition present
    const UCS.XT1HFOFFG;
    // XT1 HF fault condition present
 
 
enum UCS.XT1LFOFFG_t

XT1 low frequency oscillator fault flag

XDCscript usage meta-domain
values of type UCS.XT1LFOFFG_t
    const UCS.XT1LFOFFG_OFF;
    // No fault condition present
    const UCS.XT1LFOFFG;
    // XT1 LF fault condition present
 
 
enum UCS.XT1OFF_t

Turns off the XT1 oscillator

XDCscript usage meta-domain
values of type UCS.XT1OFF_t
    const UCS.XT1OFF_OFF;
    // Enable XT1
    const UCS.XT1OFF;
    // Disable XT1
 
 
enum UCS.XT2BYPASSLV_t

Selects XT2 bypass input swing level

XDCscript usage meta-domain
values of type UCS.XT2BYPASSLV_t
    const UCS.XT2BYPASSLV_OFF;
    // Input range from 0 to DVCC
    const UCS.XT2BYPASSLV;
    // Input range from 0 to DVIO
 
 
enum UCS.XT2BYPASS_t

XT2 bypass select

XDCscript usage meta-domain
values of type UCS.XT2BYPASS_t
    const UCS.XT2BYPASS_OFF;
    // XT2 sourced internally
    const UCS.XT2BYPASS;
    // XT2 sourced externally from pin
 
 
enum UCS.XT2DRIVE_t

XT2 oscillator current

XDCscript usage meta-domain
values of type UCS.XT2DRIVE_t
    const UCS.XT2DRIVE_0;
    // 4 MHz to 8 MHz
    const UCS.XT2DRIVE_1;
    // 8 MHz to 16 MHz
    const UCS.XT2DRIVE_2;
    // 16 MHz to 24 MHz
    const UCS.XT2DRIVE_3;
    // 24 MHz to 32 MHz
 
 
enum UCS.XT2OFFG_t

XT2 oscillator fault flag

XDCscript usage meta-domain
values of type UCS.XT2OFFG_t
    const UCS.XT2OFFG_OFF;
    // No fault condition present
    const UCS.XT2OFFG;
    // XT2 fault condition present
 
 
enum UCS.XT2OFF_t

Turns off the XT2 oscillator

XDCscript usage meta-domain
values of type UCS.XT2OFF_t
    const UCS.XT2OFF_OFF;
    // Enable XT2
    const UCS.XT2OFF;
    // Disable XT2
 
 
enum UCS.XTS_t

XTS mode select

XDCscript usage meta-domain
values of type UCS.XTS_t
    const UCS.XTS_OFF;
    // Low Frequency
    const UCS.XTS;
    // High Frequency
 
 
struct UCS.AvailableClockVariations_t

Available variations of clock in a device

XDCscript usage meta-domain
var obj = new UCS.AvailableClockVariations_t;
 
    obj.clockType = String  ...
    obj.hasClock = Bool  ...
 
DETAILS
Stores true/false if any of the clock variations are available.
SEE
 
struct UCS.ForceSetDefaultRegister_t

Force Set Default Register

XDCscript usage meta-domain
var obj = new UCS.ForceSetDefaultRegister_t;
 
    obj.register = String  ...
    obj.regForceSet = Bool  ...
 
DETAILS
Type to store if each register needs to be forced initialized even if the register is in default state.
SEE
 
struct UCS.UCSCTL0_t

Unified Clock System Control 0 Register

XDCscript usage meta-domain
var obj = new UCS.UCSCTL0_t;
 
    obj.DCO0 = UCS.DCO0_t  ...
    // DCO tap selection bit 0
    obj.DCO1 = UCS.DCO1_t  ...
    // DCO tap selection bit 1
    obj.DCO2 = UCS.DCO2_t  ...
    // DCO tap selection bit 2
    obj.DCO3 = UCS.DCO3_t  ...
    // DCO tap selection bit 3
    obj.DCO4 = UCS.DCO4_t  ...
    // DCO tap selection bit 4
    obj.MOD0 = UCS.MOD0_t  ...
    // Modulation bit counter bit 0
    obj.MOD1 = UCS.MOD1_t  ...
    // Modulation bit counter bit 1
    obj.MOD2 = UCS.MOD2_t  ...
    // Modulation bit counter bit 2
    obj.MOD3 = UCS.MOD3_t  ...
    // Modulation bit counter bit 3
    obj.MOD4 = UCS.MOD4_t  ...
    // Modulation bit counter bit 4
 
FIELDS
DCO — DCO tap selection.
MOD — Modulation bit counter.
 
struct UCS.UCSCTL1_t

Unified Clock System Control 1 Register

XDCscript usage meta-domain
var obj = new UCS.UCSCTL1_t;
 
    obj.DCORSEL = UCS.DCORSEL_t  ...
    // DCO frequency range select. These bits select the DCO frequency range of operation defined in the device-specific datasheet
    obj.DISMOD = UCS.DISMOD_t  ...
    // Modulation. This bit enables/disables the modulation. 0 Modulation enabled 1 Modulation disabled
 
FIELDS
DCORSEL — DCO frequency range select. These bits select the DCO frequency range of operation defined in the device-specific datasheet.
DISMOD — 0 Modulation enabled, 1 Modulation disabled.
 
struct UCS.UCSCTL2_t

Unified Clock System Control 2 Register

XDCscript usage meta-domain
var obj = new UCS.UCSCTL2_t;
 
    obj.FLLD = UCS.FLLD_t  ...
    // FLL loop divider. These bits divide fDCOCLK in the FLL feedback loop. This results in an additional multiplier for the multiplier bits. See also multiplier bits. 000 fDCOCLK/1 001 fDCOCLK/2 010 fDCOCLK/4 011 fDCOCLK/8 100 fDCOCLK/16 101 fDCOCLK/32 110 Reserved for future use. Defaults to fDCOCLK/32 111 Reserved for future use. Defaults to fDCOCLK/32
    obj.FLLN0 = UCS.FLLN0_t  ...
    // Multiplier bit 0
    obj.FLLN1 = UCS.FLLN1_t  ...
    // Multiplier bit 1
    obj.FLLN2 = UCS.FLLN2_t  ...
    // Multiplier bit 2
    obj.FLLN3 = UCS.FLLN3_t  ...
    // Multiplier bit 3
    obj.FLLN4 = UCS.FLLN4_t  ...
    // Multiplier bit 4
    obj.FLLN5 = UCS.FLLN5_t  ...
    // Multiplier bit 5
    obj.FLLN6 = UCS.FLLN6_t  ...
    // Multiplier bit 6
    obj.FLLN7 = UCS.FLLN7_t  ...
    // Multiplier bit 7
    obj.FLLN8 = UCS.FLLN8_t  ...
    // Multiplier bit 8
    obj.FLLN9 = UCS.FLLN9_t  ...
    // Multiplier bit 9
 
FIELDS
FLLD — FLL loop divider. These bits divide fDCOCLK in the FLL feedback loop. This results in an additional multiplier for the multiplier bits.
FLLN — Multiplier bits. These bits set the multiplier value N of the DCO. N must be greater than 0. Writing zero to FLLN causes N to be set to 1.
 
struct UCS.UCSCTL3_t

Unified Clock System Control 3 Register

XDCscript usage meta-domain
var obj = new UCS.UCSCTL3_t;
 
    obj.SELREF = UCS.SELREF_t  ...
    // FLL reference select. These bits select the FLL reference clock source. 000 XT1CLK 001 Reserved for future use. Defaults to XT1CLK. 010 REFOCLK 011 Reserved for future use. Defaults to REFOCLK. 100 Reserved for future use. Defaults to REFOCLK. 101 XT2CLK when available, otherwise REFOCLK. 110 Reserved for future use. XT2CLK when available, otherwise REFOCLK. 111 No selection. For the 'F543x and 'F541x non-A versions only, this defaults to XT2CLK. Reserved for future use. XT2CLK when available, otherwise REFOCLK
    obj.FLLREFDIV = UCS.FLLREFDIV_t  ...
    // FLL reference divider. These bits define the divide factor for fFLLREFCLK. The divided frequency is used as the FLL reference frequency. 000 fFLLREFCLK/1 001 fFLLREFCLK/2 010 fFLLREFCLK/4 011 fFLLREFCLK/8 100 fFLLREFCLK/12 101 fFLLREFCLK/16 110 Reserved for future use. Defaults to fFLLREFCLK/16. 111 Reserved for future use. Defaults to fFLLREFCLK/16
 
FIELDS
SELREF — FLL reference select. These bits select the FLL reference clock source.
FLLREFDIV — FLL reference divider. These bits define the divide factor for fFLLREFCLK. The divided frequency is used as the FLL reference frequency.
 
struct UCS.UCSCTL4_t

Unified Clock System Control 4 Register

XDCscript usage meta-domain
var obj = new UCS.UCSCTL4_t;
 
    obj.SELA = UCS.SELA_t  ...
    // Selects the ACLK source 000 XT1CLK 001 VLOCLK 010 REFOCLK 011 DCOCLK 100 DCOCLKDIV 101 XT2CLK when available, otherwise DCOCLKDIV 110 Reserved for future use. Defaults to XT2CLK when available, otherwise DCOCLKDIV. 111 Reserved for future use. Defaults to XT2CLK when available, otherwise DCOCLKDIV
    obj.SELS = UCS.SELS_t  ...
    // Selects the SMCLK source 000 XT1CLK 001 VLOCLK 010 REFOCLK 011 DCOCLK 100 DCOCLKDIV 101 XT2CLK when available, otherwise DCOCLKDIV 110 Reserved for future use. Defaults to XT2CLK when available, otherwise DCOCLKDIV. 111 Reserved for future use. Defaults to XT2CLK when available, otherwise DCOCLKDIV
    obj.SELM = UCS.SELM_t  ...
    // Selects the MCLK source 000 XT1CLK 001 VLOCLK 010 REFOCLK 011 DCOCLK 100 DCOCLKDIV 101 XT2CLK when available, otherwise DCOCLKDIV 110 Reserved for future use. Defaults to XT2CLK when available, otherwise DCOCLKDIV. 111 Reserved for future use. Defaults to XT2CLK when available, otherwise DCOCLKDIV
 
FIELDS
SELA — Selects the ACLK source
SELS — Selects the SMCLK source
SELM — Selects the MCLK source
 
struct UCS.UCSCTL5_t

Unified Clock System Control 5 Register

XDCscript usage meta-domain
var obj = new UCS.UCSCTL5_t;
 
    obj.DIVPA = UCS.DIVPA_t  ...
    // ACLK source divider available at external pin. Divides the frequency of ACLK and presents it to an external pin. 000 fACLK/1 001 fACLK/2 010 fACLK/4 011 fACLK/8 100 fACLK/16 101 fACLK/32 110 Reserved for future use. Defaults to fACLK/32. 111 Reserved for future use. Defaults to fACLK/32
    obj.DIVA = UCS.DIVA_t  ...
    // ACLK source divider. Divides the frequency of the ACLK clock source. 000 fACLK/1 001 fACLK/2 010 fACLK/4 011 fACLK/8 100 fACLK/16 101 fACLK/32 110 Reserved for future use. Defaults to fACLK/32. 111 Reserved for future use. Defaults to fACLK/32
    obj.DIVS = UCS.DIVS_t  ...
    // SMCLK source divider 000 fSMCLK/1 001 fSMCLK/2 010 fSMCLK/4 011 fSMCLK/8 100 fSMCLK/16 101 fSMCLK/32 110 Reserved for future use. Defaults to fSMCLK/32. 111 Reserved for future use. Defaults to fSMCLK/32
    obj.DIVM = UCS.DIVM_t  ...
    // MCLK source divider 000 fMCLK/1 001 fMCLK/2 010 fMCLK/4 011 fMCLK/8 100 fMCLK/16 101 fMCLK/32 110 Reserved for future use. Defaults to fMCLK/32. 111 Reserved for future use. Defaults to fMCLK/32
 
FIELDS
SELA — Selects the ACLK source
SELS — Selects the SMCLK source
SELM — Selects the MCLK source
 
struct UCS.UCSCTL6_t

Unified Clock System Control 6 Register

XDCscript usage meta-domain
var obj = new UCS.UCSCTL6_t;
 
    obj.XT2DRIVE = UCS.XT2DRIVE_t  ...
    // The XT2 oscillator current can be adjusted to its drive needs. Initially, it starts with the highest supply current for reliable and quick startup. If needed, user software can reduce the drive strength. 00 Lowest current consumption. XT2 oscillator operating range is 4 MHz to 8 MHz. 01 Increased drive strength XT2 oscillator. XT2 oscillator operating range is 8 MHz to 16 MHz. 10 Increased drive capability XT2 oscillator. XT2 oscillator operating range is 16 MHz to 24 MHz. 11 Maximum drive capability and maximum current consumption for both XT2 oscillator. XT2 oscillator operating range is 24 MHz to 32 MHz
    obj.XT2BYPASS = UCS.XT2BYPASS_t  ...
    // XT2 bypass select 0 XT2 sourced internally 1 XT2 sourced externally from pin
    obj.XT2OFF = UCS.XT2OFF_t  ...
    // Turns off the XT2 oscillator 0 XT2 is on if XT2 is selected via the port selection and XT2 is not in bypass mode of operation. 1 XT2 is off if it is not used as a source for ACLK, MCLK, or SMCLK or is not used as a reference source required for FLL operation
    obj.XT1DRIVE = UCS.XT1DRIVE_t  ...
    // The XT1 oscillator current can be adjusted to its drive needs. Initially, it starts with the highest supply current for reliable and quick startup. If needed, user software can reduce the drive strength. 00 Lowest current consumption for XT1 LF mode. XT1 oscillator operating range in HF mode is 4 MHz to 8 MHz. 01 Increased drive strength for XT1 LF mode. XT1 oscillator operating range in HF mode is 8 MHz to 16 MHz. 10 Increased drive capability for XT1 LF mode. XT1 oscillator operating range in HF mode is 16 MHz to 24 MHz. 11 Maximum drive capability and maximum current consumption for XT1 LF mode. XT1 oscillator operating range in HF mode is 24 MHz to 32 MHz
    obj.XTS = UCS.XTS_t  ...
    // XT1 mode select 0 Low-frequency mode. XCAP bits define the capacitance at the XIN and XOUT pins. 1 High-frequency mode. XCAP bits are not used
    obj.XT1BYPASS = UCS.XT1BYPASS_t  ...
    // XT1 bypass select 0 XT1 sourced internally 1 XT1 sourced externally from pin
    obj.XCAP = UCS.XCAP_t  ...
    // Oscillator capacitor selection. These bits select the capacitors applied to the LF crystal or resonator in the LF mode (XTS = 0). The effective capacitance (seen by the crystal) is Ceff (CXIN + 2 pF)/2. It is assumed that CXIN = CXOUT and that a parasitic capacitance of 2 pF is added by the package and the printed circuit board. For details about the typical internal and the effective capacitors, refer to the device-specific data sheet
    obj.SMCLKOFF = UCS.SMCLKOFF_t  ...
    // SMCLK off. This bit turns off the SMCLK. 0 SMCLK on 1 SMCLK off
    obj.XT1OFF = UCS.XT1OFF_t  ...
    // XT1 off. This bit turns off the XT1. 0 XT1 is on if XT1 is selected via the port selection and XT1 is not in bypass mode of operation. 1 XT1 is off if it is not used as a source for ACLK, MCLK, or SMCLK or is not used as a reference source required for FLL operation
 
FIELDS
SELA — Selects the ACLK source
SELS — Selects the SMCLK source
SELM — Selects the MCLK source
 
struct UCS.UCSCTL7_t

Unified Clock System Control 7 Register

XDCscript usage meta-domain
var obj = new UCS.UCSCTL7_t;
 
    obj.XT2OFFG = UCS.XT2OFFG_t  ...
    // XT2 oscillator fault flag. If this bit is set, the OFIFG flag is also set. XT2OFFG is set if a XT2 fault condition exists. XT2OFFG can be cleared via software. If the XT2 fault condition still remains, XT2OFFG is set. 0 No fault condition occurred after the last reset. 1 XT2 fault. An XT2 fault occurred after the last reset
    obj.XT1HFOFFG = UCS.XT1HFOFFG_t  ...
    // XT1 oscillator fault flag (HF mode). If this bit is set, the OFIFG flag is also set. XT1HFOFFG is set if a XT1 fault condition exists. XT1HFOFFG can be cleared via software. If the XT1 fault condition still remains, XT1HFOFFG is set. 0 No fault condition occurred after the last reset. 1 XT1 fault. An XT1 fault occurred after the last reset
    obj.XT1LFOFFG = UCS.XT1LFOFFG_t  ...
    // XT1 oscillator fault flag (LF mode). If this bit is set, the OFIFG flag is also set. XT1LFOFFG is set if a XT1 fault condition exists. XT1LFOFFG can be cleared via software. If the XT1 fault condition still remains, XT1LFOFFG is set. 0 No fault condition occurred after the last reset. 1 XT1 fault (LF mode). A XT1 fault occurred after the last reset
    obj.DCOFFG = UCS.DCOFFG_t  ...
    // DCO fault flag. If this bit is set, the OFIFG flag is also set. The DCOFFG bit is set if DCO = {0} or DCO = {31}. DCOFFG can be cleared via software. If the DCO fault condition still remains, DCOFFG is set. 0 No fault condition occurred after the last reset. 1 DCO fault. A DCO fault occurred after the last reset
 
FIELDS
XT2OFFG — 0 No fault condition, 1 XT2 fault
XT1HFOFFG — 0 No fault condition, 1 XT1 HF fault
XT1LFOFFG — 0 No fault condition, 1 XT1 LF fault
DCOFFG — 0 No fault condition, 1 DCO fault
 
struct UCS.UCSCTL8_t

Unified Clock System Control 8 Register

XDCscript usage meta-domain
var obj = new UCS.UCSCTL8_t;
 
    obj.MODOSCREQEN = UCS.MODOSCREQEN_t  ...
    // MODOSC clock request enable. Setting this enables conditional module requests for MODOSC. 0 MODOSC conditional requests are disabled. 1 MODOSC conditional requests are enabled
    obj.SMCLKREQEN = UCS.SMCLKREQEN_t  ...
    // SMCLK clock request enable. Setting this enables conditional module requests for SMCLK. 0 SMCLK conditional requests are disabled. 1 SMCLK conditional requests are enabled
    obj.MCLKREQEN = UCS.MCLKREQEN_t  ...
    // MCLK clock request enable. Setting this enables conditional module requests for MCLK 0 MCLK conditional requests are disabled. 1 MCLK conditional requests are enabled
    obj.ACLKREQEN = UCS.ACLKREQEN_t  ...
    // ACLK clock request enable. Setting this enables conditional module requests for ACLK 0 ACLK conditional requests are disabled. 1 ACLK conditional requests are enabled
 
FIELDS
MODOSCREQEN — 0 MODOSC conditional requests are disabled 1 MODOSC conditional requests are enabled
SMCLKREQEN — 0 SMCLK conditional requests are disabled 1 SMCLK conditional requests are enabled
MCLKREQEN — 0 MCLK conditional requests are disabled 1 MCLK conditional requests are enabled
ACLKREQEN — 0 ACLK conditional requests are disabled 1 ACLK conditional requests are enabled
 
struct UCS.UCSCTL9_t

Unified Clock System Control 9 Register

XDCscript usage meta-domain
var obj = new UCS.UCSCTL9_t;
 
    obj.XT2BYPASSLV = UCS.XT2BYPASSLV_t  ...
    // Selects XT2 bypass input swing level. Must be set for reduced swing operation. 0 Input range from 0 to DVCC 1 Input range from 0 to DVIO
    obj.XT1BYPASSLV = UCS.XT1BYPASSLV_t  ...
    // Selects XT1 bypass input swing level. Must be set for reduced swing operation. 0 Input range from 0 to DVCC 1 Input range from 0 to DVIO
 
FIELDS
XT2BYPASSLV — 0 Input range from 0 to DVCC 1 Input range from 0 to DVIO
XT1BYPASSLV — 0 Input range from 0 to DVCC 1 Input range from 0 to DVIO
 
UCS.getAll()  // module-wide

Find all peripherals of a certain type

XDCscript usage meta-domain
UCS.getAll() returns IPeripheral.Instance[]
 
DETAILS
The type of the peripherals returned is defined by the type of the caller.
RETURNS
Returns an array of IPeripheral instances
 
UCS.getRegisters()  // module-wide

Find all registers defined by the peripheral

XDCscript usage meta-domain
UCS.getRegisters() returns String[]
 
RETURNS
Returns an array of register names
Instance Config Parameters

XDCscript usage meta-domain
var params = new UCS.Params;
// Instance config-params object
    params.ACLKHz = Float undefined;
    // ACLK frequency in Hertz
    params.DCOCLKDIVHz = Float undefined;
    // Divided DCO clock frequency in Hertz
    params.DCOCLKHz = Float 1000000;
    // DCO clock frequency in Hertz
    params.MCLKHz = Float undefined;
    // MCLK frequency in Hertz
    params.REFOCLKHz = Float 32768;
    // 
    params.SMCLKHz = Float undefined;
    // SMCLK frequency in Hertz
    params.UCSCTL0 = UCS.UCSCTL0_t {
    // Unified Clock System Control 0 Register
        DCO0: UCS.DCO0_OFF,
        DCO1: UCS.DCO1_OFF,
        DCO2: UCS.DCO2_OFF,
        DCO3: UCS.DCO3_OFF,
        DCO4: UCS.DCO4_OFF,
        MOD0: UCS.MOD0_OFF,
        MOD1: UCS.MOD1_OFF,
        MOD2: UCS.MOD2_OFF,
        MOD3: UCS.MOD3_OFF,
        MOD4: UCS.MOD4_OFF
    };
    params.UCSCTL1 = UCS.UCSCTL1_t {
    // Unified Clock System Control 1 Register
        DCORSEL: UCS.DCORSEL_2,
        DISMOD: UCS.DISMOD_OFF
    };
    params.UCSCTL2 = UCS.UCSCTL2_t {
    // Unified Clock System Control 2 Register
        FLLD: UCS.FLLD_1,
        FLLN0: UCS.FLLN0,
        FLLN1: UCS.FLLN1,
        FLLN2: UCS.FLLN2,
        FLLN3: UCS.FLLN3,
        FLLN4: UCS.FLLN4,
        FLLN5: UCS.FLLN5_OFF,
        FLLN6: UCS.FLLN6_OFF,
        FLLN7: UCS.FLLN7_OFF,
        FLLN8: UCS.FLLN8_OFF,
        FLLN9: UCS.FLLN9_OFF
    };
    params.UCSCTL3 = UCS.UCSCTL3_t {
    // Unified Clock System Control 3 Register
        SELREF: UCS.SELREF_0,
        FLLREFDIV: UCS.FLLREFDIV_0
    };
    params.UCSCTL4 = UCS.UCSCTL4_t {
    // Unified Clock System Control 4 Register
        SELA: UCS.SELA_0,
        SELS: UCS.SELS_4,
        SELM: UCS.SELM_4
    };
    params.UCSCTL5 = UCS.UCSCTL5_t {
    // Unified Clock System Control 5 Register
        DIVPA: UCS.DIVPA_0,
        DIVA: UCS.DIVA_0,
        DIVS: UCS.DIVS_0,
        DIVM: UCS.DIVM_0
    };
    params.UCSCTL6 = UCS.UCSCTL6_t {
    // Unified Clock System Control 6 Register
        XT2DRIVE: UCS.XT2DRIVE_3,
        XT2BYPASS: UCS.XT2BYPASS_OFF,
        XT2OFF: UCS.XT2OFF,
        XT1DRIVE: UCS.XT1DRIVE_3,
        XTS: UCS.XTS,
        XT1BYPASS: UCS.XT1BYPASS,
        XCAP: UCS.XCAP_3,
        SMCLKOFF: UCS.SMCLKOFF_OFF,
        XT1OFF: UCS.XT1OFF
    };
    params.UCSCTL7 = UCS.UCSCTL7_t {
    // Unified Clock System Control 7 Register
        XT2OFFG: UCS.XT2OFFG_OFF,
        XT1HFOFFG: UCS.XT1HFOFFG_OFF,
        XT1LFOFFG: UCS.XT1LFOFFG,
        DCOFFG: UCS.DCOFFG
    };
    params.UCSCTL8 = UCS.UCSCTL8_t {
    // Unified Clock System Control 8 Register
        MODOSCREQEN: UCS.MODOSCREQEN_OFF,
        SMCLKREQEN: UCS.SMCLKREQEN,
        MCLKREQEN: UCS.MCLKREQEN,
        ACLKREQEN: UCS.ACLKREQEN
    };
    params.UCSCTL9 = UCS.UCSCTL9_t {
    // Unified Clock System Control 9 Register
        XT2BYPASSLV: UCS.XT2BYPASSLV_OFF,
        XT1BYPASSLV: UCS.XT1BYPASSLV_OFF
    };
    params.UCS_ACLKREQEN = UCS.ACLKREQEN_t UCS.ACLKREQEN;
    // ACLK clock request enable. Setting this enables conditional module requests for ACLK 0 ACLK conditional requests are disabled. 1 ACLK conditional requests are enabled
    params.UCS_ACLK_SOURCE = UCS.UCS_CLK_SOURCE_t UCS.UCS_XT1CLK_SELECT;
    // ACLK clock source select
    params.UCS_ACLK_SRC_DIVIDER = UCS.UCS_CLK_SRC_DIVIDER_t UCS.UCS_CLOCK_DIVIDER_1;
    // ACLK clock source divider select
    params.UCS_FLL_FREQ = Float 0;
    // Set FLL target frequency
    params.UCS_FLL_RATIO = UInt 31;
    // FLLN value
    params.UCS_FLL_REF_CLK_SOURCE = UCS.UCS_CLK_SOURCE_t UCS.UCS_XT1CLK_SELECT;
    // FLL reference clock source select
    params.UCS_FLL_REF_SRC_DIVIDER = UCS.UCS_CLK_SRC_DIVIDER_t UCS.UCS_CLOCK_DIVIDER_1;
    // FLL reference clock source divider select
    params.UCS_MCLKREQEN = UCS.MCLKREQEN_t UCS.MCLKREQEN;
    // MCLK clock request enable. Setting this enables conditional module requests for MCLK 0 MCLK conditional requests are disabled. 1 MCLK conditional requests are enabled
    params.UCS_MCLK_SOURCE = UCS.UCS_CLK_SOURCE_t UCS.UCS_DCOCLKDIV_SELECT;
    // MCLK clock source select
    params.UCS_MCLK_SRC_DIVIDER = UCS.UCS_CLK_SRC_DIVIDER_t UCS.UCS_CLOCK_DIVIDER_1;
    // MCLK clock source divider select
    params.UCS_MODOSCREQEN = UCS.MODOSCREQEN_t UCS.MODOSCREQEN_OFF;
    // MODOSC clock request enable. Setting this enables conditional module requests for MODOSC. 0 MODOSC conditional requests are disabled. 1 MODOSC conditional requests are enabled
    params.UCS_PACLK_SRC_DIVIDER = UCS.UCS_CLK_SRC_DIVIDER_t UCS.UCS_CLOCK_DIVIDER_1;
    // External pin ACLK clock source divider select
    params.UCS_SMCLKOFF = Bool false;
    // Turns OFF SMCLK using the SMCLKOFF bit 0 SMCLK On 1 SMCLK Off
    params.UCS_SMCLKREQEN = UCS.SMCLKREQEN_t UCS.SMCLKREQEN;
    // SMCLK clock request enable. Setting this enables conditional module requests for SMCLK. 0 SMCLK conditional requests are disabled. 1 SMCLK conditional requests are enabled
    params.UCS_SMCLK_SOURCE = UCS.UCS_CLK_SOURCE_t UCS.UCS_DCOCLKDIV_SELECT;
    // SMCLK clock source select
    params.UCS_SMCLK_SRC_DIVIDER = UCS.UCS_CLK_SRC_DIVIDER_t UCS.UCS_CLOCK_DIVIDER_1;
    // SMCLK clock source divider select
    params.UCS_XCAP = UCS.UCS_XCAP_t UCS.UCS_XCAP_3;
    // Set oscillator capacitor. Available only in LF mode. See device-specific datasheet for actual values
    params.UCS_XT1BYPASS = Bool false;
    // Set XT1 in bypass mode. The frequency input at XIN1 pin requires 0 to VCC
    params.UCS_XT1_DRIVE = UCS.XT1DRIVE_t UCS.XT1DRIVE_3;
    // Set XT1 drive strength
    params.UCS_XT2BYPASS = Bool false;
    // Set XT2 in bypass mode. The frequency input at XIN2 pin requires 0 to VCC
    params.UCS_XT2_DRIVE = UCS.XT2DRIVE_t UCS.XT2DRIVE_3;
    // Set XT2 drive strength
    params.VLOCLKHz = Float 12000;
    // 
    params.WATCHCRYSTALCLKHz = Float 32768;
    // 
    params.XT1CLKHz = Float 0;
    // 
    params.XT2CLKHz = Float 0;
    // 
    params.baseAddr = UInt undefined;
    // Address of the peripheral's control register
    params.baseAddress = String "__MSP430_BASEADDRESS_UCS__";
    // UCS base address
    params.forceSetDefaultRegister = UCS.ForceSetDefaultRegister_t[] [
    // Determine if each Register needs to be forced set or not
        {
            register: "UCS_SMCLKREQEN",
            regForceSet: false
        },
        {
            register: "UCS_MCLKREQEN",
            regForceSet: false
        },
        {
            register: "UCS_ACLKREQEN",
            regForceSet: false
        },
        {
            register: "UCS_MODOSCREQEN",
            regForceSet: false
        }
    ];
    params.hasAllCal = Bool false;
    // Specify if device has all calibration constants
    params.hasHFXT1 = Bool false;
    // Specify if HFXT1 is available on the device
    params.hasRosc = Bool false;
    // Specify if Rosc is available on the device
    params.hasVLO = Bool false;
    // Specify if VLO is available on the device
    params.hasXT2 = Bool false;
    // Specify if XT2 is available on the device
    params.maxCpuFrequency = Float 0;
    // Maximum CPU frequency in Hertz
    params.name = String undefined;
    // Specific peripheral name given by the device
    params.owner = String undefined;
    // String specifying the entity that manages the peripheral
 
config UCS.ACLKHz  // instance

ACLK frequency in Hertz

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
const params.ACLKHz = Float computed value;
 
 
config UCS.DCOCLKDIVHz  // instance

Divided DCO clock frequency in Hertz

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
const params.DCOCLKDIVHz = Float computed value;
 
 
config UCS.DCOCLKHz  // instance

DCO clock frequency in Hertz

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
const params.DCOCLKHz = Float 1000000;
 
 
config UCS.MCLKHz  // instance

MCLK frequency in Hertz

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
const params.MCLKHz = Float computed value;
 
 
config UCS.REFOCLKHz  // instance
XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.REFOCLKHz = Float 32768;
 
 
config UCS.SMCLKHz  // instance

SMCLK frequency in Hertz

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
const params.SMCLKHz = Float computed value;
 
 
config UCS.UCSCTL0  // instance

Unified Clock System Control 0 Register

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCSCTL0 = UCS.UCSCTL0_t {
    DCO0: UCS.DCO0_OFF,
    DCO1: UCS.DCO1_OFF,
    DCO2: UCS.DCO2_OFF,
    DCO3: UCS.DCO3_OFF,
    DCO4: UCS.DCO4_OFF,
    MOD0: UCS.MOD0_OFF,
    MOD1: UCS.MOD1_OFF,
    MOD2: UCS.MOD2_OFF,
    MOD3: UCS.MOD3_OFF,
    MOD4: UCS.MOD4_OFF
};
 
 
config UCS.UCSCTL1  // instance

Unified Clock System Control 1 Register

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCSCTL1 = UCS.UCSCTL1_t {
    DCORSEL: UCS.DCORSEL_2,
    DISMOD: UCS.DISMOD_OFF
};
 
 
config UCS.UCSCTL2  // instance

Unified Clock System Control 2 Register

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCSCTL2 = UCS.UCSCTL2_t {
    FLLD: UCS.FLLD_1,
    FLLN0: UCS.FLLN0,
    FLLN1: UCS.FLLN1,
    FLLN2: UCS.FLLN2,
    FLLN3: UCS.FLLN3,
    FLLN4: UCS.FLLN4,
    FLLN5: UCS.FLLN5_OFF,
    FLLN6: UCS.FLLN6_OFF,
    FLLN7: UCS.FLLN7_OFF,
    FLLN8: UCS.FLLN8_OFF,
    FLLN9: UCS.FLLN9_OFF
};
 
 
config UCS.UCSCTL3  // instance

Unified Clock System Control 3 Register

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCSCTL3 = UCS.UCSCTL3_t {
    SELREF: UCS.SELREF_0,
    FLLREFDIV: UCS.FLLREFDIV_0
};
 
 
config UCS.UCSCTL4  // instance

Unified Clock System Control 4 Register

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCSCTL4 = UCS.UCSCTL4_t {
    SELA: UCS.SELA_0,
    SELS: UCS.SELS_4,
    SELM: UCS.SELM_4
};
 
 
config UCS.UCSCTL5  // instance

Unified Clock System Control 5 Register

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCSCTL5 = UCS.UCSCTL5_t {
    DIVPA: UCS.DIVPA_0,
    DIVA: UCS.DIVA_0,
    DIVS: UCS.DIVS_0,
    DIVM: UCS.DIVM_0
};
 
 
config UCS.UCSCTL6  // instance

Unified Clock System Control 6 Register

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCSCTL6 = UCS.UCSCTL6_t {
    XT2DRIVE: UCS.XT2DRIVE_3,
    XT2BYPASS: UCS.XT2BYPASS_OFF,
    XT2OFF: UCS.XT2OFF,
    XT1DRIVE: UCS.XT1DRIVE_3,
    XTS: UCS.XTS,
    XT1BYPASS: UCS.XT1BYPASS,
    XCAP: UCS.XCAP_3,
    SMCLKOFF: UCS.SMCLKOFF_OFF,
    XT1OFF: UCS.XT1OFF
};
 
 
config UCS.UCSCTL7  // instance

Unified Clock System Control 7 Register

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCSCTL7 = UCS.UCSCTL7_t {
    XT2OFFG: UCS.XT2OFFG_OFF,
    XT1HFOFFG: UCS.XT1HFOFFG_OFF,
    XT1LFOFFG: UCS.XT1LFOFFG,
    DCOFFG: UCS.DCOFFG
};
 
 
config UCS.UCSCTL8  // instance

Unified Clock System Control 8 Register

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCSCTL8 = UCS.UCSCTL8_t {
    MODOSCREQEN: UCS.MODOSCREQEN_OFF,
    SMCLKREQEN: UCS.SMCLKREQEN,
    MCLKREQEN: UCS.MCLKREQEN,
    ACLKREQEN: UCS.ACLKREQEN
};
 
 
config UCS.UCSCTL9  // instance

Unified Clock System Control 9 Register

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCSCTL9 = UCS.UCSCTL9_t {
    XT2BYPASSLV: UCS.XT2BYPASSLV_OFF,
    XT1BYPASSLV: UCS.XT1BYPASSLV_OFF
};
 
 
config UCS.UCS_ACLKREQEN  // instance

ACLK clock request enable. Setting this enables conditional module requests for ACLK 0 ACLK conditional requests are disabled. 1 ACLK conditional requests are enabled

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_ACLKREQEN = UCS.ACLKREQEN_t UCS.ACLKREQEN;
 
 
config UCS.UCS_ACLK_SOURCE  // instance

ACLK clock source select

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_ACLK_SOURCE = UCS.UCS_CLK_SOURCE_t UCS.UCS_XT1CLK_SELECT;
 
 
config UCS.UCS_ACLK_SRC_DIVIDER  // instance

ACLK clock source divider select

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_ACLK_SRC_DIVIDER = UCS.UCS_CLK_SRC_DIVIDER_t UCS.UCS_CLOCK_DIVIDER_1;
 
 
config UCS.UCS_FLL_FREQ  // instance

Set FLL target frequency

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_FLL_FREQ = Float 0;
 
 
config UCS.UCS_FLL_RATIO  // instance

FLLN value

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_FLL_RATIO = UInt 31;
 
 
config UCS.UCS_FLL_REF_CLK_SOURCE  // instance

FLL reference clock source select

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_FLL_REF_CLK_SOURCE = UCS.UCS_CLK_SOURCE_t UCS.UCS_XT1CLK_SELECT;
 
 
config UCS.UCS_FLL_REF_SRC_DIVIDER  // instance

FLL reference clock source divider select

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_FLL_REF_SRC_DIVIDER = UCS.UCS_CLK_SRC_DIVIDER_t UCS.UCS_CLOCK_DIVIDER_1;
 
 
config UCS.UCS_MCLKREQEN  // instance

MCLK clock request enable. Setting this enables conditional module requests for MCLK 0 MCLK conditional requests are disabled. 1 MCLK conditional requests are enabled

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_MCLKREQEN = UCS.MCLKREQEN_t UCS.MCLKREQEN;
 
 
config UCS.UCS_MCLK_SOURCE  // instance

MCLK clock source select

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
 
 
config UCS.UCS_MCLK_SRC_DIVIDER  // instance

MCLK clock source divider select

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_MCLK_SRC_DIVIDER = UCS.UCS_CLK_SRC_DIVIDER_t UCS.UCS_CLOCK_DIVIDER_1;
 
 
config UCS.UCS_MODOSCREQEN  // instance

MODOSC clock request enable. Setting this enables conditional module requests for MODOSC. 0 MODOSC conditional requests are disabled. 1 MODOSC conditional requests are enabled

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_MODOSCREQEN = UCS.MODOSCREQEN_t UCS.MODOSCREQEN_OFF;
 
 
config UCS.UCS_PACLK_SRC_DIVIDER  // instance

External pin ACLK clock source divider select

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_PACLK_SRC_DIVIDER = UCS.UCS_CLK_SRC_DIVIDER_t UCS.UCS_CLOCK_DIVIDER_1;
 
 
config UCS.UCS_SMCLKOFF  // instance

Turns OFF SMCLK using the SMCLKOFF bit 0 SMCLK On 1 SMCLK Off

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_SMCLKOFF = Bool false;
 
 
config UCS.UCS_SMCLKREQEN  // instance

SMCLK clock request enable. Setting this enables conditional module requests for SMCLK. 0 SMCLK conditional requests are disabled. 1 SMCLK conditional requests are enabled

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_SMCLKREQEN = UCS.SMCLKREQEN_t UCS.SMCLKREQEN;
 
 
config UCS.UCS_SMCLK_SOURCE  // instance

SMCLK clock source select

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_SMCLK_SOURCE = UCS.UCS_CLK_SOURCE_t UCS.UCS_DCOCLKDIV_SELECT;
 
 
config UCS.UCS_SMCLK_SRC_DIVIDER  // instance

SMCLK clock source divider select

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_SMCLK_SRC_DIVIDER = UCS.UCS_CLK_SRC_DIVIDER_t UCS.UCS_CLOCK_DIVIDER_1;
 
 
config UCS.UCS_XCAP  // instance

Set oscillator capacitor. Available only in LF mode. See device-specific datasheet for actual values

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_XCAP = UCS.UCS_XCAP_t UCS.UCS_XCAP_3;
 
 
config UCS.UCS_XT1BYPASS  // instance

Set XT1 in bypass mode. The frequency input at XIN1 pin requires 0 to VCC

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_XT1BYPASS = Bool false;
 
 
config UCS.UCS_XT1_DRIVE  // instance

Set XT1 drive strength

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_XT1_DRIVE = UCS.XT1DRIVE_t UCS.XT1DRIVE_3;
 
 
config UCS.UCS_XT2BYPASS  // instance

Set XT2 in bypass mode. The frequency input at XIN2 pin requires 0 to VCC

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_XT2BYPASS = Bool false;
 
 
config UCS.UCS_XT2_DRIVE  // instance

Set XT2 drive strength

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.UCS_XT2_DRIVE = UCS.XT2DRIVE_t UCS.XT2DRIVE_3;
 
 
config UCS.VLOCLKHz  // instance
XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.VLOCLKHz = Float 12000;
 
 
config UCS.WATCHCRYSTALCLKHz  // instance
XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.WATCHCRYSTALCLKHz = Float 32768;
 
 
config UCS.XT1CLKHz  // instance
XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.XT1CLKHz = Float 0;
 
 
config UCS.XT2CLKHz  // instance
XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.XT2CLKHz = Float 0;
 
 
config UCS.baseAddr  // instance

Address of the peripheral's control register

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.baseAddr = UInt undefined;
 
DETAILS
A peripheral's registers are commonly accessed through a structure that defines the offsets of a particular register from the lowest address mapped to a peripheral. That lowest address is specified by this parameter.
 
config UCS.baseAddress  // instance

UCS base address

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.baseAddress = String "__MSP430_BASEADDRESS_UCS__";
 
 
config UCS.forceSetDefaultRegister  // instance

Determine if each Register needs to be forced set or not

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
const params.forceSetDefaultRegister = UCS.ForceSetDefaultRegister_t[] [
    {
        register: "UCS_SMCLKREQEN",
        regForceSet: false
    },
    {
        register: "UCS_MCLKREQEN",
        regForceSet: false
    },
    {
        register: "UCS_ACLKREQEN",
        regForceSet: false
    },
    {
        register: "UCS_MODOSCREQEN",
        regForceSet: false
    }
];
 
 
config UCS.hasAllCal  // instance

Specify if device has all calibration constants

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.hasAllCal = Bool false;
 
DETAILS
G1 devices do not.
 
config UCS.hasHFXT1  // instance

Specify if HFXT1 is available on the device

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.hasHFXT1 = Bool false;
 
DETAILS
Not all devices have high frequency clock. This specifies if it is available for a particular device.
 
config UCS.hasRosc  // instance

Specify if Rosc is available on the device

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.hasRosc = Bool false;
 
DETAILS
Not all devices have Rosc circuitry. This specifies if it is available for a particular device.
 
config UCS.hasVLO  // instance

Specify if VLO is available on the device

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.hasVLO = Bool false;
 
DETAILS
Not all devices have very low frequency clock VLO. This specifies if it is available for a particular device.
 
config UCS.hasXT2  // instance

Specify if XT2 is available on the device

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.hasXT2 = Bool false;
 
DETAILS
Not all devices have XT2 clock available. This specifies if it is available for a particular device.
 
config UCS.maxCpuFrequency  // instance

Maximum CPU frequency in Hertz

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.maxCpuFrequency = Float 0;
 
 
config UCS.name  // instance

Specific peripheral name given by the device

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.name = String undefined;
 
DETAILS
Devices can have more than one peripheral of the same type. In such cases, device data sheets give different names to the instances of a same peripheral. For example, the name for a timer module could be TimerA3, and a device that has two such timers can name them TA0 and TA1.
 
config UCS.owner  // instance

String specifying the entity that manages the peripheral

XDCscript usage meta-domain
var params = new UCS.Params;
  ...
params.owner = String undefined;
 
 
UCS.computeDCOCLKHz()  // instance

Initialize to the nearest available DCO clock frequency

XDCscript usage meta-domain
inst.computeDCOCLKHz(Float DCOCLKHz) returns Void
 
generated on Thu, 27 Sep 2012 23:23:49 GMT