Lets user code receive a notification whenever a
config param of a module or instance is read or modified.
config GetSet.debug // module-wide |
|
Print execution trace info showing the flow of getters and setters
XDCscript usage |
meta-domain |
GetSet.debug = Bool false;
config GetSet.maxIterations // module-wide |
|
Limit the number of iterations allowed for a group to converge, to
help debug. The default value of 0 means no limit
XDCscript usage |
meta-domain |
GetSet.maxIterations = Int 0;
config GetSet.maxStackDepth // module-wide |
|
Set the maximum allowed depth of recursively nested setters, as
a debugging aid. The default value of 0 means no limit
XDCscript usage |
meta-domain |
GetSet.maxStackDepth = Int 0;
GetSet.createGroup() // module-wide |
|
Create a group of related setter functions
XDCscript usage |
meta-domain |
GetSet.createGroup() returns Any
DETAILS
The purpose of a group is to control interactions between setters.
If each setter acts like an interrupt, then a group is like an
interrupt controller that determines when setters are permitted
to run.
Each group is non-reentrant. Once any setter in the group is
running, it runs to completion before any other setter in the
same group may run. This allows the setters to modify internal
state without interference from other setters that operate on
the same internal state.
Each group runs to completion. When a setter in the group runs, it
might modify other config params and cause further setters in the
same group to run. All of these complete before control is returned
to the original execution flow. From the point of view of code
outside the group, all the setters ran as an atomic operation.
Groups may be interrupted. When a setter modifies a config param
that is being monitored by a second group, the second group starts
running immediately. It will run to completion before returning
control to the first group. So the first group sees the second
group as atomic. This allows groups to be tested independently,
and combined without affecting their behavior.
Cycles aren't permitted in the execution flow between groups. If a
setter gets triggered from a group that has already been interrupted,
it is deferred and run when control eventually returns to its own
group. Cycles between groups can break the appearance of atomic
execution, and so should be avoided when possible.
RETURNS
A Java object of class
Group.
Can then use Group.onSet() to add functions to the group.
EXAMPLE
The following example code forces the values of the config params
ModA.a and ModB.b to be equal:
var group = GetSet.createGroup();
group.onSet(ModA, "a", function aToB(){ ModB.b = ModA.a; });
group.onSet(ModB, "b", function bToA(){ ModA.a = ModB.b; });
GetSet.init() // module-wide |
|
Add support for getters and setters to all fields of an object
XDCscript usage |
meta-domain |
GetSet.init(Any obj) returns Any
DETAILS
Initializes getter and setter support for every field of
the object. The object can be a module, instance, or structure.
This is a convenience function. The onSet and onGet functions
already add support to the one field of interest. The init
function is useful mostly to make fields visible to global setters
and getters, for example for debugging.
GetSet.onGet() // module-wide |
|
Add a getter function to a field
XDCscript usage |
meta-domain |
GetSet.onGet(Any obj, Any sel, Any getter) returns Any
DETAILS
Each getter acts like an interrupt that is triggered by a read
a field of an object. The field could be a config param of a module
or an instance, or a field of a struct.
EXAMPLE
The following example prints a message on any read of a
config param named cfg in module pkg.Mod:
GetSet.onGet(Mod, "cfg", function(sel, val) {
// prints "pkg.Mod.cfg returned <value>"
print(this.$name + "." + sel + " returned " + val);
});
GetSet.onSet() // module-wide |
|
Add a setter function to a field
XDCscript usage |
meta-domain |
GetSet.onSet(Any obj, Any sel, Any setter) returns Any
DETAILS
Each setter acts like an interrupt that is triggered by modifying
a field of an object. The field could be a config param of a module
or an instance, or a field of a struct.
Setters execute only when the field actually changes value. They do
not execute if the field's current value is written back to it.
Setters may themselves modify fields, and so trigger other setters.
The original execution flow resumes when all fields stop changing
value. In the case of cycles between setters, typically this means
that at least one setter executes twice and makes no further
changes the second time through.
If the setter throws a JavaScript Error or Java exception, then
the field's original value is restored. The exception bubbles back
through the call stack, so that if a setter caused a cascade of
changes, all are restored to their original values.
EXAMPLE
The following example prints a message on any write to a
config param named cfg in module pkg.Mod:
GetSet.onSet(Mod, "cfg", function(sel, val, oldVal, exception) {
// prints "pkg.Mod.cfg set to <value>"
print(this.$name + "." + sel + " changed to " + val);
// prints previous value before change
print(" was " + oldVal);
});
The following example makes it an error to change Mod.cfg:
GetSet.onSet(Mod, "cfg", function(sel, val, oldVal, exception) {
// don't throw an exception if already recovering from one
if (!exception) {
throw new Error("You'll never change me!");
}
});