enum IUSCI.UC7BIT_t |
![](../../../../../Arrow_up.png) |
Character length. Selects 7-bit or 8-bit character length
enum UC7BIT_t {
UC7BIT_OFF,
// 8-bit
UC7BIT
// 7-bit
};
enum IUSCI.UCADDR_t |
![](../../../../../Arrow_up.png) |
Address received in address-bit multiprocessor mode
enum UCADDR_t {
UCADDR_OFF,
// Received character is data
UCADDR
// Received character is an address
};
enum IUSCI.UCBRKIE_t |
![](../../../../../Arrow_up.png) |
Receive break character interrupt-enable
enum UCBRKIE_t {
UCBRKIE_OFF,
// Received break characters do not set UCAxRXIFG
UCBRKIE
// Received break characters set UCAxRXIFG
};
enum IUSCI.UCBRK_t |
![](../../../../../Arrow_up.png) |
Break detect flag
enum UCBRK_t {
UCBRK_OFF,
// No break condition
UCBRK
// Break condition occurred
};
enum IUSCI.UCBUSY_t |
![](../../../../../Arrow_up.png) |
USCI busy. This bit indicates if a transmit or receive operation is in progress
enum UCBUSY_t {
UCBUSY_OFF,
// USCI inactive
UCBUSY
// USCI transmitting or receiving
};
enum IUSCI.UCDORM_t |
![](../../../../../Arrow_up.png) |
Dormant. Puts USCI into sleep mode
enum UCDORM_t {
UCDORM_OFF,
// Not dormant. All received characters will set UCAxRXIFG
UCDORM
// Dormant. Only characters that are preceded by an idle-line or with
address bit set will set UCAxRXIFG. In UART mode with automatic baud
rate detection only the combination of a break and synch field will set
UCAxRXIFG
};
enum IUSCI.UCFE_t |
![](../../../../../Arrow_up.png) |
Framing error flag
enum UCFE_t {
UCFE_OFF,
// 0 No error
UCFE
// Character received with low stop bit
};
enum IUSCI.UCIDLE_t |
![](../../../../../Arrow_up.png) |
Idle line detected in idle-line multiprocessor mode
enum UCIDLE_t {
UCIDLE_OFF,
// No idle line detected
UCIDLE
// Idle line detected
};
enum IUSCI.UCLISTEN_t |
![](../../../../../Arrow_up.png) |
Listen enable. The UCLISTEN bit selects loopback mode
enum UCLISTEN_t {
UCLISTEN_OFF,
// Disabled
UCLISTEN
// Enabled. UCAxTXD is internally fed back to the receiver
};
enum IUSCI.UCMODE_SYNC_t |
![](../../../../../Arrow_up.png) |
USCI mode. The UCMODEx bits select the synchronous mode when UCSYNC = 1
enum UCMODE_SYNC_t {
UCMODE_0,
// 3-Pin SPI
UCMODE_1,
// 4-Pin SPI with UCxSTE active high: slave enabled when UCxSTE = 1
UCMODE_2,
// 4-Pin SPI with UCxSTE active low: slave enabled when UCxSTE = 0
UCMODE_3
// I2C Mode
};
enum IUSCI.UCMSB_t |
![](../../../../../Arrow_up.png) |
MSB first select. Controls the direction of the receive and transmit shift register
enum UCMSB_t {
UCMSB_OFF,
// LSB first
UCMSB
// MSB first
};
enum IUSCI.UCOE_t |
![](../../../../../Arrow_up.png) |
Overrun error flag
enum UCOE_t {
UCOE_OFF,
// No error
UCOE
// Overrun error occurred
};
enum IUSCI.UCPE_t |
![](../../../../../Arrow_up.png) |
Parity error flag. When UCPEN = 0, UCPE is read as 0
enum UCPE_t {
UCPE_OFF,
// No error
UCPE
// Character received with parity error
};
enum IUSCI.UCRXEIE_t |
![](../../../../../Arrow_up.png) |
Receive erroneous-character interrupt-enable
enum UCRXEIE_t {
UCRXEIE_OFF,
// Erroneous characters rejected and UCAxRXIFG is not set
UCRXEIE
// Erroneous characters received will set UCAxRXIFG
};
enum IUSCI.UCRXERR_t |
![](../../../../../Arrow_up.png) |
Bit 2 Receive error flag. This bit indicates a character was received with error(s).
When UCRXERR = 1, on or more error flags (UCFE, UCPE, UCOE) is also
set. UCRXERR is cleared when UCAxRXBUF is read
enum UCRXERR_t {
UCRXERR_OFF,
// No receive errors detected
UCRXERR
// Receive error detected
};
enum IUSCI.UCSWRST_t |
![](../../../../../Arrow_up.png) |
Software reset enable
enum UCSWRST_t {
UCSWRST_OFF,
// Disabled. USCI reset released for operation
UCSWRST
// Enabled. USCI logic held in reset state
};
enum IUSCI.UCSYNC_t |
![](../../../../../Arrow_up.png) |
Synchronous mode enable
enum UCSYNC_t {
UCSYNC_OFF,
// Asynchronous mode
UCSYNC
// Synchronous Mode
};
enum IUSCI.UCTXADDR_t |
![](../../../../../Arrow_up.png) |
Transmit address. Next frame to be transmitted will be marked as address depending on the selected multiprocessor mode
enum UCTXADDR_t {
UCTXADDR_OFF,
// Next frame transmitted is data
UCTXADDR
// Next frame transmitted is an address
};
enum IUSCI.UCTXBRK_t |
![](../../../../../Arrow_up.png) |
Transmit break. Transmits a break with the next write to the transmit buffer.
In UART mode with automatic baud rate detection 055h must be written
into UCAxTXBUF to generate the required break/synch fields. Otherwise
0h must be written into the transmit buffer
enum UCTXBRK_t {
UCTXBRK_OFF,
// Next frame transmitted is not a break
UCTXBRK
// Next frame transmitted is a break or a break/synch
};
typedef IUSCI.IPeripheralArray |
![](../../../../../Arrow_up.png) |
typedef IUSCI.StringArray |
![](../../../../../Arrow_up.png) |
typedef String StringArray[];
struct IUSCI.ForceSetDefaultRegister_t |
![](../../../../../Arrow_up.png) |
Force Set Default Register
metaonly struct ForceSetDefaultRegister_t {
String register;
Bool regForceSet;
};
DETAILS
Type to store if each register needs to be forced initialized
even if the register is in default state.
SEE
struct IUSCI.regIntVect_t |
![](../../../../../Arrow_up.png) |
Interrupt vector description
metaonly struct regIntVect_t {
String registerName;
String registerDescription;
String isrToggleString;
String priorityName;
Bool interruptEnable;
Bool interruptHandler;
Int priority;
};
DETAILS
Type to describe a single interrupt vector pin and all its possible
configurations.
SEE
IUSCI.getAll() // module-wide |
![](../../../../../Arrow_up.png) |
Find all peripherals of a certain type
DETAILS
The type of the peripherals returned is defined by the type of the
caller.
RETURNS
Returns an array of IPeripheral instances
IUSCI.getRegisters() // module-wide |
![](../../../../../Arrow_up.png) |
Find all registers defined by the peripheral
RETURNS
Returns an array of register names
config IUSCI.UCLKHz // instance |
![](../../../../../Arrow_up.png) |
Stores the UCLK external clock frequency in float
config Float UCLKHz = 1000000;
config IUSCI.name // instance |
![](../../../../../Arrow_up.png) |
Specific peripheral name given by the device
DETAILS
Devices can have more than one peripheral of the same type. In such
cases, device data sheets give different names to the instances of a
same peripheral. For example, the name for a timer module could be
TimerA3, and a device that has two such timers can name them TA0
and TA1.
config IUSCI.owner // instance |
![](../../../../../Arrow_up.png) |
String specifying the entity that manages the peripheral
IUSCI.getUCxxBR0() // instance |
![](../../../../../Arrow_up.png) |
Returns UCxxBR0 register value based on which module
SEE
IUSCI.getUCxxBR1() // instance |
![](../../../../../Arrow_up.png) |
Returns UCxxBR1 register value based on which module
SEE
IUSCI.getUCxxRXIE() // instance |
![](../../../../../Arrow_up.png) |
Gets UCxxRXIE bit
SEE
IUSCI.getUCxxTXIE() // instance |
![](../../../../../Arrow_up.png) |
Gets UCxxTXIE bit
SEE
IUSCI.setUCxxBR0() // instance |
![](../../../../../Arrow_up.png) |
Sets UCxxBR0 register value based on which module
Void setUCxxBR0(Bits8 value);
SEE
IUSCI.setUCxxBR1() // instance |
![](../../../../../Arrow_up.png) |
Sets UCxxBR1 register value based on which module
Void setUCxxBR1(Bits8 value);
SEE
IUSCI.setUCxxRXIE() // instance |
![](../../../../../Arrow_up.png) |
Sets UCxxRXIE bit
Bool setUCxxRXIE(Bool set);
SEE
IUSCI.setUCxxTXIE() // instance |
![](../../../../../Arrow_up.png) |
Sets UCxxTXIE bit
Bool setUCxxTXIE(Bool set);
SEE