metaonly module xdc.bld.Library

Model of a searchable collection of object files

A library is a collection of one or more object files that is searched to resolve undefined references at link time. [ more ... ]
XDCscript usage meta-domain sourced in xdc/bld/Library.xdc
var Library = xdc.useModule('xdc.bld.Library');
module-wide constants & types
        obj.profile// target options profile = String  ...
        obj.aopts// asm options for objects = String  ...
        obj.copts// C/C++ options for objects = String  ...
        obj.defs// definitions for added objects = String  ...
        obj.incs// include options for objects = String  ...
        obj.aropts// library-specific archiver options = String  ...
        obj.suffix// optional suffix of library name; e.g.,".lib" = String  ...
per-instance config parameters
    var params = new Library.Params// Instance config-params object;
        params.attrs// This library's optional attributes = Library.Attrs undefined;
        params.name// The base name of the library = String undefined;
per-instance functions
 
DETAILS
A library is a collection of one or more object files that is searched to resolve undefined references at link time.
Instances of this module represent a target independent collection of object files that implement a single set of APIs. Thus, a library is really a container of target-specific archives which contain the object files necessary to implement a common API. Although, a library may contain target dependent APIs, each library is expected to encapsulate the same basic functionality independent of the target.
Instances must be created via the xdc.bld.PackageContents.addLibrary() function; this ensures that each library created appears in the package's manifest and that it properly "inherits" appropriate default attributes from the containing package.
Library instances are initially create without *any* objects; this ensures that the developer complete control over what objects should be in each library. Thus, even modules declared in a package's specification, package.xdc, must be explicitly added to each library in the package (via addObjects()).
 
struct Library.Attrs

Optional attributes for a Library instance

XDCscript usage meta-domain
var obj = new Library.Attrs;
 
    obj.profile = String  ...
    // target options profile
    obj.aopts = String  ...
    // asm options for objects
    obj.copts = String  ...
    // C/C++ options for objects
    obj.defs = String  ...
    // definitions for added objects
    obj.incs = String  ...
    // include options for objects
    obj.aropts = String  ...
    // library-specific archiver options
    obj.suffix = String  ...
    // optional suffix of library name; e.g.,".lib"
    obj.exportSrc = Bool  ...
    // if true, export library sources to releases
    obj.releases = Release.Instance[]  ...
    // releases this library is a part of
 
FIELDS
incs — This string contains include path options used by the compiler (or assembler) to locate include files; e.g., "-I ../../include -I ../c55xx". Note that the syntax of this string may be target dependent.
defs — This string contains options used by the compiler (or assembler) to define macros; e.g., "-D_C6xxx -DDEBUG=1". Note that the syntax of this string may be target dependent.
aopts — This string contains options used by the assembler to produce object files; e.g., "-mP1". Note that the syntax of this string may be target dependent.
copts — This string contains options used by the C/C++ compiler to produce object files; e.g., "-o3 -mi1". Note that the syntax of this string may be target dependent.
aropts — This string contains options used by the archiver produce archive files; e.g., "-q". Note that the syntax of this string may be target dependent.
exportSrc — If this field is set to true, the sources specified via addObjects() will be part of the releases named in the releases array. If it is unspecified (or set to null) and the release specifies that sources are to be exported, the sources will be part of the release. In all other cases, the sources are not part of the release.
suffix — If this string is set to a non-null value, it specifies the suffix (or extension) of the archive produced. This suffix is used in lieu of the default suffix (".a<targ_suffix>", where <targ_suffix> is the suffix property of the target used to create the archive). So, care must be taken when creating multiple libraries for different targets to ensure that the resulting archive names are unique.
profile — This string names a profile defined by the library's target. The profile specifies a set of compiler, assembler, and archiver options that are to be used when producing the archive. Note that these tool options are in addition to any options specified via aopts, copts, etc.
releases — This array contains releases that will contain the library. Thus, a single library can be part of any set of releases. Each library is always added to the package's "default release" in addition to any releases specified in the releases array.
DETAILS
Unspecified attributes are "inherited" from xdc.bld.PackageContents.Attrs; i.e., if one of fields in this structure is unspecified *and* this field's name matches a field name in xdc.bld.PackageContents.attrs, then this field's value defaults to the value in specified by xdc.bld.PackageContents.attrs. This mechanism makes it possible to establish package-wide default values for any of the "inherited" attributes.
Suppose, for example, that you want all archives in this package to be build with the 'release' profile, but one particular archive must be built with 'debug' (because it is a source example). The following build script fragment shows how this can be accomplished:
      Pkg.attrs.profile = 'release';
      var lib = Pkg.addLibrary('example', ..., {profile: 'debug'});
SEE
Instance Config Parameters

XDCscript usage meta-domain
var params = new Library.Params;
// Instance config-params object
    params.attrs = Library.Attrs undefined;
    // This library's optional attributes
    params.name = String undefined;
    // The base name of the library
    params.target = ITarget.Module undefined;
    // The target used to build objects added to this library
 
config Library.attrs  // instance

This library's optional attributes

XDCscript usage meta-domain
var params = new Library.Params;
  ...
params.attrs = Library.Attrs undefined;
 
DETAILS
These attributes are "inherited" by all objects added to this library; i.e., any object attribute that is undefined but is defined here will be assigned the value from these attributes.
Similarly, any unspecified attributes that also appear in xdc.bld.PackageContents.Attrs are inherited from xdc.bld.PackageContents.attrs.
SEE
 
config Library.name  // instance

The base name of the library

XDCscript usage meta-domain
var params = new Library.Params;
  ...
params.name = String undefined;
 
DETAILS
This name names a sub-directory in the package directory that contains all the object files and archives created for each of the targets specified.
The name of each library is <name>/<name>.a<target_suffix>, where <name> is the base name and <target_suffix> is the suffix property of the target for which the library is built. For example, one is building a "hello" library for big endian C62 the library's file name is "hello/hello.a62e"
 
config Library.target  // instance

The target used to build objects added to this library

XDCscript usage meta-domain
var params = new Library.Params;
  ...
params.target = ITarget.Module undefined;
 
 
Library.addObjects()  // instance

Add specified object to be built and archived into this library

XDCscript usage meta-domain
inst.addObjects(String[] names, Object.Attrs objAttrs) returns Void
 
ARGUMENTS
names — array of base names of the sources of object files to be created and archived into the library. See NOTE in xdc.bld for filename rules.
objAttrs — optional Object.Attrs for the array of objects added; all objects named by names will be given the attributes objAttrs.
DETAILS
Examples
1. Locate a source file whose name starts with "fir" with an extension supported by the library's target, compile it and add to the library lib:
          lib.addObjects(["fir"]);
If fir.c exists compile and add to lib, if fir.asm exists assemble and add to lib, etc. If no such file is located, an warning is emitted.
2. Compile fir.c and iir.c and add to the library lib:
          lib.addObjects(["fir.c", "iir.c"]);
3. Names may include sub-directory prefixes. In this case, the source will be located in a sub-directory of the current package. The following statement declares that the file "foo/fir.c" should be compiled and added to the library lib:
          lib.addObjects(["foo/fir.c"]);
As in the previous examples, the extension ".c" is optional. In case an extension is not supplied, each extension understood by the target will be tried until a source file is located.
4. It is also possible to supply file specific compilation options.
          lib.addObjects(["fir.c", "iir.c"], {defs: "-D_DEBUG"});
In this case, both files fir.c and iir.c will be compiled with the "-D_DEBUG" flag. Any setting of attrs.defs in the library or package is overridden by this definition.
RETURNS
void
THROWS
Error exceptions are thrown for fatal errors
generated on Thu, 06 Sep 2012 00:42:18 GMT