metaonly module ti.catalog.peripherals.hdvicp2.HDVICP2 |
![](../../../../Arrow_up.png) |
HD Video Coprocessor
var HDVICP2 = xdc.useModule('ti.catalog.peripherals.hdvicp2.HDVICP2');
module-wide functions
per-instance config parameters
HDVICP2.getAll() // module-wide |
![](../../../../Arrow_up.png) |
Find all peripherals of a certain type
XDCscript usage |
meta-domain |
DETAILS
The type of the peripherals returned is defined by the type of the
caller.
RETURNS
Returns an array of IPeripheral instances
HDVICP2.getRegisters() // module-wide |
![](../../../../Arrow_up.png) |
Find all registers defined by the peripheral
XDCscript usage |
meta-domain |
HDVICP2.getRegisters() returns String[]
RETURNS
Returns an array of register names
Instance Config Parameters |
![](../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new HDVICP2.Params;
// Instance config-params object
params.baseAddr = UInt undefined;
// Address of the peripheral's control register
params.intNum = UInt undefined;
// Transfer completion Interrupt source number
params.name = String undefined;
// Specific peripheral name given by the device
params.owner = String undefined;
// String specifying the entity that manages the peripheral
config HDVICP2.baseAddr // instance |
![](../../../../Arrow_up.png) |
Address of the peripheral's control register
XDCscript usage |
meta-domain |
var params = new HDVICP2.Params;
...
params.baseAddr = UInt undefined;
DETAILS
A peripheral's registers are commonly accessed through a structure
that defines the offsets of a particular register from the lowest
address mapped to a peripheral. That lowest address is specified by
this parameter.
config HDVICP2.intNum // instance |
![](../../../../Arrow_up.png) |
Transfer completion Interrupt source number
XDCscript usage |
meta-domain |
var params = new HDVICP2.Params;
...
params.intNum = UInt undefined;
config HDVICP2.name // instance |
![](../../../../Arrow_up.png) |
Specific peripheral name given by the device
XDCscript usage |
meta-domain |
var params = new HDVICP2.Params;
...
params.name = String undefined;
DETAILS
Devices can have more than one peripheral of the same type. In such
cases, device data sheets give different names to the instances of a
same peripheral. For example, the name for a timer module could be
TimerA3, and a device that has two such timers can name them TA0
and TA1.
config HDVICP2.owner // instance |
![](../../../../Arrow_up.png) |
String specifying the entity that manages the peripheral
XDCscript usage |
meta-domain |
var params = new HDVICP2.Params;
...
params.owner = String undefined;
generated on Thu, 23 Aug 2012 18:52:41 GMT