metaonly module ti.catalog.msp430.init.Boot |
![](../../../../Arrow_up.png) |
Boot time initialization code manager
The Boot module supports boot initialization for the MSP430 devices.
A special boot init function is created based on the configuration
settings for this module. This function is hooked into the
xdc.runtime.Reset.fxns[] array and called very early at boot time (prior
to cinit processing).
[
more ... ]
var Boot = xdc.useModule('ti.catalog.msp430.init.Boot');
module-wide constants & types
module-wide config parameters
DETAILS
The Boot module supports boot initialization for the MSP430 devices.
A special boot init function is created based on the configuration
settings for this module. This function is hooked into the
xdc.runtime.Reset.fxns[] array and called very early at boot time (prior
to cinit processing).
The code to support the boot module is placed in a separate section
named
".text:bootCodeSection" to allow placement of this section in
the linker .cmd file if necessary. This section is a subsection of the
".text" section so this code will be placed into the .text section unless
explicitly placed, either through
Program.sectMap or through a linker
command file.
generated on Tue, 10 Jul 2012 02:24:07 GMT