metaonly module xdc.services.getset.GetSet

Callback notification on RTSC config parameters

Lets user code receive a notification whenever a config param of a module or instance is read or modified. [ more ... ]
XDCscript usage meta-domain sourced in xdc/services/getset/GetSet.xdc
DETAILS
Lets user code receive a notification whenever a config param of a module or instance is read or modified.
SEE
 
config GetSet.debug  // module-wide

Print execution trace info showing the flow of getters and setters

XDCscript usage meta-domain
GetSet.debug = Bool false;
 
 
config GetSet.maxIterations  // module-wide

Limit the number of iterations allowed for a group to converge, to help debug. The default value of 0 means no limit

XDCscript usage meta-domain
GetSet.maxIterations = Int 0;
 
 
config GetSet.maxStackDepth  // module-wide

Set the maximum allowed depth of recursively nested setters, as a debugging aid. The default value of 0 means no limit

XDCscript usage meta-domain
GetSet.maxStackDepth = Int 0;
 
 
GetSet.createGroup()  // module-wide

Create a group of related setter functions

XDCscript usage meta-domain
GetSet.createGroup() returns Any
 
DETAILS
The purpose of a group is to control interactions between setters. If each setter acts like an interrupt, then a group is like an interrupt controller that determines when setters are permitted to run.
Each group is non-reentrant. Once any setter in the group is running, it runs to completion before any other setter in the same group may run. This allows the setters to modify internal state without interference from other setters that operate on the same internal state.
Each group runs to completion. When a setter in the group runs, it might modify other config params and cause further setters in the same group to run. All of these complete before control is returned to the original execution flow. From the point of view of code outside the group, all the setters ran as an atomic operation.
Groups may be interrupted. When a setter modifies a config param that is being monitored by a second group, the second group starts running immediately. It will run to completion before returning control to the first group. So the first group sees the second group as atomic. This allows groups to be tested independently, and combined without affecting their behavior.
Cycles aren't permitted in the execution flow between groups. If a setter gets triggered from a group that has already been interrupted, it is deferred and run when control eventually returns to its own group. Cycles between groups can break the appearance of atomic execution, and so should be avoided when possible.
RETURNS
A Java object of class Group. Can then use Group.onSet() to add functions to the group.
EXAMPLE
The following example code forces the values of the config params ModA.a and ModB.b to be equal:
    var group = GetSet.createGroup();
    group.onSet(ModA, "a", function aToB(){ ModB.b = ModA.a; });
    group.onSet(ModB, "b", function bToA(){ ModA.a = ModB.b; });
 
GetSet.init()  // module-wide

Add support for getters and setters to all fields of an object

XDCscript usage meta-domain
GetSet.init(Any obj) returns Any
 
DETAILS
Initializes getter and setter support for every field of the object. The object can be a module, instance, or structure.
This is a convenience function. The onSet and onGet functions already add support to the one field of interest. The init function is useful mostly to make fields visible to global setters and getters, for example for debugging.
 
GetSet.onGet()  // module-wide

Add a getter function to a field

XDCscript usage meta-domain
GetSet.onGet(Any obj, Any sel, Any getter) returns Any
 
DETAILS
Each getter acts like an interrupt that is triggered by a read a field of an object. The field could be a config param of a module or an instance, or a field of a struct.
EXAMPLE
The following example prints a message on any read of a config param named cfg in module pkg.Mod:
    GetSet.onGet(Mod, "cfg", function(sel, val) {
        // prints "pkg.Mod.cfg returned <value>"
        print(this.$name + "." + sel + " returned " + val);
    });
 
GetSet.onSet()  // module-wide

Add a setter function to a field

XDCscript usage meta-domain
GetSet.onSet(Any obj, Any sel, Any setter) returns Any
 
DETAILS
Each setter acts like an interrupt that is triggered by modifying a field of an object. The field could be a config param of a module or an instance, or a field of a struct.
Setters execute only when the field actually changes value. They do not execute if the field's current value is written back to it.
Setters may themselves modify fields, and so trigger other setters. The original execution flow resumes when all fields stop changing value. In the case of cycles between setters, typically this means that at least one setter executes twice and makes no further changes the second time through.
If the setter throws a JavaScript Error or Java exception, then the field's original value is restored. The exception bubbles back through the call stack, so that if a setter caused a cascade of changes, all are restored to their original values.
EXAMPLE
The following example prints a message on any write to a config param named cfg in module pkg.Mod:
    GetSet.onSet(Mod, "cfg", function(sel, val, oldVal, exception) {
        // prints "pkg.Mod.cfg set to <value>"
        print(this.$name + "." + sel + " changed to " + val);
        // prints previous value before change
        print("  was " + oldVal);
    });
The following example makes it an error to change Mod.cfg:
    GetSet.onSet(Mod, "cfg", function(sel, val, oldVal, exception) {
        // don't throw an exception if already recovering from one
        if (!exception) {
            throw new Error("You'll never change me!");
        }
    });
generated on Fri, 10 Feb 2012 21:39:31 GMT