metaonly module ti.catalog.msp430.peripherals.communication.USI

Universal Serial Interface

XDCscript usage meta-domain sourced in ti/catalog/msp430/peripherals/communication/USI.xdc
var USI = xdc.useModule('ti.catalog.msp430.peripherals.communication.USI');
module-wide constants & types
 
    values of type USI.USIAL_t// Arbitration lost
        const USI.USIAL// Arbitration lost;
 
    values of type USI.USICKPH_t// Clock phase select
 
        const USI.USICKPL// Inactive state is high;
 
    values of type USI.USICNT0_t// USI bit count - Bit0
        const USI.USICNT0_OFF// USI bit count;
        const USI.USICNT0// USI bit count;
 
    values of type USI.USICNT1_t// USI bit count - Bit1
        const USI.USICNT1_OFF// USI bit count;
        const USI.USICNT1// USI bit count;
 
    values of type USI.USICNT2_t// USI bit count - Bit2
        const USI.USICNT2_OFF// USI bit count;
        const USI.USICNT2// USI bit count;
 
    values of type USI.USICNT3_t// USI bit count - Bit3
        const USI.USICNT3_OFF// USI bit count;
        const USI.USICNT3// USI bit count;
 
    values of type USI.USICNT4_t// USI bit count - Bit4
        const USI.USICNT4_OFF// USI bit count;
        const USI.USICNT4// USI bit count;
 
    values of type USI.USIDIV_t// Clock divider select
        const USI.USIDIV_0// Divide by 1;
        const USI.USIDIV_1// Divide by 2;
        const USI.USIDIV_2// Divide by 4;
        const USI.USIDIV_3// Divide by 8;
        const USI.USIDIV_4// Divide by 16;
        const USI.USIDIV_5// Divide by 32;
        const USI.USIDIV_6// Divide by 64;
        const USI.USIDIV_7// Divide by 128;
 
    values of type USI.USIGE_t// Output latch control
 
    values of type USI.USII2C_t// I2C mode enable
        const USI.USII2C_OFF// I2C mode disabled;
        const USI.USII2C// I2C mode enabled;
 
        const USI.USIIE_OFF// Interrupt disabled;
        const USI.USIIE// Interrupt enabled;
 
 
        const USI.USIIFG// Interrupt pending;
 
        const USI.USILSB_OFF// MSB first;
        const USI.USILSB// LSB first;
 
    values of type USI.USIMST_t// Master select
        const USI.USIMST_OFF// Slave mode;
        const USI.USIMST// Master mode;
 
    values of type USI.USIOE_t// Data output enable
        const USI.USIOE_OFF// Output disabled;
        const USI.USIOE// Output enabled;
 
        const USI.USIPE5// USI function enabled;
 
        const USI.USIPE6// USI function enabled;
 
        const USI.USIPE7// USI function enabled;
 
        const USI.USISCLREL// SCL line is released;
 
        const USI.USISSEL_1// ACLK;
        const USI.USISSEL_2// SMCLK;
        const USI.USISSEL_3// SMCLK;
        const USI.USISSEL_4// USISWCLK bit;
        const USI.USISSEL_5// TACCR0;
        const USI.USISSEL_6// TACCR1;
 
        const USI.USISTP// STOP condition received;
 
 
 
    values of type USI.USISWCLK_t// Software clock
        const USI.USISWCLK// Input clock is high;
 
    values of type USI.USISWRST_t// USI software reset
 
        obj.register = String  ...
        obj.regForceSet = Bool  ...
 
    var obj = new USI.USICKCTL_t// ;
 
    var obj = new USI.USICNT_t// ;
 
    var obj = new USI.USICTL0_t// ;
 
    var obj = new USI.USICTL1_t// ;
module-wide functions
per-instance config parameters
    var params = new USI.Params// Instance config-params object;
            USIDIV: IUSI.USIDIV_0,
            USISSEL: IUSI.USISSEL_0,
            USICKPL: IUSI.USICKPL_OFF,
            USISWCLK: IUSI.USISWCLK_OFF
        };
            USISCLREL: IUSI.USISCLREL_OFF,
            USI16B: IUSI.USI16B_OFF,
            USIIFGCC: IUSI.USIIFGCC_OFF,
            USICNT4: IUSI.USICNT4_OFF,
            USICNT3: IUSI.USICNT3_OFF,
            USICNT2: IUSI.USICNT2_OFF,
            USICNT1: IUSI.USICNT1_OFF,
            USICNT0: IUSI.USICNT0_OFF
        };
            USIPE7: IUSI.USIPE7_OFF,
            USIPE6: IUSI.USIPE6_OFF,
            USIPE5: IUSI.USIPE5_OFF,
            USILSB: IUSI.USILSB_OFF,
            USIMST: IUSI.USIMST_OFF,
            USIGE: IUSI.USIGE_OFF,
            USIOE: IUSI.USIOE_OFF,
            USISWRST: IUSI.USISWRST
        };
            USICKPH: IUSI.USICKPH_OFF,
            USII2C: IUSI.USII2C_OFF,
            USISTTIE: IUSI.USISTTIE_OFF,
            USIIE: IUSI.USIIE_OFF,
            USIAL: IUSI.USIAL_OFF,
            USISTP: IUSI.USISTP_OFF,
            USISTTIFG: IUSI.USISTTIFG_OFF,
            USIIFG: IUSI.USIIFG
        };
            {
                register: "USICTL0",
                regForceSet: false
            },
            {
                register: "USICTL1",
                regForceSet: false
            },
            {
                register: "USICKCTL",
                regForceSet: false
            },
            {
                register: "USICNT",
                regForceSet: false
            }
        ];
        params.name// Specific peripheral name given by the device = String undefined;
        params.owner// String specifying the entity that manages the peripheral = String undefined;
per-instance creation
    var inst = USI.create// Create an instance-object(IClock.Instance clock, params);
per-instance functions
    inst.getUSIIE// Gets USIIE register() returns Bool
    inst.setUSIIE// Sets USIIE register(Bool set) returns Bool
    inst.setUSISTTIE// Sets USISTTIE register(Bool set) returns Bool
 
 
enum USI.USI16B_t

16-bit shift register enable

XDCscript usage meta-domain
values of type USI.USI16B_t
    const USI.USI16B_OFF;
    // 8-bit shift register mode. Low byte register USISRL is used
    const USI.USI16B;
    // 16-bit shift register mode. Both high and low byte registers USISRL and USISRH are used. USISR addresses all 16 bits simultaneously
 
 
enum USI.USIAL_t

Arbitration lost

XDCscript usage meta-domain
values of type USI.USIAL_t
    const USI.USIAL_OFF;
    // No arbitration lost condition
    const USI.USIAL;
    // Arbitration lost
 
 
enum USI.USICKPH_t

Clock phase select

XDCscript usage meta-domain
values of type USI.USICKPH_t
    const USI.USICKPH_OFF;
    // Data is changed on the first SCLK edge and captured on the following edge
    const USI.USICKPH;
    // Data is captured on the first SCLK edge and changed on the following edge
 
 
enum USI.USICKPL_t

Clock polarity select

XDCscript usage meta-domain
values of type USI.USICKPL_t
    const USI.USICKPL_OFF;
    // Inactive state is low
    const USI.USICKPL;
    // Inactive state is high
 
 
enum USI.USICNT0_t

USI bit count - Bit0

XDCscript usage meta-domain
values of type USI.USICNT0_t
    const USI.USICNT0_OFF;
    // USI bit count
    const USI.USICNT0;
    // USI bit count
 
 
enum USI.USICNT1_t

USI bit count - Bit1

XDCscript usage meta-domain
values of type USI.USICNT1_t
    const USI.USICNT1_OFF;
    // USI bit count
    const USI.USICNT1;
    // USI bit count
 
 
enum USI.USICNT2_t

USI bit count - Bit2

XDCscript usage meta-domain
values of type USI.USICNT2_t
    const USI.USICNT2_OFF;
    // USI bit count
    const USI.USICNT2;
    // USI bit count
 
 
enum USI.USICNT3_t

USI bit count - Bit3

XDCscript usage meta-domain
values of type USI.USICNT3_t
    const USI.USICNT3_OFF;
    // USI bit count
    const USI.USICNT3;
    // USI bit count
 
 
enum USI.USICNT4_t

USI bit count - Bit4

XDCscript usage meta-domain
values of type USI.USICNT4_t
    const USI.USICNT4_OFF;
    // USI bit count
    const USI.USICNT4;
    // USI bit count
 
 
enum USI.USIDIV_t

Clock divider select

XDCscript usage meta-domain
values of type USI.USIDIV_t
    const USI.USIDIV_0;
    // Divide by 1
    const USI.USIDIV_1;
    // Divide by 2
    const USI.USIDIV_2;
    // Divide by 4
    const USI.USIDIV_3;
    // Divide by 8
    const USI.USIDIV_4;
    // Divide by 16
    const USI.USIDIV_5;
    // Divide by 32
    const USI.USIDIV_6;
    // Divide by 64
    const USI.USIDIV_7;
    // Divide by 128
 
 
enum USI.USIGE_t

Output latch control

XDCscript usage meta-domain
values of type USI.USIGE_t
    const USI.USIGE_OFF;
    // Output latch enable depends on shift clock
    const USI.USIGE;
    // Output latch always enabled and transparent
 
 
enum USI.USII2C_t

I2C mode enable

XDCscript usage meta-domain
values of type USI.USII2C_t
    const USI.USII2C_OFF;
    // I2C mode disabled
    const USI.USII2C;
    // I2C mode enabled
 
 
enum USI.USIIE_t

USI counter interrupt enable

XDCscript usage meta-domain
values of type USI.USIIE_t
    const USI.USIIE_OFF;
    // Interrupt disabled
    const USI.USIIE;
    // Interrupt enabled
 
 
enum USI.USIIFGCC_t

USI interrupt flag clear control. When USIIFGCC = 1 the USIIFG will not be cleared automatically when USICNTx is written with a value > 0

XDCscript usage meta-domain
values of type USI.USIIFGCC_t
    const USI.USIIFGCC_OFF;
    // USIIFG automatically cleared on USICNTx update
    const USI.USIIFGCC;
    // USIIFG is not cleared automatically
 
 
enum USI.USIIFG_t

USI counter interrupt flag. Set when the USICNTx = 0. Automatically cleared if USICNTx is loaded with a value > 0 when USIIFGCC = 0

XDCscript usage meta-domain
values of type USI.USIIFG_t
    const USI.USIIFG_OFF;
    // No interrupt pending
    const USI.USIIFG;
    // Interrupt pending
 
 
enum USI.USILSB_t

LSB first select. This bit controls the direction of the receive and transmit shift register

XDCscript usage meta-domain
values of type USI.USILSB_t
    const USI.USILSB_OFF;
    // MSB first
    const USI.USILSB;
    // LSB first
 
 
enum USI.USIMST_t

Master select

XDCscript usage meta-domain
values of type USI.USIMST_t
    const USI.USIMST_OFF;
    // Slave mode
    const USI.USIMST;
    // Master mode
 
 
enum USI.USIOE_t

Data output enable

XDCscript usage meta-domain
values of type USI.USIOE_t
    const USI.USIOE_OFF;
    // Output disabled
    const USI.USIOE;
    // Output enabled
 
 
enum USI.USIPE5_t

USI SCLK port enable. Input in SPI slave mode, or I2C mode, output in SPI master mode

XDCscript usage meta-domain
values of type USI.USIPE5_t
    const USI.USIPE5_OFF;
    // USI function disabled
    const USI.USIPE5;
    // USI function enabled
 
 
enum USI.USIPE6_t

USI SDO/SCL port enable. Output in SPI mode, input or open drain output in I2C mode

XDCscript usage meta-domain
values of type USI.USIPE6_t
    const USI.USIPE6_OFF;
    // USI function disabled
    const USI.USIPE6;
    // USI function enabled
 
 
enum USI.USIPE7_t

USI SDI/SDA port enable. Input in SPI mode, input or open drain output in I2C mode

XDCscript usage meta-domain
values of type USI.USIPE7_t
    const USI.USIPE7_OFF;
    // USI function disabled
    const USI.USIPE7;
    // USI function enabled
 
 
enum USI.USISCLREL_t

SCL release. The SCL line is released from low to idle. USISCLREL is cleared if a START condition is detected

XDCscript usage meta-domain
values of type USI.USISCLREL_t
    const USI.USISCLREL_OFF;
    // SCL line is held low if USIIFG is set
    const USI.USISCLREL;
    // SCL line is released
 
 
enum USI.USISSEL_t

Clock source select. Not used in slave mode

XDCscript usage meta-domain
values of type USI.USISSEL_t
    const USI.USISSEL_0;
    // SCLK (Not used in SPI mode)
    const USI.USISSEL_1;
    // ACLK
    const USI.USISSEL_2;
    // SMCLK
    const USI.USISSEL_3;
    // SMCLK
    const USI.USISSEL_4;
    // USISWCLK bit
    const USI.USISSEL_5;
    // TACCR0
    const USI.USISSEL_6;
    // TACCR1
    const USI.USISSEL_7;
    // TACCR2 (Reserved on MSP430F20xx devices)
 
 
enum USI.USISTP_t

STOP condition received. USISTP is automatically cleared if USICNTx is loaded with a value > 0 when USIIFGCC = 0

XDCscript usage meta-domain
values of type USI.USISTP_t
    const USI.USISTP_OFF;
    // No STOP condition received
    const USI.USISTP;
    // STOP condition received
 
 
enum USI.USISTTIE_t

START condition interrupt-enable

XDCscript usage meta-domain
values of type USI.USISTTIE_t
    const USI.USISTTIE_OFF;
    // Interrupt on START condition disabled
    const USI.USISTTIE;
    // Interrupt on START condition enabled
 
 
enum USI.USISTTIFG_t

START condition interrupt flag

XDCscript usage meta-domain
values of type USI.USISTTIFG_t
    const USI.USISTTIFG_OFF;
    // No START condition received. No interrupt pending
    const USI.USISTTIFG;
    // START condition received. Interrupt pending
 
 
enum USI.USISWCLK_t

Software clock

XDCscript usage meta-domain
values of type USI.USISWCLK_t
    const USI.USISWCLK_OFF;
    // Input clock is low
    const USI.USISWCLK;
    // Input clock is high
 
 
enum USI.USISWRST_t

USI software reset

XDCscript usage meta-domain
values of type USI.USISWRST_t
    const USI.USISWRST_OFF;
    // USI released for operation
    const USI.USISWRST;
    // USI logic held in reset state
 
 
struct USI.ForceSetDefaultRegister_t

Force Set Default Register

XDCscript usage meta-domain
var obj = new USI.ForceSetDefaultRegister_t;
 
    obj.register = String  ...
    obj.regForceSet = Bool  ...
 
DETAILS
Type to store if each register needs to be forced initialized even if the register is in default state.
SEE
 
struct USI.USICKCTL_t
XDCscript usage meta-domain
var obj = new USI.USICKCTL_t;
 
    obj.USIDIV = IUSI.USIDIV_t  ...
    // Clock divider select 000 Divide by 1 001 Divide by 2 010 Divide by 4 011 Divide by 8 100 Divide by 16 101 Divide by 32 110 Divide by 64 111 Divide by 128
    obj.USISSEL = IUSI.USISSEL_t  ...
    // Clock source select. Not used in slave mode. 000 SCLK (Not used in SPI mode) 001 ACLK 010 SMCLK 011 SMCLK 100 USISWCLK bit 101 TACCR0 110 TACCR1 111 TACCR2 (Reserved on MSP430F20xx devices)
    obj.USICKPL = IUSI.USICKPL_t  ...
    // Clock polarity select 0 Inactive state is low 1 Inactive state is high
    obj.USISWCLK = IUSI.USISWCLK_t  ...
    // Software clock 0 Input clock is low 1 Input clock is high
 
 
struct USI.USICNT_t
XDCscript usage meta-domain
var obj = new USI.USICNT_t;
 
    obj.USISCLREL = IUSI.USISCLREL_t  ...
    // SCL release. The SCL line is released from low to idle. USISCLREL is cleared if a START condition is detected. 0 SCL line is held low if USIIFG is set 1 SCL line is released
    obj.USI16B = IUSI.USI16B_t  ...
    // 16-bit shift register enable 0 8-bit shift register mode. Low byte register USISRL is used. 1 16-bit shift register mode. Both high and low byte registers USISRL and USISRH are used. USISR addresses all 16 bits simultaneously
    obj.USIIFGCC = IUSI.USIIFGCC_t  ...
    // USI interrupt flag clear control. When USIIFGCC = 1 the USIIFG will not be cleared automatically when USICNTx is written with a value > 0. 0 USIIFG automatically cleared on USICNTx update 1 USIIFG is not cleared automatically
    obj.USICNT4 = IUSI.USICNT4_t  ...
    // USI bit count bit 4 The USICNTx bits set the number of bits to be received or transmitted
    obj.USICNT3 = IUSI.USICNT3_t  ...
    // USI bit count bit 3 The USICNTx bits set the number of bits to be received or transmitted
    obj.USICNT2 = IUSI.USICNT2_t  ...
    // USI bit count bit 2 The USICNTx bits set the number of bits to be received or transmitted
    obj.USICNT1 = IUSI.USICNT1_t  ...
    // USI bit count bit 1 The USICNTx bits set the number of bits to be received or transmitted
    obj.USICNT0 = IUSI.USICNT0_t  ...
    // USI bit count bit 0 The USICNTx bits set the number of bits to be received or transmitted
 
 
struct USI.USICTL0_t
XDCscript usage meta-domain
var obj = new USI.USICTL0_t;
 
    obj.USIPE7 = IUSI.USIPE7_t  ...
    // USI SDI/SDA port enable. Input in SPI mode, input or open drain output in I2C mode. 0 USI function disabled 1 USI function enabled
    obj.USIPE6 = IUSI.USIPE6_t  ...
    // USI SDO/SCL port enable. Output in SPI mode, input or open drain output in I2C mode. 0 USI function disabled 1 USI function enabled
    obj.USIPE5 = IUSI.USIPE5_t  ...
    // USI SCLK port enable. Input in SPI slave mode, or I2C mode, output in SPI master mode. 0 USI function disabled 1 USI function enabled
    obj.USILSB = IUSI.USILSB_t  ...
    // LSB first select. This bit controls the direction of the receive and transmit shift register. 0 MSB first 1 LSB first
    obj.USIMST = IUSI.USIMST_t  ...
    // Master select 0 Slave mode 1 Master mode
    obj.USIGE = IUSI.USIGE_t  ...
    // Output latch control 0 Output latch enable depends on shift clock 1 Output latch always enabled and transparent
    obj.USIOE = IUSI.USIOE_t  ...
    // Data output enable 0 Output disabled 1 Output enabled
    obj.USISWRST = IUSI.USISWRST_t  ...
    // USI software reset 0 USI released for operation. 1 USI logic held in reset state
 
 
struct USI.USICTL1_t
XDCscript usage meta-domain
var obj = new USI.USICTL1_t;
 
    obj.USICKPH = IUSI.USICKPH_t  ...
    // Clock phase select 0 Data is changed on the first SCLK edge and captured on the following edge. 1 Data is captured on the first SCLK edge and changed on the following edge
    obj.USII2C = IUSI.USII2C_t  ...
    // I2C mode enable 0 I2C mode disabled 1 I2C mode enabled
    obj.USISTTIE = IUSI.USISTTIE_t  ...
    // START condition interrupt-enable 0 Interrupt on START condition disabled 1 Interrupt on START condition enabled
    obj.USIIE = IUSI.USIIE_t  ...
    // USI counter interrupt enable 0 Interrupt disabled 1 Interrupt enabled
    obj.USIAL = IUSI.USIAL_t  ...
    // Arbitration lost 0 No arbitration lost condition 1 Arbitration lost
    obj.USISTP = IUSI.USISTP_t  ...
    // STOP condition received. USISTP is automatically cleared if USICNTx is loaded with a value > 0 when USIIFGCC = 0. 0 No STOP condition received 1 STOP condition received
    obj.USISTTIFG = IUSI.USISTTIFG_t  ...
    // START condition interrupt flag 0 No START condition received. No interrupt pending. 1 START condition received. Interrupt pending
    obj.USIIFG = IUSI.USIIFG_t  ...
    // USI counter interrupt flag. Set when the USICNTx = 0. Automatically cleared if USICNTx is loaded with a value > 0 when USIIFGCC = 0. 0 No interrupt pending 1 Interrupt pending
 
 
USI.getAll()  // module-wide

Find all peripherals of a certain type

XDCscript usage meta-domain
USI.getAll() returns IPeripheral.Instance[]
 
DETAILS
The type of the peripherals returned is defined by the type of the caller.
RETURNS
Returns an array of IPeripheral instances
 
USI.getRegisters()  // module-wide

Find all registers defined by the peripheral

XDCscript usage meta-domain
USI.getRegisters() returns String[]
 
RETURNS
Returns an array of register names
Instance Config Parameters

XDCscript usage meta-domain
var params = new USI.Params;
// Instance config-params object
    params.USICKCTL = USI.USICKCTL_t {
    // USI Clock Control Register
        USIDIV: IUSI.USIDIV_0,
        USISSEL: IUSI.USISSEL_0,
        USICKPL: IUSI.USICKPL_OFF,
        USISWCLK: IUSI.USISWCLK_OFF
    };
    params.USICNT = USI.USICNT_t {
    // USI Bit Counter Register
        USISCLREL: IUSI.USISCLREL_OFF,
        USI16B: IUSI.USI16B_OFF,
        USIIFGCC: IUSI.USIIFGCC_OFF,
        USICNT4: IUSI.USICNT4_OFF,
        USICNT3: IUSI.USICNT3_OFF,
        USICNT2: IUSI.USICNT2_OFF,
        USICNT1: IUSI.USICNT1_OFF,
        USICNT0: IUSI.USICNT0_OFF
    };
    params.USICTL0 = USI.USICTL0_t {
    // USI Control Register 0
        USIPE7: IUSI.USIPE7_OFF,
        USIPE6: IUSI.USIPE6_OFF,
        USIPE5: IUSI.USIPE5_OFF,
        USILSB: IUSI.USILSB_OFF,
        USIMST: IUSI.USIMST_OFF,
        USIGE: IUSI.USIGE_OFF,
        USIOE: IUSI.USIOE_OFF,
        USISWRST: IUSI.USISWRST
    };
    params.USICTL1 = USI.USICTL1_t {
    // USI Control Register 1
        USICKPH: IUSI.USICKPH_OFF,
        USII2C: IUSI.USII2C_OFF,
        USISTTIE: IUSI.USISTTIE_OFF,
        USIIE: IUSI.USIIE_OFF,
        USIAL: IUSI.USIAL_OFF,
        USISTP: IUSI.USISTP_OFF,
        USISTTIFG: IUSI.USISTTIFG_OFF,
        USIIFG: IUSI.USIIFG
    };
    params.forceSetDefaultRegister = USI.ForceSetDefaultRegister_t[] [
    // Determine if each Register needs to be forced set or not
        {
            register: "USICTL0",
            regForceSet: false
        },
        {
            register: "USICTL1",
            regForceSet: false
        },
        {
            register: "USICKCTL",
            regForceSet: false
        },
        {
            register: "USICNT",
            regForceSet: false
        }
    ];
    params.name = String undefined;
    // Specific peripheral name given by the device
    params.owner = String undefined;
    // String specifying the entity that manages the peripheral
 
config USI.USICKCTL  // instance

USI Clock Control Register

XDCscript usage meta-domain
var params = new USI.Params;
  ...
params.USICKCTL = USI.USICKCTL_t {
    USIDIV: IUSI.USIDIV_0,
    USISSEL: IUSI.USISSEL_0,
    USICKPL: IUSI.USICKPL_OFF,
    USISWCLK: IUSI.USISWCLK_OFF
};
 
 
config USI.USICNT  // instance

USI Bit Counter Register

XDCscript usage meta-domain
var params = new USI.Params;
  ...
params.USICNT = USI.USICNT_t {
    USISCLREL: IUSI.USISCLREL_OFF,
    USI16B: IUSI.USI16B_OFF,
    USIIFGCC: IUSI.USIIFGCC_OFF,
    USICNT4: IUSI.USICNT4_OFF,
    USICNT3: IUSI.USICNT3_OFF,
    USICNT2: IUSI.USICNT2_OFF,
    USICNT1: IUSI.USICNT1_OFF,
    USICNT0: IUSI.USICNT0_OFF
};
 
 
config USI.USICTL0  // instance

USI Control Register 0

XDCscript usage meta-domain
var params = new USI.Params;
  ...
params.USICTL0 = USI.USICTL0_t {
    USIPE7: IUSI.USIPE7_OFF,
    USIPE6: IUSI.USIPE6_OFF,
    USIPE5: IUSI.USIPE5_OFF,
    USILSB: IUSI.USILSB_OFF,
    USIMST: IUSI.USIMST_OFF,
    USIGE: IUSI.USIGE_OFF,
    USIOE: IUSI.USIOE_OFF,
    USISWRST: IUSI.USISWRST
};
 
 
config USI.USICTL1  // instance

USI Control Register 1

XDCscript usage meta-domain
var params = new USI.Params;
  ...
params.USICTL1 = USI.USICTL1_t {
    USICKPH: IUSI.USICKPH_OFF,
    USII2C: IUSI.USII2C_OFF,
    USISTTIE: IUSI.USISTTIE_OFF,
    USIIE: IUSI.USIIE_OFF,
    USIAL: IUSI.USIAL_OFF,
    USISTP: IUSI.USISTP_OFF,
    USISTTIFG: IUSI.USISTTIFG_OFF,
    USIIFG: IUSI.USIIFG
};
 
 
config USI.forceSetDefaultRegister  // instance

Determine if each Register needs to be forced set or not

XDCscript usage meta-domain
var params = new USI.Params;
  ...
const params.forceSetDefaultRegister = USI.ForceSetDefaultRegister_t[] [
    {
        register: "USICTL0",
        regForceSet: false
    },
    {
        register: "USICTL1",
        regForceSet: false
    },
    {
        register: "USICKCTL",
        regForceSet: false
    },
    {
        register: "USICNT",
        regForceSet: false
    }
];
 
 
config USI.name  // instance

Specific peripheral name given by the device

XDCscript usage meta-domain
var params = new USI.Params;
  ...
params.name = String undefined;
 
DETAILS
Devices can have more than one peripheral of the same type. In such cases, device data sheets give different names to the instances of a same peripheral. For example, the name for a timer module could be TimerA3, and a device that has two such timers can name them TA0 and TA1.
 
config USI.owner  // instance

String specifying the entity that manages the peripheral

XDCscript usage meta-domain
var params = new USI.Params;
  ...
params.owner = String undefined;
 
Instance Creation

XDCscript usage meta-domain
var params = new USI.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = USI.create(IClock.Instance clock, params);
// Create an instance-object
 
USI.getUSIIE()  // instance

Gets USIIE register

XDCscript usage meta-domain
inst.getUSIIE() returns Bool
 
SEE
 
USI.getUSISTTIE()  // instance

Gets USISTTIE register

XDCscript usage meta-domain
inst.getUSISTTIE() returns Bool
 
SEE
 
USI.setUSIIE()  // instance

Sets USIIE register

XDCscript usage meta-domain
inst.setUSIIE(Bool set) returns Bool
 
SEE
 
USI.setUSISTTIE()  // instance

Sets USISTTIE register

XDCscript usage meta-domain
inst.setUSISTTIE(Bool set) returns Bool
 
SEE
generated on Thu, 17 Nov 2011 02:05:05 GMT