metaonly module ti.catalog.msp430.peripherals.svs.SVS

MSP430F2xx Family SVS Module

XDCscript usage meta-domain sourced in ti/catalog/msp430/peripherals/svs/SVS.xdc
var SVS = xdc.useModule('ti.catalog.msp430.peripherals.svs.SVS');
module-wide constants & types
    values of type SVS.PORON_t// PORON Bit
        const SVS.PORON// SVSFG causes a POR;
 
    values of type SVS.SVSFG_t// SVSFG Bit
        const SVS.SVSFG_OFF;
        const SVS.SVSFG;
 
    values of type SVS.SVSON_t// SVSON Bit
        const SVS.SVSON_OFF;
        const SVS.SVSON;
 
    values of type SVS.SVSOP_t// SVSOP Bit
        const SVS.SVSOP_OFF;
        const SVS.SVSOP;
 
    values of type SVS.VLD0_t// VLD0 Bit
        const SVS.VLD0_OFF;
        const SVS.VLD0;
 
    values of type SVS.VLD1_t// VLD1 Bit
        const SVS.VLD1_OFF;
        const SVS.VLD1;
 
    values of type SVS.VLD2_t// VLD2 Bit
        const SVS.VLD2_OFF;
        const SVS.VLD2;
 
    values of type SVS.VLD3_t// VLD3 Bit
        const SVS.VLD3_OFF;
        const SVS.VLD3;
 
        obj.register = String  ...
        obj.regForceSet = Bool  ...
 
    var obj = new SVS.SVSCTL_t// SVSCTL Register;
module-wide functions
per-instance config parameters
    var params = new SVS.Params// Instance config-params object;
        params.SVSCTL// SVSCTL Register = SVS.SVSCTL_t {
            VLD3: ISVS.VLD3_OFF,
            VLD2: ISVS.VLD2_OFF,
            VLD1: ISVS.VLD1_OFF,
            VLD0: ISVS.VLD0_OFF,
            PORON: ISVS.PORON_OFF,
            SVSON: ISVS.SVSON_OFF,
            SVSOP: ISVS.SVSOP_OFF,
            SVSFG: ISVS.SVSFG_OFF
        };
            {
                register: "SVSCTL",
                regForceSet: false
            }
        ];
        params.name// Specific peripheral name given by the device = String undefined;
        params.owner// String specifying the entity that manages the peripheral = String undefined;
per-instance creation
    var inst = SVS.create// Create an instance-object(params);
 
 
enum SVS.PORON_t

PORON Bit

XDCscript usage meta-domain
values of type SVS.PORON_t
    const SVS.PORON_OFF;
    // SVSFG does not cause a POR
    const SVS.PORON;
    // SVSFG causes a POR
 
 
enum SVS.SVSFG_t

SVSFG Bit

XDCscript usage meta-domain
values of type SVS.SVSFG_t
    const SVS.SVSFG_OFF;
    const SVS.SVSFG;
 
 
enum SVS.SVSON_t

SVSON Bit

XDCscript usage meta-domain
values of type SVS.SVSON_t
    const SVS.SVSON_OFF;
    const SVS.SVSON;
 
 
enum SVS.SVSOP_t

SVSOP Bit

XDCscript usage meta-domain
values of type SVS.SVSOP_t
    const SVS.SVSOP_OFF;
    const SVS.SVSOP;
 
 
enum SVS.VLD0_t

VLD0 Bit

XDCscript usage meta-domain
values of type SVS.VLD0_t
    const SVS.VLD0_OFF;
    const SVS.VLD0;
 
 
enum SVS.VLD1_t

VLD1 Bit

XDCscript usage meta-domain
values of type SVS.VLD1_t
    const SVS.VLD1_OFF;
    const SVS.VLD1;
 
 
enum SVS.VLD2_t

VLD2 Bit

XDCscript usage meta-domain
values of type SVS.VLD2_t
    const SVS.VLD2_OFF;
    const SVS.VLD2;
 
 
enum SVS.VLD3_t

VLD3 Bit

XDCscript usage meta-domain
values of type SVS.VLD3_t
    const SVS.VLD3_OFF;
    const SVS.VLD3;
 
 
struct SVS.ForceSetDefaultRegister_t

Force Set Default Register

XDCscript usage meta-domain
var obj = new SVS.ForceSetDefaultRegister_t;
 
    obj.register = String  ...
    obj.regForceSet = Bool  ...
 
DETAILS
Type to store if each register needs to be forced initialized even if the register is in default state.
SEE
 
struct SVS.SVSCTL_t

SVSCTL Register

XDCscript usage meta-domain
var obj = new SVS.SVSCTL_t;
 
    obj.VLD3 = SVS.VLD3_t  ...
    // Voltage level detect. These bits turn on the SVS and select the nominal SVS threshold voltage level. See the device specific data sheet for parameters. 0000 SVS is off 0001 1.9 V 0010 2.1 V 0011 2.2 V 0100 2.3 V 0101 2.4 V 0110 2.5 V 0111 2.65 V 1000 2.8 V 1001 2.9 V 1010 3.05 1011 3.2 V 1100 3.35 V 1101 3.5 V 1110 3.7 V 1111 Compares external input voltage SVSIN to 1.25 V
    obj.VLD2 = SVS.VLD2_t  ...
    // Voltage level detect. These bits turn on the SVS and select the nominal SVS threshold voltage level. See the device specific data sheet for parameters. 0000 SVS is off 0001 1.9 V 0010 2.1 V 0011 2.2 V 0100 2.3 V 0101 2.4 V 0110 2.5 V 0111 2.65 V 1000 2.8 V 1001 2.9 V 1010 3.05 1011 3.2 V 1100 3.35 V 1101 3.5 V 1110 3.7 V 1111 Compares external input voltage SVSIN to 1.25 V
    obj.VLD1 = SVS.VLD1_t  ...
    // Voltage level detect. These bits turn on the SVS and select the nominal SVS threshold voltage level. See the device specific data sheet for parameters. 0000 SVS is off 0001 1.9 V 0010 2.1 V 0011 2.2 V 0100 2.3 V 0101 2.4 V 0110 2.5 V 0111 2.65 V 1000 2.8 V 1001 2.9 V 1010 3.05 1011 3.2 V 1100 3.35 V 1101 3.5 V 1110 3.7 V 1111 Compares external input voltage SVSIN to 1.25 V
    obj.VLD0 = SVS.VLD0_t  ...
    // Voltage level detect. These bits turn on the SVS and select the nominal SVS threshold voltage level. See the device specific data sheet for parameters. 0000 SVS is off 0001 1.9 V 0010 2.1 V 0011 2.2 V 0100 2.3 V 0101 2.4 V 0110 2.5 V 0111 2.65 V 1000 2.8 V 1001 2.9 V 1010 3.05 1011 3.2 V 1100 3.35 V 1101 3.5 V 1110 3.7 V 1111 Compares external input voltage SVSIN to 1.25 V
    obj.PORON = SVS.PORON_t  ...
    // POR on. This bit enables the SVSFG flag to cause a POR device reset. 0 SVSFG does not cause a POR 1 SVSFG causes a POR
    obj.SVSON = SVS.SVSON_t  ...
    // SVS on. This bit reflects the status of SVS operation. This bit DOES NOT turn on the SVS. The SVS is turned on by setting VLDx > 0. 0 SVS is Off 1 SVS is On
    obj.SVSOP = SVS.SVSOP_t  ...
    // SVS output. This bit reflects the output value of the SVS comparator. 0 SVS comparator output is low 1 SVS comparator output is high
    obj.SVSFG = SVS.SVSFG_t  ...
    // SVS flag. This bit indicates a low voltage condition. SVSFG remains set after a low voltage condition until reset by software. 0 No low voltage condition occurred 1 A low condition is present or has occurred
 
 
SVS.getAll()  // module-wide

Find all peripherals of a certain type

XDCscript usage meta-domain
SVS.getAll() returns IPeripheral.Instance[]
 
DETAILS
The type of the peripherals returned is defined by the type of the caller.
RETURNS
Returns an array of IPeripheral instances
 
SVS.getRegisters()  // module-wide

Find all registers defined by the peripheral

XDCscript usage meta-domain
SVS.getRegisters() returns String[]
 
RETURNS
Returns an array of register names
Instance Config Parameters

XDCscript usage meta-domain
var params = new SVS.Params;
// Instance config-params object
    params.SVSCTL = SVS.SVSCTL_t {
    // SVSCTL Register
        VLD3: ISVS.VLD3_OFF,
        VLD2: ISVS.VLD2_OFF,
        VLD1: ISVS.VLD1_OFF,
        VLD0: ISVS.VLD0_OFF,
        PORON: ISVS.PORON_OFF,
        SVSON: ISVS.SVSON_OFF,
        SVSOP: ISVS.SVSOP_OFF,
        SVSFG: ISVS.SVSFG_OFF
    };
    params.forceSetDefaultRegister = SVS.ForceSetDefaultRegister_t[] [
    // Determine if each Register needs to be forced set or not
        {
            register: "SVSCTL",
            regForceSet: false
        }
    ];
    params.name = String undefined;
    // Specific peripheral name given by the device
    params.owner = String undefined;
    // String specifying the entity that manages the peripheral
 
config SVS.SVSCTL  // instance

SVSCTL Register

XDCscript usage meta-domain
var params = new SVS.Params;
  ...
params.SVSCTL = SVS.SVSCTL_t {
    VLD3: ISVS.VLD3_OFF,
    VLD2: ISVS.VLD2_OFF,
    VLD1: ISVS.VLD1_OFF,
    VLD0: ISVS.VLD0_OFF,
    PORON: ISVS.PORON_OFF,
    SVSON: ISVS.SVSON_OFF,
    SVSOP: ISVS.SVSOP_OFF,
    SVSFG: ISVS.SVSFG_OFF
};
 
 
config SVS.forceSetDefaultRegister  // instance

Determine if each Register needs to be forced set or not

XDCscript usage meta-domain
var params = new SVS.Params;
  ...
const params.forceSetDefaultRegister = SVS.ForceSetDefaultRegister_t[] [
    {
        register: "SVSCTL",
        regForceSet: false
    }
];
 
 
config SVS.name  // instance

Specific peripheral name given by the device

XDCscript usage meta-domain
var params = new SVS.Params;
  ...
params.name = String undefined;
 
DETAILS
Devices can have more than one peripheral of the same type. In such cases, device data sheets give different names to the instances of a same peripheral. For example, the name for a timer module could be TimerA3, and a device that has two such timers can name them TA0 and TA1.
 
config SVS.owner  // instance

String specifying the entity that manages the peripheral

XDCscript usage meta-domain
var params = new SVS.Params;
  ...
params.owner = String undefined;
 
Instance Creation

XDCscript usage meta-domain
var params = new SVS.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = SVS.create(params);
// Create an instance-object
generated on Wed, 20 Jul 2011 20:35:47 GMT